Other Parts Discussed in Thread: TMDSHVMTRINSPIN
硬件配置:TMDSHVMTRINSPIN + 28069
软件环境:使用的是TMDSHVMTRINSPIN自带的板上仿真器 + CCS6.1,驱动都安装了。
硬件配置步骤也是参考了TI提供的文档。
没有上高电压,只用了15V电源。
现在的问题:无法连接到target:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMDSHVMTRINSPIN
硬件配置:TMDSHVMTRINSPIN + 28069
软件环境:使用的是TMDSHVMTRINSPIN自带的板上仿真器 + CCS6.1,驱动都安装了。
硬件配置步骤也是参考了TI提供的文档。
没有上高电压,只用了15V电源。
现在的问题:无法连接到target:
我升级到了CCS V8了,还是不行呢。
我进行Test Connection后,出现:
This error is generated by TI's USCIF driver or utilities.
The value is '-151' (0xffffff69).
The title is 'SC_ERR_FTDI_OPEN'.
The explanation is:
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
[End: Texas Instruments XDS100v2 USB Debug Probe_0]