想问下。经过交流输入后的直流源范围能有多少?,
AC Power Entry [M1]: The [M1] macro can rectify AC input (85-132VAC/ 170-250VAC) fed to the board through [Main]-P1. This rectified AC can then generate DC voltage with help of capacitor bank present at input of the inverter stage. For this a cable needs to be connected between [Main]-BS1 and [Main]-BS5. Note that no connection to the ground i.e. [Main]-BS6 is necessary as the GND after rectification is the same as the board ground.
问下这个整流后DC voltage的范围