This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28069高压套件交流源(170v-250v)整流为直流源之后直流源范围多少?



想问下。经过交流输入后的直流源范围能有多少?,

AC Power Entry [M1]: The [M1] macro can rectify AC input (85-132VAC/ 170-250VAC) fed to the board through [Main]-P1. This rectified AC can then generate DC voltage with help of capacitor bank present at input of the inverter stage. For this a cable needs to be connected between [Main]-BS1 and [Main]-BS5. Note that no connection to the ground i.e. [Main]-BS6 is necessary as the GND after rectification is the same as the board ground.

问下这个整流后DC voltage的范围