This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320方8377DZWT的内核电压1.2V和IO电压3.3V的上电顺序?

Other Parts Discussed in Thread: TMS320F28335

TMS320方8377DZWT的内核电压1.2V和IO电压3.3V的上电顺序?如果是先上电IO 3.3V,为什么与TMS320F28335 DSP不一样?

  • 能解释一下,为什么和TMS320F28335上电顺序不一样?上电顺序不一样的原理?上电顺序相反可能会出现的风险?谢谢!

  • 能解释一下,为什么和TMS320F28335上电顺序不一样?上电顺序不一样的原理?上电顺序相反可能会出现的风险?谢谢!
    Eric:
    F2837x 的上电顺序要求:
    The voltage on VDDIO should be greater than VDD or no less than 0.3 V below VDD at all times. VDDIO,
    VDD3VFL, VDDOSC, and VDDA should be powered up together and be kept within 0.3 V of each other during
    operation. Before powering the device, no voltage larger than 0.3 V above VDDIO should be applied to any
    digital pin, and no voltage larger than 0.3 V above VDDA should be applied to any analog pin.

    F28335的上电顺序要求:
    No requirements are placed on the power up/down sequence of the various power pins to ensure the
    correct reset state for all the modules. However, if the 3.3-V transistors in the level shifting output buffers
    of the I/O pins are powered prior to the 1.9-V transistors, it is possible for the output buffers to turn on,
    causing a glitch to occur on the pin during power up. To avoid this behavior, power the VDD pins prior to or
    simultaneously with the VDDIO pins, ensuring that the VDD pins have reached 0.7 V before the VDDIO pins
    reach 0.7 V.

    上面的内容也没有说F2837x的上电需要VDDIO先上电,也可以是同时上电,只要满足别低于VDD 0.3V即可。
    至于上电顺序没满足要求,有可能是芯片不能正确初始化,导致一些外设异常。