This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于EQEP的x4功能



 在eqep模块中,具有一个x4的设置寄存器,个人有点不明白,编码器线束都是出厂设定的,内部对编码器的信号进行逻辑处理,会提高精度么?

 

  • 楼主你好!

    编码器是线数是指转一圈说输出的A或者B输出的脉冲数,如果值测一个输入(A或者B)的一个边缘的话,那么转一圈QEP所记脉冲数就是编码器的线数,但是QEP模块采用对A和B信号的上升沿和下降沿分别计数的话,电机转一圈QEP所能计的脉冲数将变成是编码器线数的4倍。等效成同样转速转一圈的话,每个计数之间的时间间隔减小,因此精度也就提高了!

  • johnson chen :

           目前有一个只输出单相脉冲信号的256线编码器,一个方向信号。

           用28035进行上升/下降沿计数,如果我单纯通过一个倍频电路,对这个信号进行倍频,然后再进行转速测量,那么这样对提高转速采集的精度应该是有帮助的吧?