本人刚开始学习TMS320F28335开发板,使用音频模块的时候有如下两个问题,还请前辈们解答:
1、使用lab7例程时,为什么停止仿真之后为什么语音录放不暂停?
2、当我把中断函数里的代码屏蔽之后还可以正常录放音,难道录放音的实现与中断没有关系?
#include "DSP2833x_Device.h" // DSP2833x Headerfile Include File
#include "DSP2833x_Examples.h" // DSP2833x Examples Include File
Uint16 volume,tAicRegs;
int ADbuf[500];
int DA_wptr,DA_rptr,y;
Uint16 play_mode=1;
void main(void)
{
Uint16 temp,i;
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2833x_SysCtrl.c file.
InitSysCtrl();
// Step 2. Initalize GPIO:
// This example function is found in the DSP2833x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio(); // Skipped for this example
// For this example, only enable the GPIO for McBSP-A
InitXintf16Gpio();
InitMcbspaGpio();
EALLOW;
GpioCtrlRegs.GPAMUX1.bit.GPIO12 = 0; //aic_dat 0为数字IO模式,1为外设IO模式
GpioCtrlRegs.GPADIR.bit.GPIO12 = 1; //0为输入方向,1为输出方向
GpioCtrlRegs.GPAPUD.bit.GPIO12 = 0; //使能内部上拉电阻
GpioCtrlRegs.GPAMUX1.bit.GPIO13 = 0; //aic_CS
GpioCtrlRegs.GPADIR.bit.GPIO13 = 1;
GpioCtrlRegs.GPAPUD.bit.GPIO13 = 0;
GpioCtrlRegs.GPBMUX2.bit.GPIO61 = 0; //aic_clk
GpioCtrlRegs.GPBDIR.bit.GPIO61 = 1;
GpioCtrlRegs.GPBPUD.bit.GPIO61 = 0;
EDIS;
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;
// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2833x_PieCtrl.c file.
InitPieCtrl(); //IER\IFR寄存器清零
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in DSP2833x_DefaultIsr.c.
// This function is found in DSP2833x_PieVect.c.
InitPieVectTable(); //**初始化向量表(为PIE向量表中的所有中断向量配置对应向量的入口地址)
// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP2833x_InitPeripherals.c
// InitPeripherals(); // Not required for this example
InitMcbspa(); // Initalize the Mcbsp-A in loopback test mode
// tAicRegs = 0xFF;
// SysReg = tAicRegs;
InitAic23(); //aic23配置(单步调试声音变大)
delay(500);
volume=90;
WriteAic23(L_HEADPHONE_VOLUME,0x0180+volume);//改变音量
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.MRINTA = &ISRMcbspSend; //把函数的地址赋值给中断向量MRINTA的向量地址中
EDIS; // This is needed to disable write to EALLOW protected registers
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
PieCtrlRegs.PIEIER6.bit.INTx5=1; // Enable PIE Group 6, INT 5
IER |= M_INT6; // Enable CPU INT6
EINT; // Enable Global interrupt INTM
while(1)
{
for(temp=30000;temp>0;temp-=100)
{
for(i=0;i<2;i++)
{
y=5000;
delay(temp); //播放警报
// McbspaRegs.DXR1.all = y;
y=-5000;
delay(temp); //播放警报
// McbspaRegs.DXR1.all = y;
}
}
}
}
interrupt void ISRMcbspSend(void)
{
// int temp;
//
// PieCtrlRegs.PIEACK.all = PIEACK_GROUP6;
// temp=McbspaRegs.DRR1.all;
//
// DA_rptr++;
// if(DA_rptr>=500)
// DA_rptr=0;
//
// ADbuf[DA_rptr]=temp; //保存录音数据
//
// if(play_mode==0)
// McbspaRegs.DXR1.all = y;
// //警报声的幅值
// else
// McbspaRegs.DXR1.all = temp; //放音
}