This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP28335单句浮点除法运算耗时1.5us,如何优化



  1. 最近在写28335的程序的时候,发现单句浮点除法的耗时达到1.5us,这正常吗?如何优化呢?
  2. 本句比较关键,需要在短时间内完成,1.5us的时间太长,所以才想优化。看到别人测试1000次除法运算需要458us,是因为连续运算所以可以达到平均每次除法能够达到0.45us吗?

网友测试:blog.csdn.net/.../49720813

具体信息如下:

  • 时钟频率150MHz
  • 计算时间采用计算前拉高电平,计算后那低电平,用示波器看时间间隔的方式得到
  • 工程Property中已经设置rts2000_fpu32.lib
  • 程序在RAM中运行
  • 除数与被除数都是变量