我想估计一下TMS320F28335的功耗来选择合适的电源芯片,请问DSP的功耗是按照数据手册里的功耗与频率的曲线进行估计吗?按照TMS320F28335频率150MHZ查曲线大概是880mW,这样对吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想估计一下TMS320F28335的功耗来选择合适的电源芯片,请问DSP的功耗是按照数据手册里的功耗与频率的曲线进行估计吗?按照TMS320F28335频率150MHZ查曲线大概是880mW,这样对吗?
您好,这个是表5-1,如果我需要计算所有引脚都使用的情况下的功耗,我是应该将上表中的所有电流最大值*对应VDD吗?如P=315mA*VDD+50mA*VDDIO+40mA*VDD3VFL+35mA*VDDA18+2mA*VDDA33,这样对吗?IDDIO是每个引脚的电流还是该电源对应所有引脚的总电流呢?
此外,留意到test conditions中的最后一句话,所有IO管脚都保持未连接的状态,意思是上表中的电源电流均为IO悬空时的电流吗?但是注释中又说IDDIO取决于IO引脚上的电气负载,那么上表中的电流究竟是IO连接负载还是没连接的情况呢?
这是表5-3,如果我的外设实际没有全用到,那么上表的电流指的是我每有一个引脚闲置所造成的电流减少吗?如ADC引脚有两个闲置,那么我的IDD=315mA-2*8mA?这样算的对吗?