This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dsp28335调用FFT库函数问题



你好,我现在正在用28335写一个FFT求谐波畸变率程序,由于是第一次次写,所以遇到些问题,首先问一下,调用FFT库需要对CCS进行配置吗?现在我写的程序感觉虽然调用的函数,但是该函数并没有执行

  • #include "DSP2833x_Device.h"     // DSP2833x Headerfile Include File

    #include "DSP2833x_Examples.h"   // DSP2833x Examples Include File

    #include <math.h>

    //#include "AdRead.h"

    #include "rms.h"

    #include "Harmonic.h"

    #include "Power.h"

    #include "GridFrequency.h"

    #include "FPU.h"

    #include "C28X_FPU_FASTRTS.h"

    int16    Adiniflag=0;     //AD开始初始化该标志为1,AD采样中为0

    int16    Adiniover=0;     //AD初始化结束标志

    Uint16 N = 32;         //32采样点数

    float32 NNi = 0.0078125;

    Uint16 MAX = 50;

    int16 x1=0;

    int A=0;

    void ADdatadeal();

    void Para_deal();

    void Adinitial();

    void FFtCaculate(RFFT_F32_STRUCT fft,float32 ipcb1[],float32 mag[],float32 Inbuffer[]);

    #define     Np   128

    #define FFT_STAGES 7

    float32  TwiddleBuffer[Np];

    RFFT_F32_STRUCT  fft32;

    float32 sin_table[128],cos_table[128];

    //ADREAD   adread1 = ADREAD_DEFAULTS;

    POWER    power1 = POWER_DEFAULTS;

    HARMONIC harmonic1 = HARMONIC_DEFAULTS;

    RMS      rms1 = RMS_DEFAULTS;

    union Urms Urms1;

    union Irms Irms1;

    union Pmeas Pmeas1;

    union UIgain Us,Is,Ig;

    int16 Uab_flag=0;

    int16 Ubc_flag=0;

    int16 Uca_flag=0;

    int16 Isa_flag=0;

    int16 Isb_flag=0;

    int16 Isc_flag=0;

    int16 Ila_flag=0;

    int16 Ilb_flag=0;

    int16 Ilc_flag=0;

    int16 Ica_flag=0;

    int16 Icb_flag=0;

    int16 Icc_flag=0;

    float32 ipcbUab[Np];//实部,虚部

    float32 ipcbUbc[Np];

    float32 ipcbUca[Np];

    float32 ipcbIsa[Np];

    float32 ipcbIsb[Np];

    float32 ipcbIsc[Np];

    float32 ipcbIla[Np];

    float32 ipcbIlb[Np];

    float32 ipcbIlc[Np];

    float32 magUab[Np/2];//幅值

    float32 magUbc[Np/2];

    float32 magUca[Np/2];

    float32 magIsa[Np/2];

    float32 magIsb[Np/2];

    float32 magIsc[Np/2];

    float32 magIla[Np/2];

    float32 magIlb[Np/2];

    float32 magIlc[Np/2];

    float32 f_Uab[Np];//FFT输入

    float32 f_Ubc[Np];

    float32 f_Uca[Np];

    float32 f_Isa[Np];

    float32 f_Isb[Np];

    float32 f_Isc[Np];

    float32 f_Ila[Np];

    float32 f_Ilb[Np];

    float32 f_Ilc[Np];

    void Para_deal()

    {

      unsigned int i;

      for(i=0;i<128;i++)

      {

      sin_table[i]=3*sin(i/128.0*6.283185307179586476925286766559);

    cos_table[i]=3*cos(i/128.0*6.283185307179586476925286766559);

    if(i==127)

     A=1;

      }

     /* if(Adiniflag==1)

      Adinitial();

     adread1.Ugain=Us.Kabcf;  //变比

     adread1.Isgain=Is.Kabcf;

     adread1.Iggain=Ig.Kabcf;

     ADdatadeal(&adread1);

     rms1.N = Np;

     rms1.Ni = NNi;

     rms1.Uabp = adread1.Umeasabgrid;   //实际值

     //rms1.Ubcp = adread1.Umeasbcpt; //实际值

     //rms1.Ucap = adread1.Umeascapt;

     rms1.Ilap = adread1.ImeasIagrid1;

     //rms1.Ilbp = adread1.ImeasIlbpt;

     //rms1.Ilcp = adread1.ImeasIlcpt;

     //rms1.Isap = adread1.ImeasIsapt;

     // rms1.Isbp = adread1.ImeasIsbpt;

     rms1.Iscp = adread1.ImeasIcgrid2;

     rms1.Icap = adread1.ImeasIasvg1;

     //rms1.Icbp = adread1.ImeasIcbpt;

     //rms1.Iccp = adread1.ImeasIccpt;

     rms_calc(&rms1);

    // ------------------------------------------------------------------------------  

     if ((Uab_flag==1)&&(Ubc_flag==1)&&(Uca_flag==1)

          &&(Isa_flag==1)&&(Isb_flag==1)&&(Isc_flag==1)

          &&(Ila_flag==1)&&(Ila_flag==1)&&(Ila_flag==1))// If the samples are acquired */    

               if(A==1)

               {                                    

                 FFtCaculate(fft32,ipcbUab,magUab,sin_table);

     FFtCaculate(fft32,ipcbUbc,magUbc,cos_table);

     //FFtCaculate(fft32,ipcbUca,magUca,f_Uca);

    // FFtCaculate(fft32,ipcbIsa,magIsa,f_Isa);

     //FFtCaculate(fft32,ipcbIsa,magIsa,f_Isb);

     //FFtCaculate(fft32,ipcbIsc,magIsc,f_Isc);

     //FFtCaculate(fft32,ipcbIla,magIla,f_Ila);

     //FFtCaculate(fft32,ipcbIlb,magIlb,f_Ilb);

     //FFtCaculate(fft32,ipcbIlc,magIlc,f_Ilc);  

     A=0;                                                        

               }

    这是我写的程序