"../Source/28004x_generic_flash_lnk.cmd", line 77: error #10099-D: program will not fit into available memory. placement with alignment/blocking fails for section ".text" size 0x5a60 page 0. Available memory ranges:
FLASH_BANK0_SEC2 size: 0x1000 unused: 0x0 max hole: 0x0
FLASH_BANK0_SEC3 size: 0x1000 unused: 0x1 max hole: 0x1
FLASH_BANK0_SEC4 size: 0x1000 unused: 0x5 max hole: 0x5
FLASH_BANK0_SEC5 size: 0x1000 unused: 0x3 max hole: 0x3
FLASH_BANK0_SEC6 size: 0x1000 unused: 0x88c max hole: 0x88c
FLASH_BANK0_SEC7 size: 0x1000 unused: 0x6e0 max hole: 0x6e0
FLASH_BANK0_SEC8 size: 0x1000 unused: 0x1000 max hole: 0x1000
FLASH_BANK0_SEC9 size: 0x1000 unused: 0x1000 max hole: 0x1000
請問目前遇到了上述問題,但是他所寫出來.text需要的大小是0x5a60,但是我給予的空間有8個page = 0x8000的空間,應該是足夠的,但是還是會跳出這個問題