This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

error #10099-D 報錯 但是空間足夠



"../Source/28004x_generic_flash_lnk.cmd", line 77: error #10099-D: program will not fit into available memory. placement with alignment/blocking fails for section ".text" size 0x5a60 page 0. Available memory ranges:


FLASH_BANK0_SEC2 size: 0x1000 unused: 0x0 max hole: 0x0 
FLASH_BANK0_SEC3 size: 0x1000 unused: 0x1 max hole: 0x1 
FLASH_BANK0_SEC4 size: 0x1000 unused: 0x5 max hole: 0x5 
FLASH_BANK0_SEC5 size: 0x1000 unused: 0x3 max hole: 0x3 
FLASH_BANK0_SEC6 size: 0x1000 unused: 0x88c max hole: 0x88c 
FLASH_BANK0_SEC7 size: 0x1000 unused: 0x6e0 max hole: 0x6e0 
FLASH_BANK0_SEC8 size: 0x1000 unused: 0x1000 max hole: 0x1000 
FLASH_BANK0_SEC9 size: 0x1000 unused: 0x1000 max hole: 0x1000

請問目前遇到了上述問題,但是他所寫出來.text需要的大小是0x5a60,但是我給予的空間有8個page = 0x8000的空間,應該是足夠的,但是還是會跳出這個問題

  • 请您给出一下您的CMD文件,谢谢
  • MEMORY
    {
    PAGE 0 :
    /* BEGIN is used for the "boot to Flash" bootloader mode */

    BEGIN : origin = 0x080000, length = 0x000002
    RAMM0 : origin = 0x0000F5, length = 0x00030B

    RAMLS0 : origin = 0x008000, length = 0x000800
    RAMLS1 : origin = 0x008800, length = 0x000800
    RAMLS2 : origin = 0x009000, length = 0x000800
    RAMLS3 : origin = 0x009800, length = 0x000800
    RAMLS4 : origin = 0x00A000, length = 0x000800
    //RAMLS24 : origin = 0x009000, length = 0x001800


    RESET : origin = 0x3FFFC0, length = 0x000002

    /* Flash sectors */
    /* BANK 0 */
    FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x000FFE /* on-chip Flash */
    FLASH_BANK0_SEC1 : origin = 0x081000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC3 : origin = 0x083000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC4 : origin = 0x084000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC5 : origin = 0x085000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC6 : origin = 0x086000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC7 : origin = 0x087000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC9 : origin = 0x089000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x001000 /* on-chip Flash */

    /* BANK 1 */
    FLASH_BANK1_SEC0 : origin = 0x090000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK1_SEC1 : origin = 0x091000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK1_SEC2 : origin = 0x092000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK1_SEC3 : origin = 0x093000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK1_SEC4 : origin = 0x094000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK1_SEC5 : origin = 0x095000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK1_SEC6 : origin = 0x096000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK1_SEC7 : origin = 0x097000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK1_SEC8 : origin = 0x098000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK1_SEC9 : origin = 0x099000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x001000 /* on-chip Flash */

    PAGE 1 :

    BOOT_RSVD : origin = 0x000002, length = 0x0000F3 /* Part of M0, BOOT rom will use this for stack */
    RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */

    RAMLS5 : origin = 0x00A800, length = 0x000800
    RAMLS6 : origin = 0x00B000, length = 0x000800
    RAMLS7 : origin = 0x00B800, length = 0x000800

    RAMGS0 : origin = 0x00C000, length = 0x002000
    RAMGS1 : origin = 0x00E000, length = 0x002000
    RAMGS2 : origin = 0x010000, length = 0x002000
    RAMGS3 : origin = 0x012000, length = 0x002000
    }


    SECTIONS
    {
    codestart : > BEGIN, PAGE = 0, ALIGN(4)
    ///.text : >>FLASH_BANK0_SEC1 | FLASH_BANK0_SEC2 | FLASH_BANK0_SEC3, PAGE = 0, ALIGN(4)
    .text : >> FLASH_BANK0_SEC5 | FLASH_BANK0_SEC6 | FLASH_BANK0_SEC7 | FLASH_BANK0_SEC8 | FLASH_BANK0_SEC9 | FLASH_BANK0_SEC10| FLASH_BANK0_SEC11| FLASH_BANK0_SEC12, PAGE = 0, ALIGN(4)

    .cinit : > FLASH_BANK0_SEC1, PAGE = 0, ALIGN(4)
    .pinit : > FLASH_BANK0_SEC1, PAGE = 0, ALIGN(4)
    .switch : > FLASH_BANK0_SEC1, PAGE = 0, ALIGN(4)
    .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */

    .cio : > RAMLS0, PAGE = 0
    .stack : > RAMM1, PAGE = 1
    .ebss : > RAMLS5, PAGE = 1
    .esysmem : > RAMLS5, PAGE = 1
    .econst : > FLASH_BANK0_SEC7 , PAGE = 0, ALIGN(4)

    ramgs0 : > RAMGS0, PAGE = 1
    ramgs1 : > RAMGS1, PAGE = 1

    .TI.ramfunc : LOAD = FLASH_BANK0_SEC0,
    RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
    LOAD_START(_RamfuncsLoadStart),
    LOAD_SIZE(_RamfuncsLoadSize),
    LOAD_END(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart),
    RUN_SIZE(_RamfuncsRunSize),
    RUN_END(_RamfuncsRunEnd),
    PAGE = 0, ALIGN(4)

    }

    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
  • 目前試過將目前BANK0的SEC改成這樣

    原本

    FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x000FFE /* on-chip Flash */
    FLASH_BANK0_SEC1 : origin = 0x081000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC3 : origin = 0x083000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC4 : origin = 0x084000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC5 : origin = 0x085000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC6 : origin = 0x086000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC7 : origin = 0x087000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC9 : origin = 0x089000, length = 0x001000 /* on-chip Flash */

    修改過後

    FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x000FFE /* on-chip Flash */
    FLASH_BANK0_SEC1 : origin = 0x081000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000 /* on-chip Flash */
    FLASH_BANK0_SEC3 : origin = 0x083000, length = 0x005000 /* on-chip Flash */
    FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000 /* on-chip Flash */

    再把SECTIONS裡面的.text改成這樣就不會報錯

    .text : >> FLASH_BANK1_SEC2 | FLASH_BANK1_SEC3 , PAGE = 0, ALIGN(4)

    順便問一下這樣設定是正常的嗎?