This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335的spi使用问题



Ti工程师您好:

我需要使用spi对AT45db321进行操作,首先我想读取芯片ID,根据手册需要向芯片发送功能码9F,之后读取四字节的芯片信息,不过RXBUF中的值都是我发送的值。而且DSP的MISO引脚一直是高电平,我不明白DSP是怎么收到的这些数据。

SPI配置:

***=0x87;

***=0X06;

SPIBRR=0X7F;

SPIPRI.bit.FREE=1;

SPIFFTX=0XE040;

SPIFFRX=0X204F;

SPIFFCT=0;

程序大致是这样

send_byte(0x9f); // 发送功能码

temp1=get_byte(0xa5);

temp2=get_byte(0xa5);

temp3=get_byte(0xa5);

temp3=get_byte(0xa5);//我感觉应该是随便发数据,进而得到外设的ID信息

但是我收到的都是temp1temp2temp3temp4都是A5FF,而且dsp的MISO引脚一直是高电平,其他引脚像CLK引脚、MOSI引脚的脉冲都是对的,但是就是不呢个得到芯片ID信息,请大神们指点指点。