This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SCI中断接收数据,查询发送,单步调试,当DSP接收完数据后,转为发送,这个过程中会显示有了3次中断,并且Rx引脚电压为1.18V。多次测试,现象一样,都是在转换过程中多了3次中断,不知道这是由于干扰造成还是由于其他原因造成。通信中用了一个隔离芯片ADM2587,其中有个类似片选的信号,低电平为接收,高电平为发送。Tx和Rx均有下拉电阻。
PS:程序下载完成后测量Tx和Rx引脚,电压为1.18V,单步运行程序,SCI和引脚的初始化完成后Tx引脚为3.3V,Rx引脚没变,还是为1.18V,28335上的SCIA,SCIB,SCIC情况都是一样,不知道这是否属于正常情况。1.18V的状态是否为高阻状态?
楼主你好!
上电时,TX和TX都默认配置为输入高阻态状态,其电平取决于外面的输入信号,看起来应该你的电路像有点问题,没有输入的情况下应该RX管脚应该是高电平即3.3V左右。ADM2587接RX是什么结构,如果是开漏极的话,楼主可以接一个上拉电阻试一下。
谢谢Johnson Chen1的解答!把ADM2587和DSP的连接断开,任然是之前的情况,应该是电路设计的问题。再追问一个问题,28335的复位引脚XRS一般加多大的上拉电阻?
Johnson Chen1你好,再请教一个问题啊,28335 BOOT控制引脚XA12-XA15是不是必须得给定确定的状态?我的原理图中XA12和XA13是悬空的,XA14,XA15是拉低的,谢谢~