This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335SCI问题



SCI中断接收数据,查询发送,单步调试,当DSP接收完数据后,转为发送,这个过程中会显示有了3次中断,并且Rx引脚电压为1.18V。多次测试,现象一样,都是在转换过程中多了3次中断,不知道这是由于干扰造成还是由于其他原因造成。通信中用了一个隔离芯片ADM2587,其中有个类似片选的信号,低电平为接收,高电平为发送。Tx和Rx均有下拉电阻。

PS:程序下载完成后测量Tx和Rx引脚,电压为1.18V,单步运行程序,SCI和引脚的初始化完成后Tx引脚为3.3V,Rx引脚没变,还是为1.18V,28335上的SCIA,SCIB,SCIC情况都是一样,不知道这是否属于正常情况。1.18V的状态是否为高阻状态?