This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335的GPIO引脚作为输入



各位午安,我最近在用28335外接一个模块来读取其测量结果,用的是普通GPIO模式与其通信;这个模块之前我在STM32上调通了,可在28335上就怎么也读不回来数据,二者都是用杜邦线连接的。

我对比了源码,发现读寄存器函数有区别,具体如下:

28335:

……

if(GpioDataRegs.GPADAT.bit.GPIO10==1)

{

    dat |= 0x0001;

}

else

{

    dat &= 0xFFFE;

}

……

GPIO配置如下:

EALLOW;

……

GpioCtrlRegs.GPAMUX1.bit.GPIO10 = 0;

GpioCtrlRegs.GPADIR.bit.GPIO10 = 0;

……

EDIS;

STM32读寄存器代码如下:

if(GPIO_ReadInputDataBit(GPIOD, GPIO_Pin_4))
dat |= 0x01;
else
dat &= 0xFE;

另附GPIO_ReadInputDataBit的源代码:

uint8_t GPIO_ReadInputDataBit(GPIO_TypeDef* GPIOx, uint16_t GPIO_Pin)
{
uint8_t bitstatus = 0x00;

/* Check the parameters */
assert_param(IS_GPIO_ALL_PERIPH(GPIOx));
assert_param(IS_GET_GPIO_PIN(GPIO_Pin));

if ((GPIOx->IDR & GPIO_Pin) != (uint32_t)Bit_RESET)
{
bitstatus = (uint8_t)Bit_SET;
}
else
{
bitstatus = (uint8_t)Bit_RESET;
}
return bitstatus;
}

我想问的是CCS有没有这类读取输入引脚的库函数?我好直接调用。我用的版本是CCSv4.12。