使用外置XDS110调试器没问题,板载XDS110提示一下错误
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
根据文档
第10页描述:
2.2.2 XDS110 Output
The connector J102 is provided to debug an external target with the on-board XDS110 debug probe. This connector allows the LaunchPad to be used as a stand-alone XDS110 debug probe. If the LaunchPad is being used in this manner, ensure that all of the shunts are removed from J101. This isolates the JTAG signals from going to the F280049C MCU.
你是否按照上述的内容操作了呢?
如果仍有问题,可以参考以下网页进行排除:
software-dl.ti.com/.../ccsv7_debugging_jtag_connectivity_issues.html