This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用2837x 的ADC 关于参考电压VREHI的供电



请教一个关于2837x系列的ADC的参考电压的供电问题

资料上是这样说的

基本就是说每个ADC模块都用一个放大器来供电,也可以两个共用一个放大器,但是要满足手册上的要求。

我的问题:

1,共用放大器时的要求是什么?从data manual中没太看明白

2,如果ADC A,B,C,D四个模块共用一个放大器供电,会有什么影响?

谢谢!

  • 图片没粘贴上,补发一下;
    Figure 10-22 shows the basic organization of the external voltage reference generation circuitry. A single
    reference voltage generation should be shared by all ADC modules. This will minimize reference voltage
    mismatch between ADC modules. The reference voltage should then be buffered by a precision op-amp
    with good bandwidth and low output impedance before being driven into the reference pin. A capacitor
    between the high and low reference pins should be placed on the PCB as close to the pins as practical to
    help absorb high frequency currents. A series resistor (typically <1Ω ) in series with this capacitor may be
    necessary to ensure op-amp
    It is also possible to share two reference pins between one op-amp driver. This organization is shown in
    Figure 10-24. This will give slightly reduced performance compared to the case where each reference pin
    has a dedicated op-amp buffer, but it should still be possible to achieve all ADC specifications in the data
    manual..
  • 为更加有效地解决您的问题,我们建议您将问题发布在E2E英文技术论坛上“http://e2e.ti.com/support/microcontrollers/c2000/f/171”,将由资深的工程师为您提供帮助。我们的E2E英文社区有TI专家进行回复,并得到全球各地工程师的支持,分享他们的知识和经验。