今天测试了,和在RAM中一样能跑到150M。是否正确?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
是如何测试的?
CPU跑150MHz是没有问题的,但是,M35的Flash是采用F021工艺的,最高速度可达40MHz,但是由于两级128bit的预取指的存在,在100MHz的时候,效率可到达92%。要插入几个等待时间的。Flash速度没有那么快。
C28 frequency |
Wait state |
Efficiency |
Effective speed |
40 MHz |
0 |
100 % |
40 MHz |
80 MHz |
1 |
96 % |
77 MHz |
100 MHz |
2 |
94 % |
94 MHz |
150 MHz |
3 |
91 % |
137 MHz |