This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
C28 frequency |
Wait state |
Efficiency |
Effective speed |
40 MHz |
0 |
100 % |
40 MHz |
80 MHz |
1 |
96 % |
77 MHz |
100 MHz |
2 |
94 % |
94 MHz |
150 MHz |
3 |
91 % |
137 MHz |