This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377S的FLASH烧写问题



您好!

我使用的是28377S,仿真器是XDS100V2,在FLASH烧写的时候出现以下error:(3.3V和1.2V供电都测试过没问题,但是XRS脚的电压是3.18V,这是不是说明供电功率不够呢,还是我的DSP锁住了?)

C28xx_CPU1: Error: (Error -1135 @ 0xC0CC) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 6.0.407.3)

C28xx_CPU1: Trouble Halting Target CPU: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 6.0.407.3)

C28xx_CPU1: Error: (Error -1135 @ 0xC0CC) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 6.0.407.3)

C28xx_CPU1: Unable to determine target status after 20 attempts

C28xx_CPU1: Failed to remove the debug state from the target before disconnecting.  There may still be breakpoint op-codes embedded in program memory.  It is recommended that you reset the emulator before you connect and reload your program before you continue debugging

C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not read 0x00130@Program: target is not connected

C28xx_CPU1: Error writing the PLL values. (Flash algorithm returned error code). Operation cancelled.

C28xx_CPU1: File Loader: Memory write failed: Unknown error

C28xx_CPU1: GEL: File: F:\space\28377xin\Debug\28377xin.out: Load failed.

C28xx_CPU1: Error occurred during flash operation: Could not read register PC: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F800@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005FC00@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected

C28xx_CPU1: Error occurred during flash operation: Cannot enable while the target is disconnected

C28xx_CPU1: Error occurred during flash operation: Could not read 0x00000064@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Failed to run target while trying to execute pwrite_en.alg

C28xx_CPU1: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.

C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D22E@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D208@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D208@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D208@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D208@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D222@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D222@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D214@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D222@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected

C28xx_CPU1: Error occurred during flash operation: Cannot enable while the target is disconnected

C28xx_CPU1: Error occurred during flash operation: Could not read 0x00000064@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Failed to run target while trying to execute pwrite_dis.alg

C28xx_CPU1: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.

C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected

C28xx_CPU1: Error occurred during flash operation: Could not write register PC: target is not connected