This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS4.1.2 for C2000 MCU编程遇到的问题



您好,

        因工作需要,我是刚刚接触DSP C2000编程方面,但是用了CCS编译代码时,总是建工程不能编译成功,我用了DSP281x    V120版本的库函数,但是我自己建立工程的workspace是在D盘的一个专用文件夹,我把库函数里面的include文件个source文件都是直接复制到我建立的工程文件夹下面,但是每次编译都提示ERROR,还有特别的想请教一下各位高手我如何在工程里选择添加CMD和GEL文件,因为我看见库函数里面有好几个这样的文件,不甚感激!

Severity and Description Path Resource Location Creation Time Id

could not open source file "DSP281x_Device.h" new DSP281x_Adc.c line 14 1357049647953 883

"../Example_281xGpioLoopback.c", line 78: fatal error: could not open source file "DSP281x_Device.h"
1 fatal error detected in the compilation of "../Example_281xGpioLoopback.c".
Compilation terminated.

上面是出错的信息!

  • 出现楼主的报错信息是因为没有找到相关文件,楼主请在工程配置里设置正确的include目录;

    建议楼主在TI官网下载你要开发的芯片的例程,例程都包括了必要的文件和设置,楼主可以在例程基础上开发自己的项目。

  • 您好,麻烦在请教一下,我是用的TI官网的例子,而且把它里面的.h和 .c文件都复制到我自己的工程下面来了,包括报错的“DSP281x_Device.h"这个文件也是在我的工程里面,您说的配置正确的include目录,请问是如何来配置,我用的是CCS4.1.2版本,希望能得到您更为详细的解释,手头这个项目弄的很急,非常谢谢!

  • 在CCS的菜单中选择Project->Properties,弹出的设置窗口中选择Build->Include Options,添加正确的路径到Add dir to # include search path