您好,
因工作需要,我是刚刚接触DSP C2000编程方面,但是用了CCS编译代码时,总是建工程不能编译成功,我用了DSP281x V120版本的库函数,但是我自己建立工程的workspace是在D盘的一个专用文件夹,我把库函数里面的include文件个source文件都是直接复制到我建立的工程文件夹下面,但是每次编译都提示ERROR,还有特别的想请教一下各位高手我如何在工程里选择添加CMD和GEL文件,因为我看见库函数里面有好几个这样的文件,不甚感激!
Severity and Description Path Resource Location Creation Time Id
could not open source file "DSP281x_Device.h" new DSP281x_Adc.c line 14 1357049647953 883
"../Example_281xGpioLoopback.c", line 78: fatal error: could not open source file "DSP281x_Device.h"
1 fatal error detected in the compilation of "../Example_281xGpioLoopback.c".
Compilation terminated.
上面是出错的信息!