TI 工程师你好,有个问题:BOOT设置默认引脚(GPIO72和GPIO84)硬件设计时给占用了,那么在芯片未编程情况下如何进入get boot mode 模式?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI 工程师你好,有个问题:BOOT设置默认引脚(GPIO72和GPIO84)硬件设计时给占用了,那么在芯片未编程情况下如何进入get boot mode 模式?
您好,请帮我纠正下我的理解是否有误:当默认引脚被占用,在单机运行且芯片第一次使用时则不能满足boot to flash条件,解决方法是链接仿真器,创建工程,通过修改文件DCSM_Z2_ZoneSelectBlock.asm中bootctr寄存器的值(根据我的理解是不是只需要对模式设置相关位进行设置,引脚就不用了吧)可以实现boot to flash,以后再单机运行时就没问题了。
1、当默认引脚被占用,而且在上电瞬间无法改变引脚上下拉状态的情况下,只能先通过连接仿真器将包含修改过的.asm文件(具体如何修改请参考 10# 的回复,本人没有操作过,不是很清楚)的工程烧写进DSP从而更改默认boot引脚。
2、当默认引脚被占用,但在上电瞬间可以通过弱上下拉的方式更改GPIO引脚状态的。那么在确保上电瞬间的引脚上下拉状态后,可以跟普通芯片一样使用。