This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电机300rpm时扭矩输出偏弱

Other Parts Discussed in Thread: DRV8301, MOTORWARE

TI的评估板:DRV8301-HC-EVM Rev D。

选用sw\solutions\instaspin_foc\boards\drv8301kit_revD\f28x\f2806xF\projects\ccs5\proj_lab10a例程。

电机300rpm时扭矩输出偏弱指:我用扭力计测试我们的产品在300rpm可以让电机输出50N.cm,德国有一款和我们一样的产品,我用扭力计测试在300rpm同样是让电机输出50N.cm,但是用户在实际使用的过程中明细觉得我们的产品扭矩偏小10N.cm左右,用户感觉我们的产品60N.cm和德国产品的50N.cm一样大。(用户实际使用过程中的负载突变比用扭力计测试的负载突变大)

请TI的工程师给出电机300rpm时扭矩输出偏弱、偏软的解决方案,非感谢!德国的那款产品给我的感觉就是扭矩输出很稳定、很足。

电机参数如下

Nominal voltage V                  24
No load speed rpm                60800
No load current mA               282 
Nominal speed rpm               57500
Nominal torque (max. continuous torque) mNm           23.6
Nominal current (max. continuous current) A               6.45
Stall torque mNm                  561
Stall current A                      149
Max. efciency %                   91.6
Terminal resistance W         0.161
Terminal inductance mH     0.0171
Torque constant mNm/A     3.76
Speed constant rpm/V        2540
Speed/torque gradient rpm/mNm      109
Mechanical time constant ms            2.04
Rotor inertia gcm                               1.79

 

  • 你好,你的意思是DRV8301-HC-EVM在正常测试的时候扭矩能打到50H.cm。但当负载发生突变(大)的时候,这款套件的稳定性会不足,实际输出会小于50N.cm的扭矩?
    负载突变的时候有测试过对应状态的扭矩吗?
  • 不管负载是否突变,实际测试都是50N.cm,但是用户感觉输出只有40N.cm,德国的产品实际测试是50N.cm,用户感觉也是50N.cm,请给出解决方案,非常感谢!
  • 抱歉,由于DRV8301 EVM是专为评估而设计的,并不是为了最佳性能,所以体验上会有差距。而且,对于全扭矩输出,无传感器控制而言,300RPM也是一个有挑战的速度范围,为了优化低速运行,PCB板也必须进行优化。特别是对电流、电压等反馈信号的分辨率进行优化,使其在低速下具有更好的性能。
    但TI的另一款产品:F280049C中的rom代码由定点编码改为浮点编码,在低速下具有更高的性能。所以以我的经验,它的低速性能应该优于F28069F。
    但是很遗憾,用于F280049C的SDK:MotorSDK (v1.0)不包含DRV8301 EVM。但如果你熟悉MotorWare和InstaSPIN-FOC解决方案的话,我建议你可以自己为DRV8301构建一些类似HAL的代码。