This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC Interrupt Select 1 And 2 Register

 Interrupt Select 1 And 2 Register (INTSEL1N2) (Address Offset 08h) 是什么意思?选择ADC中断源吗?

  • 另外参考例程内的定义

    struct INTSEL1N2_BITS {     // bits description
    	Uint16	INT1SEL:5;			// 4:0	INT1 EOC Source Select
    	Uint16	INT1E:1;			// 5	INT1 Interrupt Enable
    	Uint16	INT1CONT:1;			// 6	INT1 Continuous Mode Enable
    	Uint16	rsvd1:1;			// 7	Reserved
    	Uint16	INT2SEL:5;			// 12:8	INT2 EOC Source Select
    	Uint16	INT2E:1;			// 13	INT2 Interrupt Enable
    	Uint16	INT2CONT:1;			// 14	INT2 Continuous Mode Enable
    	Uint16	rsvd2:1;			// 15	Reserved
    };

x 出现错误。请重试或与管理员联系。