This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dsp2808 ecap1~ecap4值相同



我使用了DSP自己的PWM端口进行输出,,捕获后值是对的,但接入其他方波信号,出现捕获的ECAP1~ECAP4值一样,用示波器观察,信号质量还可以,怎么回事

  • 你好。请问你使用的是哪种模式,Absolute Stamp Mode还是Delta Mode?两个CAP事件是上升沿触发还是下降沿触发?

  • ECAP1 上升触发,ECAP2 下降触发,ECAP3 上升触发,,ECAP4 下降触发\在event4设置中断,读取数据.  ECap2Regs.ECEINT.all = 0x0000;             // Disable all capture interrupts
       ECap2Regs.ECCLR.all = 0xFFFF;              // Clear all CAP interrupt flags
       ECap2Regs.ECCTL1.bit.CAPLDEN = 0;          // Disable CAP1-CAP4 register loads
       ECap2Regs.ECCTL2.bit.TSCTRSTOP = 0;        // Make sure the counter is stopped
     // EC_ABS_MODE;
     //  Configure peripheral registers
       ECap2Regs.ECCTL2.bit.CONT_ONESHT = 0;      // continue
       ECap2Regs.ECCTL2.bit.STOP_WRAP = 3;        // Wrap after Capture Event 4 .
       ECap2Regs.ECCTL1.bit.CAP1POL = EC_RISING;          // Rising edge
       ECap2Regs.ECCTL1.bit.CAP2POL = EC_FALLING;          // Falling edge
       ECap2Regs.ECCTL1.bit.CAP3POL = EC_RISING;          // Rising edge
       ECap2Regs.ECCTL1.bit.CAP4POL = EC_FALLING;          // Falling edge
       ECap2Regs.ECCTL1.bit.CTRRST1 = EC_ABS_MODE;          // absolute time stamp    
       ECap2Regs.ECCTL1.bit.CTRRST2 = EC_ABS_MODE;          // Difference operation        
       ECap2Regs.ECCTL1.bit.CTRRST3 = EC_ABS_MODE;          // Difference operation        
       ECap2Regs.ECCTL1.bit.CTRRST4 = EC_DELTA_MODE;          // Difference operation        
       ECap2Regs.ECCTL2.bit.SYNCI_EN = 0;         // Enable sync in
       ECap2Regs.ECCTL2.bit.SYNCO_SEL = 1;        // disable sync signal out
       ECap2Regs.ECCTL1.bit.CAPLDEN = 1;          // Enable capture units
       ECap1Regs.ECCTL2.bit.CAP_APWM = EC_CAP_MODE;
    //   ECap1Regs.ECCTL2.bit.TSCTRSTOP = 1;        // Start Counter
    //   ECap1Regs.ECCTL2.bit.REARM = 1;            // Rearm one-Shot
    //   ECap1Regs.ECCTL1.bit.CAPLDEN = 1;          // Enable CAP1-CAP4 register loads
       ECap2Regs.ECEINT.bit.CEVT4  = 1;             // 2 events = interrupt

     

  • 你好。根据你设置,只有CAP4是Delta模式,也就是说Counter在CEVT4后会复位,其他三个事件后是不复位的。

    假设,输入的PWM周期为T,且不发生变化,占空比为D,那么,4个CAP寄存器的值应为:

    CAP1=(1-D)*T*SYSCLK  // 低电平时间

    CAP2=T*SYSCLK

    CAP3=(2-D)*T*SYSCLK

    CAP4=2*T*SYSCLK

    由于每次CEVT4后,Counter都会复位,所以四个CAP寄存器的数值总是不变的。

    请问你的测试结果是否如此?