This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于instaSPIN的FAST观测器,在特殊类型的电机(内阻极大)中运行失效的问题



你好;

       最近我们基于instaSPIN的FAST算法,开发了一款无人机的动力电调(48V、24V系列30A~60A级别),运行一切正常,包括参数辨识、电机运行等等功能。

      现在是想将这个方案来运行其他的小电机(<12V,1A级别),就是下面这类电机,这类电机的电阻远(>2欧姆)大于正常的动力电机(<=0.1欧姆)。目前遇到的问题就是,按照例程中的调试方法,怎么都无法正常启动这个电机(包括直接使用厂家给定的电气参数,也无法启动);使用参数辨识功能,也无法执行,电机内阻可测,但下一步过渡到磁链、电感测试就电机不转。调试细查,整个算法输出的角度和转速,就不像正常运行时那样,快速收敛到真实状态。

     因此,现在问题是,TI的FAST无感算法,对这类定子内阻极大的电机,是否从原理上就无法准确辨识转子角度(算法不收敛),还是我控制参数设置不合理导致的?

电机

电机1

电机2

极对数

7

4

定子内阻:欧姆

2.7

2.8

定子电感:mH

1.3

0.85

转子磁链

未知

未知

额定电压:V

12

12