This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

调用单相SOGI锁相环锁相不精确的问题

您好,

我选择用的是SPLL_1ph_SOGI_IQ_H_,环路滤波器的PI参数按照TI太阳能库里给的excel文件计算得。

原SPLL_1ph_SOGI_IQ.h文件是IQ23格式,我改成了IQ18格式。这个是可以更改的吧。锁相有时候会锁住,有时在同样工况下就明显观察到角度差变大。

而且在取得相角的基础上,经过sin后乘以一个电流基准值,可从放大的波形中发现电网电压,相角,相角正弦值*电流,三者均不在同一相位上。请问这是什么问题?

程序和波形见下方。

 这是正常的时候

  同样工况下有时候就明显观察到相角差变大

1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
#include "DSP281x_Device.h"
#include "DSP281x_Examples.h"
#include "Solar_IQ.h"
#include <math.h>
#define PI 3.1415926
#define Ts 0.00005
#define GRID_FREQ 50
#define N 400
// Variable defs
long ia1,ia,i1,ig,ig_ref;
long us1,us2,us,factor_us[2]={0,0},us_0,uss,uss0;
SPLL_1ph_SOGI_IQ spll1;
long id1[3]={0,0,0},ed1[3]={0,0,0}; // Current Loop output and error
float kc1=4.000246740102,kc3=1.999753275118,kp=0.002,kr=10; // Current loop PR
int i=0;
long g1,g2,g3,M;
float ig_r=1;
ioport unsigned int port00;
ioport unsigned int port01;
ioport unsigned int port02;
ioport unsigned int port03;
interrupt void T1_Compare_isr(void);
void AD_Sampling(void);
void Current_Loop(void);
void SPWM(void);
void DA_Viewer(void);
void main(void)
{
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP281x_SysCtrl.c file.
InitSysCtrl();
// Step 2. Initalize GPIO:
// This example function is found in the DSP281x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
InitGpio();
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;
// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP281x_PieCtrl.c file.
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER=0x0000;
IFR=0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in DSP281x_DefaultIsr.c.
// This function is found in DSP281x_PieVect.c.
InitPieVectTable();
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

十分感谢您的回答。