This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP2812 程序copy问题请教



   我的程序在flash里运行正常,我将部分程序copy到H0SARAM里后只要运行到H0SARAM里的程序就会进入非法中断(中断如下所示),但如果把同样的程序copy到L0SARAMA就没有这问题可以顺利运行。H0里不能移植程序么?请教高手帮忙解答一下,谢谢!

interrupt void ILLEGAL_ISR(void) // Illegal operation TRAP
{
// Insert ISR Code here

// Next two lines for debug only to halt the processor here
// Remove after inserting ISR Code
asm(" ESTOP0");
for(;;);

}

  • 麻烦把函数复制的那一段程序发过来看一下。
  • 相关的帖子 可以参考一下 看着他也没解决
    e2echina.ti.com/.../536475
  • 这是复制函数:
    KickDog();

    // Initialize the PLLCR to 0xA
    InitPll(0xA);

    /* Copy the secureRamFuncs section */
    memcpy(&FLASH_SET_FUNCS_runstart, &FLASH_SET_FUNCS_loadstart,
    &FLASH_SET_FUNCS_loadend - &FLASH_SET_FUNCS_loadstart);
    /* Initialize the on-chip flash registers */

    InitFlash();
    // Initialize the peripheral clocks
    InitPeripheralClocks();

    这是CMD
    PRAMH0 : origin = 0x3F8000, length = 0x002000 /*used as program segment*/

    FLASH_SET_FUNCS : LOAD = FLASHCD, PAGE = 0
    RUN =PRAMH0 , PAGE = 0

    RUN_START(_FLASH_SET_FUNCS_runstart),
    LOAD_START(_FLASH_SET_FUNCS_loadstart),
    LOAD_END(_FLASH_SET_FUNCS_loadend)

    请帮忙谢谢!
  • 我认为你的memcpy()函数的参数出了问题,可能导致了这个问题。见下面,应该是加载开始,然后加载结束,然后运行开始:
    你的:
    /* Copy the secureRamFuncs section */

    memcpy(&FLASH_SET_FUNCS_runstart, &FLASH_SET_FUNCS_loadstart,

    &FLASH_SET_FUNCS_loadend - &FLASH_SET_FUNCS_loadstart);

    改为:
    // Copy time critical code and Flash setup code to RAM
    // The RamfuncsLoadStart, RamfuncsLoadEnd, and RamfuncsRunStart
    // symbols are created by the linker. Refer to the F2812.cmd file.
    MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);

    更改后测试一下,如果还是有问题的话麻烦将进入非法中断的函数告知给我一下。
  • 您好,感谢帮忙,我按您说的配置memcpy()这个函数参数顺序也还会进入非法中断。我目前这个配置方式是按照《Copying Compiler Sections From Flash to RAM on the TMS320F28xxx DSCs》这个文档上说明进行的,同时相同的程序如果COPY到其他RAM中运行就不会出现问题,如果COPY到PRAMH0 就会运行到其程序就进入非法中断。请指导,谢谢!
  • 你好,你还需要什么信息我可以提供过去,麻烦帮我看看。
  • 你好,相关问题我这边已经咨询了美国工程师,有回复了尽快给你答案
  • 工程师回复:是否存在导致非法ISR的特定函数或代码行?在调试代码(单步执行或设置断点)时,你能将执行后跳转到ISR的函数或代码行定位吗?
    是否在代码中使用了pragma来配置从RAM运行的函数,如下所示?

    // Functions that will be run from RAM need to be assigned to
    // a different section. This section will then be mapped using
    // the linker cmd file.
    #pragma CODE_SECTION(eva_timer1_isr, "ramfuncs");
    #pragma CODE_SECTION(eva_timer2_isr, "ramfuncs");
    #pragma CODE_SECTION(evb_timer3_isr, "ramfuncs");

    此外,你还可以按以下页面的步骤进一步调试ITRAP:
    processors.wiki.ti.com/.../Interrupt_FAQ_for_C2000
  • 您好,附件中是我程序的CMD文件如下,

    /*==================================================================
    注:在flash烧写之前,应将程序载入ram(load program)后,检查CsmRegs
    (0x000AE0)的八个寄存器的内容,其对应于dsp芯片安全密码,该值不能全
    部为0x0000,当密码不设置时,该值全部为0xFFFF。当任何一个内部flash段
    被烧写时,CsmRegs中内容将被同时烧写。
    ==================================================================*/

    MEMORY
    {
    PAGE 0 :
      
     RAML0    : origin = 0x008000, length = 0x001800
        EXTRAM0  : origin = 0x100000, length = 0x004000  
        OTP         : origin = 0x3D7800, length = 0x000800
        FLASHJ      : origin = 0x3D8000, length = 0x002000
     FLASHI      : origin = 0x3DA000, length = 0x002000
        FLASHH      : origin = 0x3DC000, length = 0x004000
        FLASHG      : origin = 0x3E0000, length = 0x004000
    /*   FLASHF      : origin = 0x3E4000, length = 0x004000*/
    /*   FLASHE      : origin = 0x3E8000, length = 0x004000*/
     FLASHEF     : origin = 0x3E4000, length = 0x008000
    /*    FLASHD      : origin = 0x3EC000, length = 0x004000 */
        FLASHCD     : origin = 0x3EC000, length = 0x008000
        FLASHB      : origin = 0x3F4000, length = 0x002000
        FLASHA      : origin = 0x3F6000, length = 0x001F80
       CSM_RSVD    : origin = 0x3F7F80, length = 0x000076    /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */  
        BEGIN       : origin = 0x3F7FF6, length = 0x000002
        PASSWDS     : origin = 0x3F7FF8, length = 0x000008

        PRAMH0      : origin = 0x3F8000, length = 0x002000  /*used as program segment*/
        ROM         : origin = 0x3FF000, length = 0x000FC0
       RESET       : origin = 0x3FFFC0, length = 0x000002          
        VECTORS     : origin = 0x3FFFC2, length = 0x00003E
            
    PAGE 1 :
       /* SARAM                     */    
     RAMM0    : origin = 0x000040, length = 0x0003c0
       RAMM1     : origin = 0x000400, length = 0x000400
       RAML1    : origin = 0x009800, length = 0x000800
     EXTRAM1  : origin = 0x104000, length = 0x01c000
       
       /*-------------------------------------------------------------*/
       DEV_EMU     : origin = 0x000880, length = 0x000180     /* device emulation registers */
       PIE_VECT    : origin = 0x000D00, length = 0x000100     /* PIE Vector Table */
       FLASH_REGS  : origin = 0x000A80, length = 0x000060     /* FLASH registers */
       CSM         : origin = 0x000AE0, length = 0x000010     /* code security module registers */
       XINTF       : origin = 0x000B20, length = 0x000020     /* external interface registers */
       CPU_TIMER0  : origin = 0x000C00, length = 0x000008     /* CPU Timer0 registers (CPU Timer1 and Timer2 are reserved for BIOS)*/
       CPU_TIMER1  : origin = 0x000C08, length = 0x000008  
       CPU_TIMER2  : origin = 0x000C10, length = 0x000008  
       PIE_CTRL    : origin = 0x000CE0, length = 0x000020     /* PIE control registers */
       ECANA       : origin = 0x006000, length = 0x000040     /* eCAN control and status registers */
       ECANA_LAM   : origin = 0x006040, length = 0x000040     /* eCAN local acceptance masks */
       ECANA_MOTS  : origin = 0x006080, length = 0x000040     /* eCAN message object time stamps */
       ECANA_MOTO  : origin = 0x0060C0, length = 0x000040     /* eCAN object time-out registers */
       ECANA_MBOX  : origin = 0x006100, length = 0x000100     /* eCAN mailboxes */
       SYSTEM      : origin = 0x007010, length = 0x000020     /* System control registers */
       SPIA        : origin = 0x007040, length = 0x000010     /* SPI registers */
       SCIA        : origin = 0x007050, length = 0x000010     /* SCI-A registers */
       XINTRUPT    : origin = 0x007070, length = 0x000010     /* external interrupt registers */
       GPIOMUX     : origin = 0x0070C0, length = 0x000020     /* GPIO mux registers */
       GPIODAT     : origin = 0x0070E0, length = 0x000020     /* GPIO data registers */
       ADC         : origin = 0x007100, length = 0x000020     /* ADC registers */
       EVA         : origin = 0x007400, length = 0x000040     /* Event Manager A registers */
       EVB         : origin = 0x007500, length = 0x000040     /* Event Manager B registers */
       SCIB        : origin = 0x007750, length = 0x000010     /* SCI-B registers */
       MCBSPA      : origin = 0x007800, length = 0x000040     /* McBSP registers */
       CSM_PWL     : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations. */
     /*--------------------------------------------------------------*/
    }
     

    SECTIONS
    {
     PieVectTableFile : > PIE_VECT,   PAGE = 1

     /*** Peripheral Frame 0 Register Structures ***/
     DevEmuRegsFile    : > DEV_EMU,     PAGE = 1
     FlashRegsFile     : > FLASH_REGS,  PAGE = 1
     CsmRegsFile       : > CSM,         PAGE = 1
     XintfRegsFile     : > XINTF,       PAGE = 1
     CpuTimer0RegsFile : > CPU_TIMER0,  PAGE = 1
     CpuTimer1RegsFile : > CPU_TIMER1,  PAGE = 1     
     CpuTimer2RegsFile : > CPU_TIMER2,  PAGE = 1       
     PieCtrlRegsFile   : > PIE_CTRL,    PAGE = 1     

     /*** Peripheral Frame 1 Register Structures ***/
     SysCtrlRegsFile   : > SYSTEM,      PAGE = 1
     SpiaRegsFile      : > SPIA,        PAGE = 1
     SciaRegsFile      : > SCIA,        PAGE = 1
     XIntruptRegsFile  : > XINTRUPT,    PAGE = 1
     GpioMuxRegsFile   : > GPIOMUX,     PAGE = 1
     GpioDataRegsFile  : > GPIODAT      PAGE = 1
     AdcRegsFile       : > ADC,         PAGE = 1
     EvaRegsFile       : > EVA,         PAGE = 1
     EvbRegsFile       : > EVB,         PAGE = 1
     ScibRegsFile      : > SCIB,        PAGE = 1
     McbspaRegsFile    : > MCBSPA,      PAGE = 1

     /*** Peripheral Frame 2 Register Structures ***/
     ECanaRegsFile     : > ECANA,       PAGE = 1
     ECanaLAMRegsFile  : > ECANA_LAM    PAGE = 1  
     ECanaMboxesFile   : > ECANA_MBOX   PAGE = 1
     ECanaMOTSRegsFile : > ECANA_MOTS   PAGE = 1
     ECanaMOTORegsFile : > ECANA_MOTO   PAGE = 1
     
     /*** Code Security Module Register Structures ***/
     CsmPwlFile        : > CSM_PWL,     PAGE = 1


        codestart         : > BEGIN,        PAGE = 0
       .text             : > FLASHCD,       PAGE = 0
       .cinit            : > FLASHCD,       PAGE = 0
       .pinit            : > FLASHCD,       PAGE = 0
     .switch    : > FLASHCD,       PAGE = 0
       .reset            : > RESET,       PAGE = 0,TYPE = DSECT
       .stack            : > RAMM1,        PAGE = 1
       .ebss             : > RAML1,       PAGE = 1
       .bss             : > RAML1,       PAGE = 1
       .econst           : > FLASHEF,      PAGE = 0
       .esysmem          : > RAML1,       PAGE = 1

        FLASH_SET_FUNCS  : LOAD = FLASHCD, PAGE = 0
            RUN = PRAMH0,    PAGE = 0

            RUN_START(_FLASH_SET_FUNCS_runstart),
            LOAD_START(_FLASH_SET_FUNCS_loadstart),
            LOAD_END(_FLASH_SET_FUNCS_loadend)
       ramfuncs             : LOAD = FLASHCD, PAGE = 0
                           RUN = PRAMH0, PAGE = 0

                             LOAD_START(_RamfuncsLoadStart),
                             LOAD_END(_RamfuncsLoadEnd),
                             RUN_START(_RamfuncsRunStart)


     MONISECT0   : > EXTRAM1,    PAGE = 1
     MONISECT1   : > EXTRAM1,    PAGE = 1
     MONISECT2   : > EXTRAM1,    PAGE = 1
     MONISECT3   : > EXTRAM1,    PAGE = 1
     MONISECT4   : > EXTRAM1,    PAGE = 1
     MONISECT5   : > EXTRAM1,    PAGE = 1
     MONISECT6   : > EXTRAM1,    PAGE = 1
     MONISECT7   : > EXTRAM1,    PAGE = 1
     MONISECT8   : > EXTRAM1,    PAGE = 1
     MONISECT9   : > EXTRAM1,    PAGE = 1
     MONISECT10   : > EXTRAM1,    PAGE = 1
     MONISECT11   : > EXTRAM1,    PAGE = 1
     MONISECT12   : > EXTRAM1,    PAGE = 1
     MONISECT13   : > EXTRAM1,    PAGE = 1
     MONISECT14   : > EXTRAM1,    PAGE = 1
     MONISECT15   : > EXTRAM1,    PAGE = 1
     MONISECT16   : > EXTRAM1,    PAGE = 1
     MONISECT17   : > EXTRAM1,    PAGE = 1
     MONISECT18   : > EXTRAM1,    PAGE = 1
     MONISECT19   : > EXTRAM1,    PAGE = 1
     MONISECT20   : > EXTRAM1,    PAGE = 1
     MONISECT21   : > EXTRAM1,    PAGE = 1
     MONISECT22   : > EXTRAM1,    PAGE = 1
     MONISECT23   : > EXTRAM1,    PAGE = 1
     MONISECT24   : > EXTRAM1,    PAGE = 1
     MONISECT25   : > EXTRAM1,    PAGE = 1
     MONISECT26   : > EXTRAM1,    PAGE = 1
     MONISECT27   : > EXTRAM1,    PAGE = 1
     MONISECT28   : > EXTRAM1,    PAGE = 1
     MONISECT29   : > EXTRAM1,    PAGE = 1
     MONISECT30   : > EXTRAM1,    PAGE = 1
     MONISECT31   : > EXTRAM1,    PAGE = 1
     MONISECT32   : > EXTRAM1,    PAGE = 1
     MONISECT33   : > EXTRAM1,    PAGE = 1
     MONISECT34   : > EXTRAM1,    PAGE = 1
     MONISECT35   : > EXTRAM1,    PAGE = 1
     MONISECT36   : > EXTRAM1,    PAGE = 1
     MONISECT37   : > EXTRAM1,    PAGE = 1
     MONISECT38   : > EXTRAM1,    PAGE = 1
     MONISECT39   : > EXTRAM1,    PAGE = 1


    }

    只是将INIT_FLASH(void)COPY 到PRAMH0中,INIT_FLASH程序如下:EALLOW;

    FlashRegs.FPWR.bit.PWR=3;               //Flash运行于活跃模式

    FlashRegs.FSTATUS.bit.V3STAT=1;         //清除报警

    FlashRegs.FBANKWAIT.bit.RANDWAIT=5;     //随机存取时间

    FlashRegs.FBANKWAIT.bit.PAGEWAIT=5;     //页面存取时间

    //FlashRegs.FOTPWAIT.bit.OPTWAIT=5;       //OTP读等待时间

    FlashRegs.FOPT.bit.ENPIPE=1;            //启动管线模式以提高性能

    EDIS;

    asm(" RPT #7 || NOP ");

    当单步运行进入INIT_FLASH程序中的第二条或者第三条都可能跳入

    interrupt void ILLEGAL_ISR(void) // Illegal operation TRAP

    {

    // Insert ISR Code here

    // Next two lines for debug only to halt the processor here

    // Remove after inserting ISR Code

    asm(" ESTOP0");

    for(;;);

    }

    这个非法的中断中。

    但如果吧INIT_FLASH  copy到RAMM0中就不会出现进入非法中断的情况。

    谢谢!