This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2812DSP复位后无法继续运行

您好,

控制板采用如下的复位电路,当我按下复位按钮后,我可以通过示波器观察到XRS引脚的电平恢复了,而PWM驱动被拉低了,无法恢复。从CCS变量观察窗口可以看见PDPINTA的值由1变为0,可是硬件上并没有焊有关PDPINT的电路,程序中也没有使能这个中断,这是怎么一回事呢?

希望得到您的解答。

谢谢

  • 不确定问题的原因,但是可以考虑外部上拉处理一下
  • 我可以请教您一个其他的问题吗,就不重新开贴了。
    除了PDPINT之外那个引脚还能让2812实现PWM保护的功能呢,最好是将PWM驱动强制拉低。
  • 可以通过外部中断来控制PWM的应该只有PDPINT引脚了
  • 芯片复位后没有跑起来 出来芯片复位管脚的处理 看看复位是否会带来板上其他电路功能异常
    PDPINT硬件快速是PWM输出为高祖 如果全要低需要外部做下拉处理
  • 如果我想采用软件中断的方式,将EXTCONA寄存器INDCOE位设为1,将三路比较单元分开控制。当采样检测电流,当大于阈值时,我需要切断6路PWM信号中的4路。在中断程序中将EvaRegs.COMCONA.bit.FCMPxOE设为0(高阻态),但是当我实验时发现,PWM信号并不能关断,请问这是怎么回事呢?

    十分感谢您的耐心解答,程序我在后面附上。

    // �ز���ֵ���ƿ�������
    // This program is used for buck-boost inverter
    // Date: Sep 8th , 2019  Version: 1.2
    // Author: ZhangYuyao
    // Description��
    // �ɼ�ֱ�����е�����ͨ���ӳٵ��������ķ������˳�����Ƶ�ɷݡ��ڷ�����ͨ���ı��ز���ֵ��С��ɵ��ƣ�����ʵ���У���ı���Ʋ��ķ�ֵ��
    
    #include "DSP281x_Device.h"
    #include "DSP281x_Examples.h"
    #include "IQmathLib.h"
    #include <math.h>
    #define Ts 0.00005
    #define  N    400                 // 50*400=20000Hz  �ز���Ϊ400
    
    /*#pragma CODE_SECTION(T1_Compare_isr, "ramfuncs");  // ���жϺ���T1PINT_isrд��RAM�У���Ϊad_isr���������ã�����ʡ��ÿ�ζ���flash��д��RAM
                                      // ������Initflash()�ij�ʼ���ͱ�д����
    extern Uint16 RamfuncsLoadStart;  // ��Ϊ����memcpy�����ı���������MemCopy�����еı����������ȫ�ֱ�������
    extern Uint16 RamfuncsLoadEnd;
    extern Uint16 RamfuncsRunStart;*/
    
    // Variable defs
    int32 idc_s;                      // idc_s---ֱ������е�������
    int32 idc;
    int32 idc_Q = 0;
    int32 idc_Q1 = 0;                 // ����ʱ�ź�
    int32 idc_Q2 = 0;                 // ��ʱT/4�ź�
    int32 idc_avg1 = 0;               // the avg value after T/4 delay
    int32 idc_avg1_Q1 = 0;            // ����ʱ�ź�
    int32 idc_avg1_Q2 = 0;            // ��ʱT/8�ź�
    int32 idc_avg2 = 0;               // the avg value after all delay
    int32 buffer[400];
    float32 coefficient_k;            // ��ֵ����ϵ��
    int16 i = 0;
    int16 j = 0;
    int16 k = 301;
    int16 jj = 0;
    int16 kk = 351;
    int32 g1,g2,g3,P,G;
    float32 Modu_Index=0.4;            // Modulation index, ���Ʊ�
    
    // Sine table
    
    float32 sina[400]=
    {
    	0,0.0157,0.0314,0.0471,0.0628,0.0785,0.0941,0.1097,0.1253,0.1409,0.1564,0.1719,0.1874,0.2028,0.2181,0.2334,
        0.2487,0.2639,0.2790,0.2940,0.3090,0.3239,0.3387,0.3535,0.3681,0.3827,0.3971,0.4115,0.4258,0.4399,0.4540,
    	0.4679,0.4818,0.4955,0.5090,0.5225,0.5358,0.5490,0.5621,0.5750,0.5878,0.6004,0.6129,0.6252,0.6374,0.6494,
    	0.6613,0.6730,0.6845,0.6959,0.7071,0.7181,0.7290,0.7396,0.7501,0.7604,0.7705,0.7804,0.7902,0.7997,0.8090,
    	0.8181,0.8271,0.8358,0.8443,0.8526,0.8607,0.8686,0.8763,0.8838,0.8910,0.8980,0.9048,0.9114,0.9178,0.9239,
    	0.9298,0.9354,0.9409,0.9461,0.9511,0.9558,0.9603,0.9646,0.9686,0.9724,0.9759,0.9792,0.9823,0.9851,0.9877,
    	0.9900,0.9921,0.9940,0.9956,0.9969,0.9980,0.9989,0.9995,0.9999,1.0000,0.9999,0.9995,0.9989,0.9980,0.9969,
        0.9956,0.9940,0.9921,0.9900,0.9877,0.9851,0.9823,0.9792,0.9759,0.9724,0.9686,0.9646,0.9603,0.9558,0.9511,
    	0.9461,0.9409,0.9354,0.9298,0.9239,0.9178,0.9114,0.9048,0.8980,0.8910,0.8838,0.8763,0.8686,0.8607,0.8526,
    	0.8443,0.8358,0.8271,0.8181,0.8090,0.7997,0.7902,0.7804,0.7705,0.7604,0.7501,0.7396,0.7290,0.7181,0.7071,
    	0.6959,0.6845,0.6730,0.6613,0.6494,0.6374,0.6252,0.6129,0.6004,0.5878,0.5750,0.5621,0.5490,0.5358,0.5225,
    	0.5090,0.4955,0.4818,0.4679,0.4540,0.4399,0.4258,0.4115,0.3971,0.3827,0.3681,0.3535,0.3387,0.3239,0.3090,
    	0.2940,0.2790,0.2639,0.2487,0.2334,0.2181,0.2028,0.1874,0.1719,0.1564,0.1409,0.1253,0.1097,0.0941,0.0785,
        0.0628,0.0471,0.0314,0.0157,0,-0.0157,-0.0314,-0.0471,-0.0628,-0.0785,-0.0941,-0.1097,-0.1253,-0.1409,
    	-0.1564,-0.1719,-0.1874,-0.2028,-0.2181,-0.2334,-0.2487,-0.2639,-0.2790,-0.2940,-0.3090,-0.3239,-0.3387,
    	-0.3535,-0.3681,-0.3827,-0.3971,-0.4115,-0.4258,-0.4399,-0.4540,-0.4679,-0.4818,-0.4955,-0.5090,-0.5225,
    	-0.5358,-0.5490,-0.5621,-0.5750,-0.5878,-0.6004,-0.6129,-0.6252,-0.6374,-0.6494,-0.6613,-0.6730,-0.6845,
    	-0.6959,-0.7071,-0.7181,-0.7290,-0.7396,-0.7501,-0.7604,-0.7705,-0.7804,-0.7902,-0.7997,-0.8090,-0.8181,
    	-0.8271,-0.8358,-0.8443,-0.8526,-0.8607,-0.8686,-0.8763,-0.8838,-0.8910,-0.8980,-0.9048,-0.9114,-0.9178,
    	-0.9239,-0.9298,-0.9354,-0.9409,-0.9461,-0.9511,-0.9558,-0.9603,-0.9646,-0.9686,-0.9724,-0.9759,-0.9792,
        -0.9823,-0.9851,-0.9877,-0.9900,-0.9921,-0.9940,-0.9956,-0.9969,-0.9980,-0.9989,-0.9995,-0.9999,-1.0000,
    	-0.9999,-0.9995,-0.9989,-0.9980,-0.9969,-0.9956,-0.9940,-0.9921,-0.9900,-0.9877,-0.9851,-0.9823,-0.9792,
    	-0.9759,-0.9724,-0.9686,-0.9646,-0.9603,-0.9558,-0.9511,-0.9461,-0.9409,-0.9354,-0.9298,-0.9239,-0.9178,
    	-0.9114,-0.9048,-0.8980,-0.8910,-0.8838,-0.8763,-0.8686,-0.8607,-0.8526,-0.8443,-0.8358,-0.8271,-0.8181,
    	-0.8090,-0.7997,-0.7902,-0.7804,-0.7705,-0.7604,-0.7501,-0.7396,-0.7290,-0.7181,-0.7071,-0.6959,-0.6845,
    	-0.6730,-0.6613,-0.6494,-0.6374,-0.6252,-0.6129,-0.6004,-0.5878,-0.5750,-0.5621,-0.5490,-0.5358,-0.5225,
    	-0.5090,-0.4955,-0.4818,-0.4679,-0.4540,-0.4399,-0.4258,-0.4115,-0.3971,-0.3827,-0.3681,-0.3535,-0.3387,
    	-0.3239,-0.3090,-0.2940,-0.2790,-0.2639,-0.2487,-0.2334,-0.2181,-0.2028,-0.1874,-0.1719,-0.1564,-0.1409,
    	-0.1253,-0.1097,-0.0941,-0.0785,-0.0628,-0.0471,-0.0314,-0.0157
    };
    
    // ��������
    
    interrupt void T1_Compare_isr(void);
    void AD_Sampling(void);
    void Carrier_Modulation(void);
    void SPWM(void);
    void PROTECT_PDPINTA_ISR(void);
    
    void main(void)
    {
    
    	// Step 1. Initialize System Control:
    	// PLL, WatchDog, enable Peripheral Clocks
    	// This example function is found in the DSP281x_SysCtrl.c file.
    	InitSysCtrl();
    
    	//��memcpy֮��ִ��Initflash()��������д��Ĺ��ܺ���
    	//MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);
    	//InitFlash();
    
    	// Step 2. Initalize GPIO:
    	// This example function is found in the DSP281x_Gpio.c file and
    	// illustrates how to set the GPIO to it's default state.
    	InitGpio();
    
    	// Step 3. Clear all interrupts and initialize PIE vector table:
    	// Disable CPU interrupts
    	DINT;
    
    	// Initialize PIE control registers to their default state.
    	// The default state is all PIE interrupts disabled and flags
    	// are cleared.
    	// This function is found in the DSP281x_PieCtrl.c file.
    	InitPieCtrl();
    
    	// Disable CPU interrupts and clear all CPU interrupt flags:
    	IER=0x0000;
    	IFR=0x0000;
    
    	// Initialize the PIE vector table with pointers to the shell Interrupt
    	// Service Routines (ISR).
    	// This will populate the entire table, even if the interrupt
    	// is not used in this example.  This is useful for debug purposes.
    	// The shell ISR routines are found in DSP281x_DefaultIsr.c.
    	// This function is found in DSP281x_PieVect.c.
    	InitPieVectTable();
    
    	// Interrupts that are used in this example are re-mapped to
    	// ISR functions found within this file.
    	EALLOW;  // This is needed to write to EALLOW protected registers
    	PieVectTable.T1PINT=&T1_Compare_isr;
    	EDIS;    // This is needed to disable write to EALLOW protected registers
    
    	// Step 4. Initialize all the Device Peripherals:
    	// This function is found in DSP281x_InitPeripherals.c
    	// InitPeripherals(); // Not required for this example
    	InitEv();
    	InitAdc();
    
    	// Step 5. User specific code, enable interrupts:
    	PieCtrlRegs.PIEIER2.all=M_INT4;      // PIE interrupt enable,T1��ʱ���ж�λ��INT2.4
    	IER|=M_INT2;
    
    	// Enable global Interrupts and higher priority real-time debug events:
    	EINT;                                // Enable Global interrupt INTM
    	ERTM;                                // Enable Global realtime interrupt DBGM
    	EvaRegs.T1CON.bit.TENABLE = 1;       // Timer1 number counter enable
    
    	// Step 6. Just sit and loop forever:
    	for(;;);
    
    }
    
    //  ADC������
    void AD_Sampling(void)
    {
    
    	idc_s=(AdcRegs.ADCRESULT0>>4);//���������ӽ�20A,��������Ϊ51ŷʱ��A6ͨ��
    	idc=(idc_s-2092+15);
    	idc_Q=_IQmpy(_IQ(idc),_IQ(0.01436472));
    
    }
    void Carrier_Modulation(void)
    {
    
    // delay time T/4
    
    	if (j<N)
    	{
    		buffer[j]=idc_Q;
    		j++;
    	}
    
    	else
    	{
    		j=0;
    	}
    
    	if (k<N)
    	{
    		idc_Q1=idc_Q;
    		idc_Q2=buffer[k];
    		k++;
    	}
    
    	else
    	{
    		k=0;
    	}
    
    	idc_avg1=_IQmpy(idc_Q1+idc_Q2,_IQ(0.5));
    
    // delay time T/8
    
    	if (jj<N)
    	{
    		buffer[jj]=idc_avg1;
    		jj++;
    	}
    
    	else
    	{
    		jj=0;
    	}
    
    	if (kk<N)
    	{
    		idc_avg1_Q1=idc_avg1;
    		idc_avg1_Q2=buffer[kk];
    		kk++;
    	}
    
    	else
    	{
    		kk=0;
    	}
    
    	idc_avg2=_IQmpy(idc_avg1_Q1+idc_avg1_Q2,_IQ(0.5));
    	coefficient_k=_IQdiv(idc_avg2,idc_Q);    // ������ѡ�����ز����Է�ֵ����ϵ��k1��k1=idc˲ʱֵ/idcƽ��ֵ��ʵ����ѡ���ɵ��Ʋ����Է�ֵ����ϵ��k��k=1/k1��
    
    	if (coefficient_k<=_IQ(0.5))
    	{
    		coefficient_k=_IQ(0.5);
    	}
    	if (coefficient_k>=_IQ(2.5))
    	{
    		coefficient_k=_IQ(2.5);
    	}
    }
    
    void SPWM(void)
    {
    	P=_IQmpy(_IQ(sina[i]),_IQ(Modu_Index));
    	G=_IQmpy(P,coefficient_k);
    
    	//G=_IQmpy(_IQ(sina[i]),_IQ(Modu_Index));//�������
    
    	if (G>=0)
    	{
    		g1=(int)((long)3750*G>>18);    // S5,S6�����ܸ�Ƶ, ��ʵ��ʱ��Ҫ���߼����ߣ��ϵ�ʱע����������������DSP G2
    		//g1=3751;
    		//g2=(int)((long)3750*G>>18);    // S2,S3�����ܸ�Ƶ, ��DSP G3
    		g2 = 3751;//��Ƶ
    		g3=0;                          // S1,S4�����ܵ͵�ƽ, ��DSP G5
    	}
    
    	if (G<0)
    	{
    	    g1=(int)((long)3750*(-G)>>18); // S5,S6�����ܸ�Ƶ, �����ܵ��Ʋ�ȡABS
    	    //g1=0;
    		g2=0;                          // S2,S3�����ܵ͵�ƽ
    		g3 = 3751;//��Ƶ
    		//g3=(int)((long)3750*(-G)>>18); // S1,S4�����ܸ�Ƶ
    	}
    	i++;
    	if (i>=N)
    	{
    	    i=0;
    	}
        if (g1<=0)
    	g1=0;
    	if (g1>=3750)
    	g1=3750;
        if (g2<=0)
    	g2=0;
    	if (g2>=3750)
    	g2=3750;
    	if (g3<=0)
    	g3=0;
    	if (g3>=3750)
    	g3=3750;
    
        EvaRegs.CMPR1=g1;
        EvaRegs.CMPR2=g2;
    	EvaRegs.CMPR3=g3;
    
    }
    
    void PROTECT_PDPINTA_ISR(void)    // EV-A, INT1.1
    {
    // Insert ISR Code here, ��GPIO���Ž������ߺ����ͣ��������ʱ��S1/4�㵼ͨ��S2/3/5�ض�
    	if (idc_Q>=_IQ(5.5))
    	{
    	  EvaRegs.COMCONA.bit.FCMP1OE = 0;
    	  EvaRegs.COMCONA.bit.FCMP2OE = 1;
    	  EvaRegs.COMCONA.bit.FCMP3OE = 0;
    	}
    	if (idc_Q<_IQ(5.5))
    	{
    
    	}
    }
    interrupt void T1_Compare_isr(void)
    {
    	AD_Sampling();
    	Carrier_Modulation();
    	SPWM();
    	PROTECT_PDPINTA_ISR();
    	//DA_Viewer();
        EvaRegs.EVAIFRA.bit.T1PINT=1;        // ���T1�����ж��еı�־λ
        PieCtrlRegs.PIEACK.bit.ACK2=1;       // ��Ӧͬ���ж�
        EINT;                                // ��ȫ���ж�
    }
    
    // TI File $Revision: /main/2 $
    // Checkin $Date: April 29, 2005   11:10:23 $
    //###########################################################################
    //
    // FILE:	DSP281x_Ev.c
    //
    // TITLE:	DSP281x Event Manager Initialization & Support Functions.
    //
    //###########################################################################
    // $TI Release: DSP281x C/C++ Header Files V1.20 $
    // $Release Date: July 27, 2009 $
    //###########################################################################
    
    #include "DSP281x_Device.h"     // DSP281x Headerfile Include File
    #include "DSP281x_Examples.h"   // DSP281x Examples Include File
    
    //---------------------------------------------------------------------------
    // InitEv: 
    //---------------------------------------------------------------------------
    // This function initializes to a known state.
    //
    void InitEv(void)
    {
    
    // EVA Configure T1PWM, T2PWM, PWM1-PWM6
    
    	  // Initalize the timers
    	  // Initalize EVA Timer1
    	  EvaRegs.T1PR = 3750;          // Timer1 period, the frequency of carrier is 20kHz
    	  EvaRegs.T1CMPR = 0x0000;      // Timer1 compare
    	  EvaRegs.T1CNT = 0x0000;       // Timer1 counter
    
    	  EvaRegs.T1CON.bit.TMODE=1;    // TMODE = continuous up/down
    	  EvaRegs.T1CON.bit.TPS=0;      // T1CLK = HSPCLK/1 = 150MHz
    	  EvaRegs.T1CON.bit.TENABLE=0;  // Timer disable
    	  EvaRegs.T1CON.bit.TCLKS10=0;  // Select the internal clock
    	  EvaRegs.T1CON.bit.TECMPR=1;   // Timer compare enable
    
    	  // Setup T1PWM and T2PWM
    	  // Drive T1/T2 PWM by compare logic
    //	  EvaRegs.GPTCONA.bit.TCMPOE = 1;
    	  // Polarity of GP Timer 1 Compare = Active low
    //	  EvaRegs.GPTCONA.bit.T1PIN = 1;
    	  // Polarity of GP Timer 2 Compare = Active high
    //	  EvaRegs.GPTCONA.bit.T2PIN = 2;
    	  EvaRegs.GPTCONA.bit.T1TOADC=2;   // ��������ADC
    
    	  // Enable compare for PWM1-PWM6
    	  EvaRegs.CMPR1 = 0x0000;
    	  EvaRegs.CMPR2 = 0x0000;
    	  EvaRegs.CMPR3 = 0x0000;
    
    	  // Compare action control.  Action that takes place
    	  // on a cmpare event
    	  // output pin 1 CMPR1 - active high
    	  // output pin 2 CMPR1 - active low
    	  // output pin 3 CMPR2 - active high
    	  // output pin 4 CMPR2 - active low
    	  // output pin 5 CMPR3 - active high
    	  // output pin 6 CMPR3 - active low
    	  //EvaRegs.ACTRA.all = 0x0666;
    
    	  EvaRegs.ACTRA.all = 0x0999;
    
    	  //EvaRegs.DBTCONA.all = 0x0000;    // Disable deadband
    
    /*	  Overlap_time 1us   */
    	  EvaRegs.DBTCONA.bit.DBT = 6;
    	  EvaRegs.DBTCONA.bit.EDBT1 = 1;
    	  EvaRegs.DBTCONA.bit.EDBT2 = 1;
    	  EvaRegs.DBTCONA.bit.EDBT3 = 1;
    	  EvaRegs.DBTCONA.bit.DBTPS = 5;
    
    	  EvaRegs.COMCONA.bit.CENABLE=1;   // ʹ�ܱȽϵ�Ԫ�ıȽϲ���
    	  //EvaRegs.COMCONA.bit.FCOMPOE=1;   // ȫ�Ƚ����ʹ��
    	  EvaRegs.COMCONA.bit.CLD=2;
    
    	  EvaRegs.EVAIMRA.bit.T1PINT=1;  // Timer1 period interrupt enable
    	  EvaRegs.EVAIFRA.bit.T1PINT=1;  // ���T1�����ж��еı�־λ
    
    /*	  Protect   */
    	  EvaRegs.COMCONA.bit.PDPINTASTATUS;
    	  //EvaRegs.EVAIMRA.bit.PDPINTA=1;  // PDPINTA interrupt enable
    
    	  EvaRegs.EXTCONA.bit.INDCOE =1;  // ȫ�Ƚ������Ϊ�����ֵ�������
    	  EvaRegs.COMCONA.bit.FCMP1OE = 1;
    	  EvaRegs.COMCONA.bit.FCMP2OE = 1;
    	  EvaRegs.COMCONA.bit.FCMP3OE = 1;
    }	
    	
    //===========================================================================
    // No more.
    //===========================================================================
    
    // TI File $Revision: /main/2 $
    // Checkin $Date: April 29, 2005   11:11:45 $
    //###########################################################################
    //
    // FILE:	DSP281x_Adc.c
    //
    // TITLE:	DSP281x ADC Initialization & Support Functions.
    //
    //###########################################################################
    // $TI Release: DSP281x C/C++ Header Files V1.20 $
    // $Release Date: July 27, 2009 $
    //###########################################################################
    
    #include "DSP281x_Device.h"     // DSP281x Headerfile Include File
    #include "DSP281x_Examples.h"   // DSP281x Examples Include File
    
    #define ADC_usDELAY  8000L
    #define ADC_usDELAY2 20L
    
    //---------------------------------------------------------------------------
    // InitAdc: 
    //---------------------------------------------------------------------------
    // This function initializes ADC to a known state.
    //
    void InitAdc(void)
    {
    	extern void DSP28x_usDelay(Uint32 Count);
    	
        // To powerup the ADC the ADCENCLK bit should be set first to enable
        // clocks, followed by powering up the bandgap and reference circuitry.
        // After a 5ms delay the rest of the ADC can be powered up. After ADC
        // powerup, another 20us delay is required before performing the first
        // ADC conversion. Please note that for the delay function below to
        // operate correctly the CPU_CLOCK_SPEED define statement in the
        // DSP28_Examples.h file must contain the correct CPU clock period in
        // nanoseconds. For example:
    
    	AdcRegs.ADCTRL1.bit.RESET = 1;         // reset the ADC
    	asm(" RPT #0 || NOP");                 // one cycle
    	AdcRegs.ADCTRL1.bit.RESET = 0;
    
    	AdcRegs.ADCTRL3.bit.ADCBGRFDN = 0x3;   // Power up bandgap/reference circuitry
    	DELAY_US(ADC_usDELAY);                 // Delay before powering up rest of ADC
    	AdcRegs.ADCTRL3.bit.ADCPWDN = 1;	   // Power up rest of ADC
    	DELAY_US(ADC_usDELAY2);                // Delay after powering up ADC
    
    	/*AdcRegs.ADCTRL1.bit.RESET = 1;       // reset the ADC
    	asm(" RPT #0 || NOP");                 // one cycle
    	AdcRegs.ADCTRL1.bit.RESET = 0;*/
    
    	AdcRegs.ADCTRL1.bit.SUSMOD = 3;         // ������ͣʱ�����з��������������ֵ�·�߼�����ֹͣ
    
    	AdcRegs.ADCTRL1.bit.ACQ_PS = 2;         // S/H width in ADC module periods = (ACQ_PS+1)/ADCLK = 1.2 us
    	AdcRegs.ADCTRL1.bit.CPS = 1;            // �ں�ʱ���ٽ���һ�ζ���Ƶ
    	AdcRegs.ADCTRL3.bit.ADCCLKPS = 15;      // ADC module clock = HSPCLK/(2*ADCCLKPS)*(CPS+1)=2.5 MHz
    	AdcRegs.ADCTRL1.bit.CONT_RUN = 1;       // 0,���/ֹͣģʽ 1,����ģʽ
    	AdcRegs.ADCTRL1.bit.SEQ_CASC = 1;       // 0 Dual Sequencer Mode, 1 Cascaded Mode
    	AdcRegs.ADCTRL3.bit.SMODE_SEL = 0;      // 0 Sequential Sampling Mode, 1 Simultaneous Sampling Mode
    	AdcRegs.ADCMAXCONV.bit.MAX_CONV1 = 0;   // ������·
    	AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x6;  // ADCINA6
    
    	AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1;     // ���SEQ1���жϱ�־λ
    	AdcRegs.ADCST.bit.INT_SEQ2_CLR = 1;     // ���SEQ2���жϱ�־λ
    
    	AdcRegs.ADCTRL2.bit.EVA_SOC_SEQ1 = 1;   // Allows SEQ1/SEQ to be started by Event Manager A trigger
    	AdcRegs.ADCTRL2.bit.EVB_SOC_SEQ = 0;    // EVB SOC enable for cascaded sequencer (Note: This bit is active only in cascaded mode.) 0, No action.
    	AdcRegs.ADCTRL2.bit.EVB_SOC_SEQ2 = 0;   // Event Manager B SOC mask bit for SEQ2. 0, SEQ2 cannot be started by EVB trigger.
    	AdcRegs.ADCTRL2.bit.EXT_SOC_SEQ1 = 0;   // External signal start-of-conversion bit for SEQ1. 0, No action.
    	AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 0;   // SEQ1 interrupt enable. This bit enables the interrupt request to CPU by INT SEQ1.
    	AdcRegs.ADCTRL2.bit.INT_ENA_SEQ2 = 0;   // SEQ2 interrupt disable. This bit enables or disables an interrupt request to the CPU by INT SEQ2.
    	AdcRegs.ADCTRL2.bit.INT_MOD_SEQ1 = 0;   // SEQ1 interrupt mode. 0, INT SEQ1 is set at the end of every SEQ1 sequence.
    	AdcRegs.ADCTRL2.bit.INT_MOD_SEQ2 = 0;   // SEQ2 interrupt mode. 0, INT SEQ2 is set at the end of every SEQ2 sequence.
    	AdcRegs.ADCTRL2.bit.RST_SEQ1 = 0;       // Reset sequencer1
    	AdcRegs.ADCTRL2.bit.RST_SEQ2 = 0;       // Reset sequencer2 0, No action.
    	AdcRegs.ADCTRL2.bit.SOC_SEQ1 = 1;       // Start of conversion (SOC) trigger for Sequencer 1 (SEQ1).
    	AdcRegs.ADCTRL2.bit.SOC_SEQ2 = 0;       // Start of conversion trigger for sequencer 2 (SEQ2). (Only applicable in dual-sequencer mode; ignored in cascaded mode.) 0 Clears a Pending SOC trigger
    
    }	
    
    //===========================================================================
    // No more.
    //===========================================================================