This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用 fcl_f2838x_tmdxiddk_cpu1 範例開發自己的伺服馬達,目前遇到一個問題,在使用仿真器開發時燒錄 Flash 正常,功能執行起來也都正常,但是我想要用 Flash 開機時卻無法正常啟動,我將我的原始碼刪除一部分後就可以從 Flash 啟動了,所以確定不是硬體問題,請問是我的 CMD 檔配置錯誤嗎?
//############################################################################# // // FILE: iddk_servo_2838x_flash_lnk_cpu1.cmd // //############################################################################# // $TI Release: MotorControl SDK v2.01.00.00 $ // $Release Date: Mon Nov 11 15:18:12 CST 2019 $ // $Copyright: // Copyright (C) 2017-2019 Texas Instruments Incorporated // // http://www.ti.com/ ALL RIGHTS RESERVED // $ //############################################################################# // In addition to this memory linker command file, // add the header linker command file directly to the project. // The header linker command file is required to link the // peripheral structures to the proper locations within the memory map. // // The header linker files are found in <base>\2837x_headers\cmd // // For BIOS applications add: f2837x_Headers_BIOS.cmd // For nonBIOS applications add: f2837x_Headers_nonBIOS.cmd // // The user must define CLA_C in the project linker settings if using the // CLA C compiler // Project Properties -> C2000 Linker -> Advanced Options -> Command File // Preprocessing -> --define #ifdef CLA_C // Define a size for the CLA scratchpad area that will be used // by the CLA compiler for local symbols and temps // Also force references to the special symbols that mark the // scratchpad are. CLA_SCRATCHPAD_SIZE = 0x100; --undef_sym=__cla_scratchpad_end --undef_sym=__cla_scratchpad_start #endif //CLA_C MEMORY { /* BEGIN is used for the "boot to Flash" bootloader mode */ BEGIN : origin = 0x080000, length = 0x000002 BOOT_RSVD : origin = 0x000002, length = 0x0001AE /* Part of M0, BOOT rom will use this for stack */ RAMM0 : origin = 0x0001B0, length = 0x000250 RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */ /* RAMD0 : origin = 0x00C000, length = 0x000800 */ /* RAMD1 : origin = 0x00C800, length = 0x000800 */ RAMD0_1 : origin = 0x00C000, length = 0x001000 RAMLS0 : origin = 0x008000, length = 0x000800 RAMLS1 : origin = 0x008800, length = 0x000800 RAMLS2 : origin = 0x009000, length = 0x000800 RAMLS_BLK : origin = 0x009800, length = 0x002800 /* RAMLS3 : origin = 0x009800, length = 0x000800 RAMLS4 : origin = 0x00A000, length = 0x000800 RAMLS5 : origin = 0x00A800, length = 0x000800 RAMLS6 : origin = 0x00B000, length = 0x000800 RAMLS7 : origin = 0x00B800, length = 0x000800 */ RAMGS0 : origin = 0x00D000, length = 0x001000 RAMGS1 : origin = 0x00E000, length = 0x001000 RAMGS2 : origin = 0x00F000, length = 0x001000 RAMGS3 : origin = 0x010000, length = 0x001000 RAMGS4 : origin = 0x011000, length = 0x001000 RAMGS5 : origin = 0x012000, length = 0x001000 RAMGS6 : origin = 0x013000, length = 0x001000 RAMGS7 : origin = 0x014000, length = 0x001000 RAMGS8 : origin = 0x015000, length = 0x001000 RAMGS9 : origin = 0x016000, length = 0x001000 RAMGS10 : origin = 0x017000, length = 0x001000 RAMGS11 : origin = 0x018000, length = 0x001000 RAMGS12 : origin = 0x019000, length = 0x001000 RAMGS13 : origin = 0x01A000, length = 0x001000 RAMGS14 : origin = 0x01B000, length = 0x001000 RAMGS15 : origin = 0x01C000, length = 0x001000 /* Flash sectors */ FLASH0 : origin = 0x080002, length = 0x001FFE /* on-chip Flash */ FLASH1 : origin = 0x082000, length = 0x002000 /* on-chip Flash */ FLASH2 : origin = 0x084000, length = 0x002000 /* on-chip Flash */ FLASH3 : origin = 0x086000, length = 0x002000 /* on-chip Flash */ FLASH4 : origin = 0x088000, length = 0x008000 /* on-chip Flash */ FLASH5 : origin = 0x090000, length = 0x008000 /* on-chip Flash */ FLASH6 : origin = 0x098000, length = 0x008000 /* on-chip Flash */ FLASH7 : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */ FLASH8 : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */ FLASH9 : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */ FLASH10 : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */ FLASH11 : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */ FLASH12 : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */ FLASH13 : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */ CPU1TOCPU2RAM : origin = 0x03A000, length = 0x000800 CPU2TOCPU1RAM : origin = 0x03B000, length = 0x000800 CPUTOCMRAM : origin = 0x039000, length = 0x000200 CMTOCPURAM : origin = 0x038000, length = 0x000200 CPUTOCMRAM_ECAT : origin = 0x039200, length = 0x000200 CMTOCPURAM_ECAT : origin = 0x038200, length = 0x000200 CANA_MSG_RAM : origin = 0x049000, length = 0x000800 CANB_MSG_RAM : origin = 0x04B000, length = 0x000800 RESET : origin = 0x3FFFC0, length = 0x000002 CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080 CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080 } SECTIONS { codestart : > BEGIN, ALIGN(4) .text : >> FLASH1 | FLASH2 | FLASH3 | FLASH4, ALIGN(4) .cinit : > FLASH5, ALIGN(4) .switch : > FLASH1, ALIGN(4) .reset : > RESET, TYPE = DSECT /* not used, */ .stack : > RAMLS0 #if defined(__TI_EABI__) .init_array : > FLASH6, ALIGN(8) .bss : > RAMLS_BLK .bss:output : > RAMLS_BLK .bss:cio : > RAMLS_BLK .data : > RAMLS_BLK .sysmem : > RAMLS_BLK /* Initalized sections go in Flash */ .const : > FLASH6, ALIGN(8) #else .pinit : > FLASH6, ALIGN(8) .ebss : > RAMLS_BLK .esysmem : > RAMLS_BLK .cio : > RAMLS_BLK /* Initalized sections go in Flash */ .econst : >> FLASH4 | FLASH5, ALIGN(4) #endif MSGRAM_CPU1_TO_CPU2 : > CPU1TOCPU2RAM, type=NOINIT MSGRAM_CPU2_TO_CPU1 : > CPU2TOCPU1RAM, type=NOINIT MSGRAM_CPU_TO_CM : > CPUTOCMRAM, type=NOINIT MSGRAM_CM_TO_CPU : > CMTOCPURAM, type=NOINIT MSGRAM_CPU_TO_CM_ECAT > CPUTOCMRAM_ECAT, type=NOINIT MSGRAM_CM_TO_CPU_ECAT > CMTOCPURAM_ECAT, type=NOINIT /* CLA specific sections */ #if defined(__TI_EABI__) Cla1Prog : LOAD = FLASH4, RUN = RAMLS2, LOAD_START(Cla1funcsLoadStart), LOAD_END(Cla1funcsLoadEnd), RUN_START(Cla1funcsRunStart), LOAD_SIZE(Cla1funcsLoadSize), ALIGN(8) #else Cla1Prog : LOAD = FLASH4, RUN = RAMLS2, LOAD_START(_Cla1funcsLoadStart), LOAD_END(_Cla1funcsLoadEnd), RUN_START(_Cla1funcsRunStart), LOAD_SIZE(_Cla1funcsLoadSize), PAGE = 0, ALIGN(8) #endif ClaData : > RAMLS1 Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, type=NOINIT CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, type=NOINIT /* SFRA specific sections */ SFRA_F32_Data : > RAMGS5, ALIGN = 64 #ifdef CLA_C /* CLA C compiler sections */ // // Must be allocated to memory the CLA has write access to // CLAscratch : { *.obj(CLAscratch) . += CLA_SCRATCHPAD_SIZE; *.obj(CLAscratch_end) } > RAMLS1 .scratchpad : > RAMLS1 .bss_cla : > RAMLS1 #if defined(__TI_EABI__) .const_cla : LOAD = FLASH2, RUN = RAMLS2, RUN_START(Cla1ConstRunStart), LOAD_START(Cla1ConstLoadStart), LOAD_SIZE(Cla1ConstLoadSize), ALIGN(4) #else .const_cla : LOAD = FLASH2, RUN = RAMLS2, RUN_START(Cla1ConstRunStart), LOAD_START(Cla1ConstLoadStart), LOAD_SIZE(Cla1ConstLoadSize), ALIGN(4) #endif #endif //CLA_C #if defined(__TI_EABI__) .TI.ramfunc : { } LOAD = FLASH3, RUN = RAMD0_1, LOAD_START(RamfuncsLoadStart), LOAD_SIZE(RamfuncsLoadSize), LOAD_END(RamfuncsLoadEnd), RUN_START(RamfuncsRunStart), RUN_SIZE(RamfuncsRunSize), RUN_END(RamfuncsRunEnd), ALIGN(4) #else .TI.ramfunc : { } LOAD = FLASH3, RUN = RAMD0_1, LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), RUN_SIZE(_RamfuncsRunSize), RUN_END(_RamfuncsRunEnd), PAGE = 0, ALIGN(4) #endif } /* //=========================================================================== // End of file. //=========================================================================== */
032 说:但是我想要用 Flash 開機時卻無法正常啟動,我將我的原始碼刪除一部分後就可以從 Flash 啟動了
您现在是用仿真器的话,可以FLASH内运行,而不使用仿真器的话就无法正常启动?
请问您删除的是具体哪些代码呢?
你好,
是的,用仿真器的話可以正常啟動,斷電重開後,連接仿真器不用再載入一次只要按 Restart 就可以執行,所以應該有載入成功。
我因為有 Porting CanFestival CANopen 協議棧,整個代碼變得有點大,所以修改原本的 CMD 檔後才能正常執行,目前測試應該是把它拿掉,讓代碼容量減少就可以開機。
Susan Yang 说:032但是我想要用 Flash 開機時卻無法正常啟動,我將我的原始碼刪除一部分後就可以從 Flash 啟動了您现在是用仿真器的话,可以FLASH内运行,而不使用仿真器的话就无法正常启动?
请问您删除的是具体哪些代码呢?
你好,請問有新的建議嗎?
自己回覆一下自己,
此問題在英文論壇有答案,
https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/900463
問題在於預設下 Watchdog 是打開的,有可能在初始化過程中就觸發了 WD,造成開不了機,
在 f2838x_codestartbranch.asm 中先關閉 WD 就可以了:
WD_DISABLE .set 1 ;set to 1 to disable WD, else set to 0