This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28388D 使用 Flash 開機問題



我使用 fcl_f2838x_tmdxiddk_cpu1 範例開發自己的伺服馬達,目前遇到一個問題,在使用仿真器開發時燒錄 Flash 正常,功能執行起來也都正常,但是我想要用 Flash 開機時卻無法正常啟動,我將我的原始碼刪除一部分後就可以從 Flash 啟動了,所以確定不是硬體問題,請問是我的 CMD 檔配置錯誤嗎?

//#############################################################################
//
// FILE:    iddk_servo_2838x_flash_lnk_cpu1.cmd
//
//#############################################################################
// $TI Release: MotorControl SDK v2.01.00.00 $
// $Release Date: Mon Nov 11 15:18:12 CST 2019 $
// $Copyright:
// Copyright (C) 2017-2019 Texas Instruments Incorporated
//
//     http://www.ti.com/ ALL RIGHTS RESERVED
// $
//#############################################################################
// In addition to this memory linker command file,
// add the header linker command file directly to the project.
// The header linker command file is required to link the
// peripheral structures to the proper locations within the memory map.
//
// The header linker files are found in <base>\2837x_headers\cmd
//
// For BIOS applications add:      f2837x_Headers_BIOS.cmd
// For nonBIOS applications add:   f2837x_Headers_nonBIOS.cmd
//
// The user must define CLA_C in the project linker settings if using the
// CLA C compiler
// Project Properties -> C2000 Linker -> Advanced Options -> Command File
// Preprocessing -> --define
#ifdef CLA_C
// Define a size for the CLA scratchpad area that will be used
// by the CLA compiler for local symbols and temps
// Also force references to the special symbols that mark the
// scratchpad are.
CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
#endif //CLA_C


MEMORY
{
   /* BEGIN is used for the "boot to Flash" bootloader mode   */
   BEGIN            : origin = 0x080000, length = 0x000002
   BOOT_RSVD        : origin = 0x000002, length = 0x0001AE     /* Part of M0, BOOT rom will use this for stack */
   RAMM0            : origin = 0x0001B0, length = 0x000250
   RAMM1            : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
/* RAMD0            : origin = 0x00C000, length = 0x000800 */
/* RAMD1            : origin = 0x00C800, length = 0x000800 */
   RAMD0_1          : origin = 0x00C000, length = 0x001000

   RAMLS0           : origin = 0x008000, length = 0x000800
   RAMLS1           : origin = 0x008800, length = 0x000800
   RAMLS2           : origin = 0x009000, length = 0x000800
   RAMLS_BLK        : origin = 0x009800, length = 0x002800
/*
   RAMLS3           : origin = 0x009800, length = 0x000800
   RAMLS4           : origin = 0x00A000, length = 0x000800
   RAMLS5           : origin = 0x00A800, length = 0x000800
   RAMLS6           : origin = 0x00B000, length = 0x000800
   RAMLS7           : origin = 0x00B800, length = 0x000800
*/
   RAMGS0           : origin = 0x00D000, length = 0x001000
   RAMGS1           : origin = 0x00E000, length = 0x001000
   RAMGS2           : origin = 0x00F000, length = 0x001000
   RAMGS3           : origin = 0x010000, length = 0x001000
   RAMGS4           : origin = 0x011000, length = 0x001000
   RAMGS5           : origin = 0x012000, length = 0x001000
   RAMGS6           : origin = 0x013000, length = 0x001000
   RAMGS7           : origin = 0x014000, length = 0x001000
   RAMGS8           : origin = 0x015000, length = 0x001000
   RAMGS9           : origin = 0x016000, length = 0x001000
   RAMGS10          : origin = 0x017000, length = 0x001000
   RAMGS11          : origin = 0x018000, length = 0x001000
   RAMGS12          : origin = 0x019000, length = 0x001000
   RAMGS13          : origin = 0x01A000, length = 0x001000
   RAMGS14          : origin = 0x01B000, length = 0x001000
   RAMGS15          : origin = 0x01C000, length = 0x001000

   /* Flash sectors */
   FLASH0           : origin = 0x080002, length = 0x001FFE  /* on-chip Flash */
   FLASH1           : origin = 0x082000, length = 0x002000  /* on-chip Flash */
   FLASH2           : origin = 0x084000, length = 0x002000  /* on-chip Flash */
   FLASH3           : origin = 0x086000, length = 0x002000  /* on-chip Flash */
   FLASH4           : origin = 0x088000, length = 0x008000  /* on-chip Flash */
   FLASH5           : origin = 0x090000, length = 0x008000  /* on-chip Flash */
   FLASH6           : origin = 0x098000, length = 0x008000  /* on-chip Flash */
   FLASH7           : origin = 0x0A0000, length = 0x008000  /* on-chip Flash */
   FLASH8           : origin = 0x0A8000, length = 0x008000  /* on-chip Flash */
   FLASH9           : origin = 0x0B0000, length = 0x008000  /* on-chip Flash */
   FLASH10          : origin = 0x0B8000, length = 0x002000  /* on-chip Flash */
   FLASH11          : origin = 0x0BA000, length = 0x002000  /* on-chip Flash */
   FLASH12          : origin = 0x0BC000, length = 0x002000  /* on-chip Flash */
   FLASH13          : origin = 0x0BE000, length = 0x002000  /* on-chip Flash */

   CPU1TOCPU2RAM   	: origin = 0x03A000, length = 0x000800
   CPU2TOCPU1RAM   	: origin = 0x03B000, length = 0x000800
   CPUTOCMRAM       : origin = 0x039000, length = 0x000200
   CMTOCPURAM       : origin = 0x038000, length = 0x000200

   CPUTOCMRAM_ECAT	: origin = 0x039200, length = 0x000200
   CMTOCPURAM_ECAT	: origin = 0x038200, length = 0x000200

   CANA_MSG_RAM     : origin = 0x049000, length = 0x000800
   CANB_MSG_RAM     : origin = 0x04B000, length = 0x000800

   RESET            : origin = 0x3FFFC0, length = 0x000002

   CLA1_MSGRAMLOW   : origin = 0x001480,   length = 0x000080
   CLA1_MSGRAMHIGH  : origin = 0x001500,   length = 0x000080
}

SECTIONS
{
   codestart           : > BEGIN, ALIGN(4)
   .text               : >> FLASH1 | FLASH2 | FLASH3 | FLASH4, ALIGN(4)
   .cinit              : > FLASH5, ALIGN(4)
   .switch             : > FLASH1, ALIGN(4)
   .reset              : > RESET, TYPE = DSECT /* not used, */
   .stack              : > RAMLS0

#if defined(__TI_EABI__)
   .init_array      : > FLASH6, ALIGN(8)
   .bss             : > RAMLS_BLK
   .bss:output      : > RAMLS_BLK
   .bss:cio         : > RAMLS_BLK
   .data            : > RAMLS_BLK
   .sysmem          : > RAMLS_BLK
   /* Initalized sections go in Flash */
   .const           : > FLASH6, ALIGN(8)
#else
   .pinit           : > FLASH6, ALIGN(8)
   .ebss            : > RAMLS_BLK
   .esysmem         : > RAMLS_BLK
   .cio             : > RAMLS_BLK
   /* Initalized sections go in Flash */
   .econst          : >> FLASH4 | FLASH5, ALIGN(4)
#endif

   MSGRAM_CPU1_TO_CPU2 : > CPU1TOCPU2RAM, type=NOINIT
   MSGRAM_CPU2_TO_CPU1 : > CPU2TOCPU1RAM, type=NOINIT
   MSGRAM_CPU_TO_CM    : > CPUTOCMRAM, type=NOINIT
   MSGRAM_CM_TO_CPU    : > CMTOCPURAM, type=NOINIT

   MSGRAM_CPU_TO_CM_ECAT   > CPUTOCMRAM_ECAT, type=NOINIT
   MSGRAM_CM_TO_CPU_ECAT   > CMTOCPURAM_ECAT, type=NOINIT

    /* CLA specific sections */
#if defined(__TI_EABI__)
   Cla1Prog         :   LOAD = FLASH4,
                        RUN = RAMLS2,
                        LOAD_START(Cla1funcsLoadStart),
                        LOAD_END(Cla1funcsLoadEnd),
                        RUN_START(Cla1funcsRunStart),
                        LOAD_SIZE(Cla1funcsLoadSize),
                        ALIGN(8)
#else
   Cla1Prog         :   LOAD = FLASH4,
                        RUN = RAMLS2,
                        LOAD_START(_Cla1funcsLoadStart),
                        LOAD_END(_Cla1funcsLoadEnd),
                        RUN_START(_Cla1funcsRunStart),
                        LOAD_SIZE(_Cla1funcsLoadSize),
                        PAGE = 0, ALIGN(8)
#endif

   ClaData			: > RAMLS1

   Cla1ToCpuMsgRAM  : > CLA1_MSGRAMLOW, type=NOINIT
   CpuToCla1MsgRAM  : > CLA1_MSGRAMHIGH, type=NOINIT

   /* SFRA specific sections */
   SFRA_F32_Data	: > RAMGS5, ALIGN = 64

#ifdef CLA_C
   /* CLA C compiler sections */
   //
   // Must be allocated to memory the CLA has write access to
   //
   CLAscratch       :
                     { *.obj(CLAscratch)
                     . += CLA_SCRATCHPAD_SIZE;
                     *.obj(CLAscratch_end) } >  RAMLS1

   .scratchpad      : > RAMLS1
   .bss_cla         : > RAMLS1

#if defined(__TI_EABI__)
   .const_cla       :   LOAD = FLASH2,
                        RUN = RAMLS2,
                        RUN_START(Cla1ConstRunStart),
                        LOAD_START(Cla1ConstLoadStart),
                        LOAD_SIZE(Cla1ConstLoadSize),
                     	ALIGN(4)
#else
   .const_cla       :   LOAD = FLASH2,
                        RUN = RAMLS2,
                        RUN_START(Cla1ConstRunStart),
                        LOAD_START(Cla1ConstLoadStart),
                        LOAD_SIZE(Cla1ConstLoadSize),
                    	ALIGN(4)
#endif
#endif //CLA_C

#if defined(__TI_EABI__)
   .TI.ramfunc : {
                  } LOAD = FLASH3,
                    RUN = RAMD0_1,
                    LOAD_START(RamfuncsLoadStart),
                    LOAD_SIZE(RamfuncsLoadSize),
                    LOAD_END(RamfuncsLoadEnd),
                    RUN_START(RamfuncsRunStart),
                    RUN_SIZE(RamfuncsRunSize),
                    RUN_END(RamfuncsRunEnd),
                    ALIGN(4)
#else
   .TI.ramfunc : {
                  } LOAD = FLASH3,
                    RUN = RAMD0_1,
                    LOAD_START(_RamfuncsLoadStart),
                    LOAD_SIZE(_RamfuncsLoadSize),
                    LOAD_END(_RamfuncsLoadEnd),
                    RUN_START(_RamfuncsRunStart),
                    RUN_SIZE(_RamfuncsRunSize),
                    RUN_END(_RamfuncsRunEnd),
                    PAGE = 0, ALIGN(4)
#endif

}

/*
//===========================================================================
// End of file.
//===========================================================================
*/