This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DMA触发源的设置

尊敬的工程师:

您好,关于DMA的触发源,是不是DMA的触发源只是监测外设的中断的标志位(无论中断是否使能)。我有个疑问,DMA触发在内部监测的是不是中断的标志位,是不是和中断是同一个标志位?谢谢。

如果对于使用AD的INT1触发DMA传输,如下图所示,是不是在AD的寄存器中只需要设置图中画红圈的那部分寄存器就可以了,图中其它部分的寄存器不需要设置了,是这样子吗,非常感谢!

祝您好心情!

  • 是的,您的理解是正确的。

    DMA的作用是在不影响CPU工作的前提下,搬移数据,所以当某触发源,如ADCINT1信号发生的时候,DMA机制就自动去搬移这些数据。具体使用的话,您可以参考附件内的代码

    //###########################################################################
    //
    // FILE:   adc_soc_continuous_dma_cpu01.c
    //
    // TITLE:  ADC continuous conversions read by DMA for F2837xD.
    //
    //! \addtogroup cpu01_example_list
    //! <h1> ADC Continuous Conversions Read by DMA (adc_soc_continuous_dma)</h1>
    //!
    //! This example sets up two ADC channels to convert simultaneously. The
    //! results will be transferred by the DMA into a buffer in RAM.
    //!
    //! After the program runs, the memory will contain:
    //!
    //! - \b adcData0 \b: a digital representation of the voltage on pin A3\n
    //! - \b adcData1 \b: a digital representation of the voltage on pin B3\n
    //!
    //
    //###########################################################################
    // $TI Release: F2837xD Support Library v3.03.00.00 $
    // $Release Date: Thu Dec  7 18:51:32 CST 2017 $
    // $Copyright:
    // Copyright (C) 2013-2017 Texas Instruments Incorporated - http://www.ti.com/
    //
    // Redistribution and use in source and binary forms, with or without
    // modification, are permitted provided that the following conditions
    // are met:
    //
    //   Redistributions of source code must retain the above copyright
    //   notice, this list of conditions and the following disclaimer.
    //
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the
    //   documentation and/or other materials provided with the
    //   distribution.
    //
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    //
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //###########################################################################
    
    //
    // Included Files
    //
    #include "F28x_Project.h"
    
    //
    // Function Prototypes
    //
    __interrupt void adca1_isr(void);
    __interrupt void dmach1_isr(void);
    
    void ConfigureEPWM(void);
    void ConfigureADC(void);
    void SetupADCContinuous(volatile struct ADC_REGS * adcRegs, Uint16 channel);
    void DMAInit(void);
    
    //
    // Defines
    //
    #define RESULTS_BUFFER_SIZE 1024    // Buffer for storing conversion results
                                        // (size must be multiple of 16)
    
    //
    // Globals
    //
    #pragma DATA_SECTION(adcData0, "ramgs0");
    #pragma DATA_SECTION(adcData1, "ramgs0");
    Uint16 adcData0[RESULTS_BUFFER_SIZE];
    Uint16 adcData1[RESULTS_BUFFER_SIZE];
    volatile Uint16 done;
    
    void main(void)
    {
        Uint16 resultsIndex;
    
    //
    // Step 1. Initialize System Control:
    // PLL, WatchDog, enable Peripheral Clocks
    // This example function is found in the F2837xD_SysCtrl.c file.
    //
        InitSysCtrl();
    
    //
    // Step 2. Initialize GPIO:
    // This example function is found in the F2837xD_Gpio.c file and
    // illustrates how to set the GPIO to it's default state.
    //
        InitGpio();
    
    //
    // Step 3. Clear all interrupts and initialize PIE vector table:
    // Disable CPU interrupts
    //
        DINT;
    
    //
    // Initialize the PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    // This function is found in the F2837xD_PieCtrl.c file.
    //
        InitPieCtrl();
    
    //
    // Disable CPU interrupts and clear all CPU interrupt flags:
    //
        IER = 0x0000;
        IFR = 0x0000;
    
    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example.  This is useful for debug purposes.
    // The shell ISR routines are found in F2837xD_DefaultIsr.c.
    // This function is found in F2837xD_PieVect.c.
    //
        InitPieVectTable();
    
    //
    // Set up ISRs used by this example
    //
    // ISR for ADCA INT1 - occurs after first conversion
    // ISR for DMA ch1 - occurs when DMA transfer is complete
    //
        EALLOW;
        PieVectTable.ADCA1_INT = &adca1_isr;
        PieVectTable.DMA_CH1_INT = &dmach1_isr;
        EDIS;
    
    //
    // Enable specific CPU interrupts: INT1 for ADCs and INT7 for DMA
    //
        IER |= M_INT1;
        IER |= M_INT7;
    
    //
    // Enable specific PIE interrupts
    //
    // ADCA INT1 - Group 1, interrupt 1
    // DMA interrupt - Group 7, interrupt 1
    //
        PieCtrlRegs.PIEIER1.bit.INTx1 = 1;
        PieCtrlRegs.PIEIER7.bit.INTx1 = 1;
    
    //
    // Stop the ePWM clock
    //
        EALLOW;
        CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0;
        EDIS;
    
    //
    // Call the set up function for ePWM 2
    //
        ConfigureEPWM();
    
    //
    // Start the ePWM clock
    //
        EALLOW;
        CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;
        EDIS;
    
    //
    // Configure the ADC and power it up
    //
        ConfigureADC();
    
    //
    // Setup the ADC for continuous conversions on channels A3 and B3
    //
        SetupADCContinuous(&AdcaRegs, 3);
        SetupADCContinuous(&AdcbRegs, 3);
    
    //
    // Initialize the DMA
    //
        DMAInit();
    
    //
    // Enable global Interrupts and higher priority real-time debug events:
    //
        EINT;  // Enable Global interrupt INTM
        ERTM;  // Enable Global realtime interrupt DBGM
    
    //
    // Initialize results buffer
    //
        for(resultsIndex = 0; resultsIndex < RESULTS_BUFFER_SIZE; resultsIndex++)
        {
            adcData0[resultsIndex] = 0;
            adcData1[resultsIndex] = 0;
        }
    
    //
    // Clearing all pending interrupt flags
    //
        EALLOW;
    
        DmaRegs.CH1.CONTROL.bit.PERINTCLR = 1;
        DmaRegs.CH2.CONTROL.bit.PERINTCLR = 1;
        AdcaRegs.ADCINTFLGCLR.all = 0x3;
        AdcbRegs.ADCINTFLGCLR.all = 0x3;
        EPwm2Regs.ETCNTINITCTL.bit.SOCAINITFRC = 1;
        EPwm2Regs.ETCLR.bit.SOCA = 1;
    
    //
    // Enable continuous operation by setting the last SOC to re-trigger the first
    //
        AdcaRegs.ADCINTSOCSEL1.bit.SOC0 = 2;
        AdcbRegs.ADCINTSOCSEL1.bit.SOC0 = 2;
    
        EDIS;
    
    //
    // Start DMA
    //
        done = 0;
        StartDMACH1();
        StartDMACH2();
    
    //
    // Finally, enable the SOCA trigger from ePWM. This will kick off
    // conversions at the next ePWM event.
    //
        EPwm2Regs.ETSEL.bit.SOCAEN = 1;
    
    //
    // Loop until the ISR signals the transfer is complete
    //
        while(done == 0)
        {
            __asm(" NOP");
        }
        ESTOP0;
    }
    
    //
    // adca1_isr - This is called after the very first conversion and will disable
    //             the ePWM SOC to avoid re-triggering problems.
    //
    #pragma CODE_SECTION(adca1_isr, ".TI.ramfunc");
    __interrupt void adca1_isr(void)
    {
        //
        // Remove ePWM trigger
        //
        EPwm2Regs.ETSEL.bit.SOCAEN = 0;
    
        //
        // Disable this interrupt from happening again
        //
        PieCtrlRegs.PIEIER1.bit.INTx1 = 0;
    
        //
        // Acknowledge
        //
        PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
    }
    
    //
    // dmach1_isr - This is called at the end of the DMA transfer, the conversions
    //              are stopped by removing the trigger of the first SOC from
    //              the last.
    //
    #pragma CODE_SECTION(dmach1_isr, ".TI.ramfunc");
    __interrupt void dmach1_isr(void)
    {
    //    //
    //    // Stop the ADC by removing the trigger for SOC0
    //    //
    //    EALLOW;
    //    AdcaRegs.ADCINTSOCSEL1.bit.SOC0 = 0;
    //    AdcbRegs.ADCINTSOCSEL1.bit.SOC0 = 0;
    //    EDIS;
    //
    //    done = 1;
    
        //
        // Acknowledge
        //
        PieCtrlRegs.PIEACK.all = PIEACK_GROUP7;
    }
    
    
    //
    // ConfigureEPWM - Set up the ePWM2 module so that the A output has a period
    //                 of 40us with a 50% duty. The SOCA signal is coincident with
    //                 the rising edge of this.
    //
    void ConfigureEPWM(void)
    {
        //
        // Make the timer count up with a period of 40us
        //
        EPwm2Regs.TBCTL.all = 0x0000;
        EPwm2Regs.TBPRD = 4000;
    
        //
        // Set the A output on zero and reset on CMPA
        //
        EPwm2Regs.AQCTLA.bit.ZRO = AQ_SET;
        EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR;
    
        //
        // Set CMPA to 20us to get a 50% duty
        //
        EPwm2Regs.CMPA.bit.CMPA = 2000;
    
        //
        // Start ADC when timer equals zero (note: don't enable yet)
        //
        EPwm2Regs.ETSEL.bit.SOCASEL = ET_CTR_ZERO;
        EPwm2Regs.ETPS.bit.SOCAPRD =  ET_1ST;
    
        //
        // Enable initialization of the SOCA event counter. Since we are
        // disabling the ETSEL.SOCAEN bit, we need a way to reset the SOCACNT.
        // Hence, enable the counter initialize control.
        //
        EPwm2Regs.ETCNTINITCTL.bit.SOCAINITEN = 1;
    }
    
    //
    // ConfigureADC - Write ADC configurations and power up the ADC for both
    //                ADC A and ADC B
    //
    void ConfigureADC(void)
    {
        EALLOW;
    
        //
        // Write prescale configurations
        //
        AdcaRegs.ADCCTL2.bit.PRESCALE = 6; // Set ADCCLK divider to /4
        AdcbRegs.ADCCTL2.bit.PRESCALE = 6;
    
        //
        // Set mode
        //
        AdcSetMode(ADC_ADCA, ADC_RESOLUTION_BF_12BIT, ADC_SIGNALMODE_SINGLE);
        AdcSetMode(ADC_ADCB, ADC_RESOLUTION_BF_12BIT, ADC_SIGNALMODE_SINGLE);
    
        //
        // Set pulse positions to late
        //
        AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1;
        AdcbRegs.ADCCTL1.bit.INTPULSEPOS = 1;
    
        //
        // Power up the ADC
        //
        AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1;
        AdcbRegs.ADCCTL1.bit.ADCPWDNZ = 1;
    
        //
        // Delay for 1ms to allow ADCs time to power up
        //
        DELAY_US(1000);
    
        EDIS;
    }
    
    //
    // SetupADCContinuous - setup the ADC to continuously convert on one channel
    //
    void SetupADCContinuous(volatile struct ADC_REGS * adcRegs, Uint16 channel)
    {
        Uint16 acqps;
    
        //
        // Determine minimum acquisition window (in SYSCLKS) based on resolution
        //
        if(ADC_RESOLUTION_BF_12BIT == AdcaRegs.ADCCTL2.bit.RESOLUTION)
        {
            acqps = 14; // 75ns
        }
        else // Resolution is 16-bit
        {
            acqps = 63; // 320ns
        }
    
        EALLOW;
    
        //
        // SOCs will convert on same specified channel
        //
        adcRegs->ADCSOC0CTL.bit.CHSEL  = channel;
        adcRegs->ADCSOC1CTL.bit.CHSEL  = channel;
        adcRegs->ADCSOC2CTL.bit.CHSEL  = channel;
        adcRegs->ADCSOC3CTL.bit.CHSEL  = channel;
        adcRegs->ADCSOC4CTL.bit.CHSEL  = channel;
        adcRegs->ADCSOC5CTL.bit.CHSEL  = channel;
        adcRegs->ADCSOC6CTL.bit.CHSEL  = channel;
        adcRegs->ADCSOC7CTL.bit.CHSEL  = channel;
        adcRegs->ADCSOC8CTL.bit.CHSEL  = channel;
        adcRegs->ADCSOC9CTL.bit.CHSEL  = channel;
        adcRegs->ADCSOC10CTL.bit.CHSEL = channel;
        adcRegs->ADCSOC11CTL.bit.CHSEL = channel;
        adcRegs->ADCSOC12CTL.bit.CHSEL = channel;
        adcRegs->ADCSOC13CTL.bit.CHSEL = channel;
        adcRegs->ADCSOC14CTL.bit.CHSEL = channel;
        adcRegs->ADCSOC15CTL.bit.CHSEL = channel;
    
        //
        // Sample window is acqps + 1 SYSCLK cycles
        //
        adcRegs->ADCSOC0CTL.bit.ACQPS  = acqps;
        adcRegs->ADCSOC1CTL.bit.ACQPS  = acqps;
        adcRegs->ADCSOC2CTL.bit.ACQPS  = acqps;
        adcRegs->ADCSOC3CTL.bit.ACQPS  = acqps;
        adcRegs->ADCSOC4CTL.bit.ACQPS  = acqps;
        adcRegs->ADCSOC5CTL.bit.ACQPS  = acqps;
        adcRegs->ADCSOC6CTL.bit.ACQPS  = acqps;
        adcRegs->ADCSOC7CTL.bit.ACQPS  = acqps;
        adcRegs->ADCSOC9CTL.bit.ACQPS  = acqps;
        adcRegs->ADCSOC10CTL.bit.ACQPS = acqps;
        adcRegs->ADCSOC11CTL.bit.ACQPS = acqps;
        adcRegs->ADCSOC12CTL.bit.ACQPS = acqps;
        adcRegs->ADCSOC13CTL.bit.ACQPS = acqps;
        adcRegs->ADCSOC14CTL.bit.ACQPS = acqps;
        adcRegs->ADCSOC15CTL.bit.ACQPS = acqps;
    
        //
        // Trigger SCO0 from EPWM2SOCA
        //
        adcRegs->ADCSOC0CTL.bit.TRIGSEL = 7;
    
        //
        // Trigger all other SOCs from INT1 (EOC on SOC0)
        //
        adcRegs->ADCINTSOCSEL1.bit.SOC1 = 1;
        adcRegs->ADCINTSOCSEL1.bit.SOC2 = 1;
        adcRegs->ADCINTSOCSEL1.bit.SOC3 = 1;
        adcRegs->ADCINTSOCSEL1.bit.SOC4 = 1;
        adcRegs->ADCINTSOCSEL1.bit.SOC5 = 1;
        adcRegs->ADCINTSOCSEL1.bit.SOC6 = 1;
        adcRegs->ADCINTSOCSEL1.bit.SOC7 = 1;
        adcRegs->ADCINTSOCSEL2.bit.SOC8 = 1;
        adcRegs->ADCINTSOCSEL2.bit.SOC9 = 1;
        adcRegs->ADCINTSOCSEL2.bit.SOC10 = 1;
        adcRegs->ADCINTSOCSEL2.bit.SOC11 = 1;
        adcRegs->ADCINTSOCSEL2.bit.SOC12 = 1;
        adcRegs->ADCINTSOCSEL2.bit.SOC13 = 1;
        adcRegs->ADCINTSOCSEL2.bit.SOC14 = 1;
        adcRegs->ADCINTSOCSEL2.bit.SOC15 = 1;
    
        adcRegs->ADCINTSEL1N2.bit.INT1E = 1;    // Enable INT1 flag
        adcRegs->ADCINTSEL1N2.bit.INT2E = 1;    // Enable INT2 flag
        adcRegs->ADCINTSEL3N4.bit.INT3E = 0;    // Disable INT3 flag
        adcRegs->ADCINTSEL3N4.bit.INT4E = 0;    // Disable INT4 flag
    
        adcRegs->ADCINTSEL1N2.bit.INT1CONT = 1;
        adcRegs->ADCINTSEL1N2.bit.INT2CONT = 1;
    
        adcRegs->ADCINTSEL1N2.bit.INT1SEL = 0;  // End of SOC0
        adcRegs->ADCINTSEL1N2.bit.INT2SEL = 15; // End of SOC15
    
        EDIS;
    }
    
    //
    // DMAInit - Initialize DMA ch 1 to transfer ADCA results and DMA ch 2 to
    //           transfer ADCB results
    //
    void DMAInit(void)
    {
        //
        // Initialize DMA
        //
        DMAInitialize();
    
        //
        // DMA set up for first ADC
        //
        DMACH1AddrConfig(adcData0, &AdcaResultRegs.ADCRESULT0);
    
        //
        // Perform enough 16-word bursts to fill the results buffer. Data will be
        // transferred 32 bits at a time hence the address steps below.
        //
        // Enable the DMA channel 1 interrupt
        //
        DMACH1BurstConfig(15, 2, 2);
        DMACH1TransferConfig((RESULTS_BUFFER_SIZE >> 4) - 1, -14, 2);
        DMACH1ModeConfig(
                            DMA_ADCAINT2,
                            PERINT_ENABLE,
                            ONESHOT_DISABLE,
                            CONT_ENABLE,
                            SYNC_DISABLE,
                            SYNC_SRC,
                            OVRFLOW_DISABLE,
                            THIRTYTWO_BIT,
                            CHINT_END,
                            CHINT_ENABLE
                        );
    
        /*
         * void DMACH1ModeConfig(Uint16 persel, Uint16 perinte, Uint16 oneshot,
                          Uint16 cont, Uint16 synce, Uint16 syncsel,
                          Uint16 ovrinte, Uint16 datasize, Uint16 chintmode,
                          Uint16 chinte)
         */
    
        //
        // DMA set up for second ADC
        //
        DMACH2AddrConfig(adcData1, &AdcbResultRegs.ADCRESULT0);
    
        //
        // Perform enough 16-word bursts to fill the results buffer. Data will be
        // transferred 32 bits at a time hence the address steps below.
        //
        DMACH2BurstConfig(15, 2, 2);
        DMACH2TransferConfig((RESULTS_BUFFER_SIZE >> 4) - 1, -14, 2);
        DMACH2ModeConfig(
                            DMA_ADCAINT2,
                            PERINT_ENABLE,
                            ONESHOT_DISABLE,
                            CONT_ENABLE,
                            SYNC_DISABLE,
                            SYNC_SRC,
                            OVRFLOW_DISABLE,
                            THIRTYTWO_BIT,
                            CHINT_END,
                            CHINT_DISABLE
                        );
    }
    
    //
    // End of file
    //
    

  • 不知您现在使用的具体芯片型号是什么?您可以在对应的用户指南中找到DMA需要设置的部分
  • 谢谢Yang工的回复,我现在用的是28375S

    因为发现文档中只是说了DMA的触发源,但是好像并没有明确指出触发源是哪一个标志位,所以以后点搞不清楚。例如DMA章节中只是说有ADCA.1这个触发源,我结合Figure 5-1知道了这个触发源其实指的是ADC INT1。但是并没有告诉我触发源是不是就是INT1的中断标志位。我猜想是不是就是那个标志位。那是不是说如果触发源是中断标志位,那我就可以标志位的寄存器去触发DMA的传输呢?  谢谢杨工!

    祝您好心情!

  • 谢谢您对TI产品的关注!

    若是后续有其他问题,您可以在论坛直接发新帖,我们会在第一时间为您解决
  • 谢谢Yang工的回复,我现在用的是28375S

    因为发现文档中只是说了DMA的触发源,但是好像并没有明确指出触发源是哪一个标志位,所以以后点搞不清楚。例如DMA章节中只是说有ADCA.1这个触发源,我结合Figure 5-1知道了这个触发源其实指的是ADC INT1。但是并没有告诉我触发源是不是就是INT1的中断标志位。我猜想是不是就是那个标志位。那是不是说如果触发源是中断标志位,那我就可以标志位的寄存器去触发DMA的传输呢? 谢谢杨工!

    祝您好心情