This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于C2000gang使用问题咨询

Other Parts Discussed in Thread: C2000-GANG, CCSTUDIO, UNIFLASH

我们公司一直使用C2000配合CCS_3.3烧录DSP文件,使用流程是用SD_FLASH开打Project,将后缀.SDP的脚本文件打开,脚本中有指向烧录文件的.OUT路径,点击flash 就直接烧录成功了,这次买了新的烧录器,买的是C2000GANG,使用发现遇到了问题,请求各位大佬帮忙解决一下 ,谢谢。

我在官网 下载了C2000gang program,驱动也安装了,但是没有使用过这个软件,在添加脚本里面没办法添加后缀.SDP的脚本,添加image也没办法添加后缀.OUT的文件,按照老的方法,使用ccs_3.3 ,没有办法进行烧录

本人对这方面没什么基础,只是想简单使用,能不能有大神帮忙解决一下,新买的怎么联系TI的技术支持。

 _

使用需要c2000gang机器上设置什么吗?我都无法确定他的好坏

  • 请问您现在是购买了C2000-GANG并下载了下面链接内的C2000 Gang Programmer Support Software - From Elprotronics, Inc.?具体的芯片型号是什么?您是想批量烧录?

    www.ti.com/.../C2000-GANG

    能否给出您烧录的相关错误信息或者截图呢?

    另外若是可以的话,建议您后续使用新版的CCS,更新和优化了很多功能
  • 目前只想单个烧录,;芯片型号  TI320C28xx,请问一下CCS哪个版本能够加载.SDP  ;.OUT的文件呢??C2000gang可以使CCStudio_v3.3烧录吗??是否会不兼容

  • 1 若是只是想单独烧录而且您没有购买C200gang的话,您可以不需要购买C200gang,毕竟对您的应用来说,性价比不高

    2 烧录单个芯片的话,软件上您可以使用CCS,也可以使用独立的uniflash等

    www.ti.com/.../UNIFLASH

    3 若是可以的话,强烈不建议使用CCS3.3,毕竟太老了

    software-dl.ti.com/.../ccs_downloads.html
  • 没看到有CCS版本的要求,只要生出的.out就应该没问题
    建议你通过TI提供的GUI控制操作实时
  • TI 提供的GUI里面 无法烧录.OUT的文件, 可能是我不太会用,能不能教一下,自带的是C2000gang program
  • 已经买了,。。。发现不会用,这是最尴尬的, TI有没有提供一下电话或者远程指导的服务- -
  • 怎么才能确定c2000gang和电脑正常连接了,还有驱动是正常的、
  • 您可以继续在论坛发帖,我们会全力支持。您也可以在英文论坛发帖询问 https://e2e.ti.com/
  • 不知您是否参考过

    www.ti.com.cn/.../spruhs0c.pdf

    理论上您电脑的设备管理器中应该会显示出该设备

    Connect the C2000 Gang Programmer hardware to a computer's USB port using a USB A-B cable.

    The C2000 Gang Programmer's internals can be supplied from the computer's USB port (5 V, 0.5 A),but an external power supply is needed for programming target devices. Target devices can be powered independently or from the C2000 Gang Programmer's 6-10V power supply connector. In this case the external power supply must provide a voltage between 6 V and 10 V DC and must be capable of providing a minimum current of 1.5 A. The center post of the power supply connector on the C2000 Gang Programmer is the positive-voltage terminal. The programmer indicates the status of the power supply connection by using system LEDs and the LCD back light. The programmer can also be
    connected to a serial port (COM1 to COM255) using a 9-pin Sub-D connector, if the computer does not have a USB port.
  • 不知道我理解的对不对, 我之前用C2000的时候, 整块板我是直接外接了24V电源的, 现在用C2000gang我还需要同时接上配件里所带的充电器吗?我从说明上字面理解是不需要, 再者还有个问题就是我只用 一号口烧录, 我应该不需要把其他接口的接头都插上把 ,说明里没有 详细的说 ;我看TI官网介绍说C2000gang 兼容 现在和未来所有的C2000,我才买的,ε=(´ο`*)))唉,我不群烧,感觉买了多此一举了
  • 我私信您了,您查看一下消息,谢谢