This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

f28335 can 無法互傳



我想做到連續a傳b 但是做不到

//###########################################################################
// Description:
//! \addtogroup f2833x_example_list
//! <h1>eCAN back to back (ecan_back2back)</h1>
//!
//! This example tests eCAN by transmitting data back-to-back at high speed
//! without stopping. The received data is verified. Any error is flagged.
//! MBX0 transmits to MBX16, MBX1 transmits to MBX17 and so on.... \n
//! This program illustrates the use of self-test mode
//!
//! This example uses the self-test mode of the CAN module. i.e. the
//! transmission/reception happens within the module itself (even the required
//! ACKnowldege is generated internally in the module). Therefore, there is no
//! need for a CAN transceiver to run this particular test case and no activity
//! will be seen in the CAN pins/bus. Because everything is internal, there is
//! no need for a 120-ohm termination resistor. Note that a real-world CAN
//! application needs a CAN transceiver and termination resistors on both ends
//! of the bus.
//!
//! \b Watch \b Variables \n
//! - PassCount
//! - ErrorCount
//! - MessageReceivedCount
//
//
//###########################################################################
// $TI Release: F2833x/F2823x Header Files and Peripheral Examples V142 $
// $Release Date: November  1, 2016 $
// $Copyright: Copyright (C) 2007-2016 Texas Instruments Incorporated -
//             www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################

#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File

// Prototype statements for functions found within this file.

void mailbox_check(int32 T1, int32 T2, int32 T3);
void mailbox_read(int16 i);
void Canb_config(void);
// Global variable for this example
Uint32  ErrorCount;
Uint32  PassCount;
Uint32  MessageReceivedCount;
long      loopcount = 0;
Uint32  TestMbox1 = 0;
Uint32  TestMbox2 = 0;
Uint32  TestMbox3 = 0;
extern void test(void);
void main(void)
{
    Uint16  j;
    test();
// eCAN control registers require read/write access using 32-bits.  Thus we
// will create a set of shadow registers for this example.  These shadow
// registers will be used to make sure the access is 32-bits and not 16.
   struct ECAN_REGS ECanaShadow;

// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2833x_SysCtrl.c file.
   InitSysCtrl();

// Step 2. Initialize GPIO:
// This example function is found in the DSP2833x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio();  // Skipped for this example

// For this example, configure CAN pins using GPIO regs here
// This function is found in DSP2833x_ECan.c
   InitECanGpio();

// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
   DINT;

// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2833x_PieCtrl.c file.
   InitPieCtrl();

// Disable CPU interrupts and clear all CPU interrupt flags:
   IER = 0x0000;
   IFR = 0x0000;

// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in DSP2833x_DefaultIsr.c.
// This function is found in DSP2833x_PieVect.c.
   InitPieVectTable();
   InitECan();
// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP2833x_InitPeripherals.c
// InitPeripherals(); // Not required for this example

// Step 5. User specific code, enable interrupts:

    MessageReceivedCount = 0;
    ErrorCount = 0;
    PassCount = 0;

    
    // Mailboxes can be written to 16-bits or 32-bits at a time
    // Write to the MSGID field of TRANSMIT mailboxes MBOX0 - 15


    ECanaMboxes.MBOX0.MSGID.all = 0x00000000;
    ECanaMboxes.MBOX1.MSGID.all = 0x00000001;
    ECanaMboxes.MBOX2.MSGID.all = 0x00000002;
    ECanaMboxes.MBOX3.MSGID.all = 0x00000003;
    ECanaMboxes.MBOX4.MSGID.all = 0x00000004;
    ECanaMboxes.MBOX5.MSGID.all = 0x00000005;
    ECanaMboxes.MBOX6.MSGID.all = 0x00000006;
    ECanaMboxes.MBOX7.MSGID.all = 0x00000007;
    ECanaMboxes.MBOX8.MSGID.all = 0x00000008;
    ECanaMboxes.MBOX9.MSGID.all = 0x00000009;
    ECanaMboxes.MBOX10.MSGID.all = 0x0000000A;
    ECanaMboxes.MBOX11.MSGID.all = 0x0000000B;
    ECanaMboxes.MBOX12.MSGID.all = 0x0000000C;
    ECanaMboxes.MBOX13.MSGID.all = 0x0000000D;
    ECanaMboxes.MBOX14.MSGID.all = 0x0000000E;
    ECanaMboxes.MBOX15.MSGID.all = 0x0000000F;

    // Configure Mailboxes 0-15 as Tx, 16-31 as Rx
    // Since this write is to the entire register (instead of a bit
    // field) a shadow register is not required.
    ECanaRegs.CANMD.all = 0xFFFF0000;// 0-15tx 16-31rx

    // Enable all Mailboxes */
    // Since this write is to the entire register (instead of a bit
    // field) a shadow register is not required.
    ECanaRegs.CANME.all = 0x0000FFFF;

    // Specify that 8 bits will be sent/received
    ECanaMboxes.MBOX0.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX1.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX2.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX3.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX4.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX5.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX6.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX7.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX8.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX9.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX10.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX11.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX12.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX13.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX14.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX15.MSGCTRL.bit.DLC = 8;


    // Write to the mailbox RAM field of MBOX0 - 15
    ECanaMboxes.MBOX0.MDL.all = 0x9555AAA0;
    ECanaMboxes.MBOX0.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX1.MDL.all = 0x9555AAA1;
    ECanaMboxes.MBOX1.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX2.MDL.all = 0x9555AAA2;
    ECanaMboxes.MBOX2.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX3.MDL.all = 0x9555AAA3;
    ECanaMboxes.MBOX3.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX4.MDL.all = 0x9555AAA4;
    ECanaMboxes.MBOX4.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX5.MDL.all = 0x9555AAA5;
    ECanaMboxes.MBOX5.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX6.MDL.all = 0x9555AAA6;
    ECanaMboxes.MBOX6.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX7.MDL.all = 0x9555AAA7;
    ECanaMboxes.MBOX7.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX8.MDL.all = 0x9555AAA8;
    ECanaMboxes.MBOX8.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX9.MDL.all = 0x9555AAA9;
    ECanaMboxes.MBOX9.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX10.MDL.all = 0x9555AAAA;
    ECanaMboxes.MBOX10.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX11.MDL.all = 0x9555AAAB;
    ECanaMboxes.MBOX11.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX12.MDL.all = 0x9555AAAC;
    ECanaMboxes.MBOX12.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX13.MDL.all = 0x9555AAAD;
    ECanaMboxes.MBOX13.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX14.MDL.all = 0x9555AAAE;
    ECanaMboxes.MBOX14.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX15.MDL.all = 0x9555AAAF;
    ECanaMboxes.MBOX15.MDH.all = 0x89ABCDEF;

    // Since this write is to the entire register (instead of a bit
    // field) a shadow register is not required.
    EALLOW;
    ECanaRegs.CANMIM.all = 0x0000FFFF;
    ECanbRegs.CANMIM.all = 0xFFFF0000;
    EDIS;
    // Configure the eCAN for self test mode
    // Enable the enhanced features of the eCAN.
    /*EALLOW;
    ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
    ECanaShadow.CANMC.bit.STM = 0;    // Configure CAN for self-test mode
    ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
    EDIS;*/
    Canb_config();
    // Begin transmitting
    for(;;)
    {

       ECanaRegs.CANTRS.all = 0x0000FFFF;  // Set TRS for all transmit mailboxes
       while(ECanaRegs.CANTA.all != 0x0000FFFF ) {}  // Wait for all TAn bits to be set..
       ECanaRegs.CANTA.all = 0x0000FFFF;   // Clear all TAn
       MessageReceivedCount++;

       //Read from Receive mailboxes and begin checking for data */
       for(j=16; j<32; j++)         // Read & check 16 mailboxes
       {
          mailbox_read(j);         // This func reads the indicated mailbox data
          mailbox_check(TestMbox1,TestMbox2,TestMbox3); // Checks the received data
       }
       loopcount++;
    }
    __asm(" ESTOP0");  // Stop here
}
void test(void)
{loopcount=2567809;}
// This function reads out the contents of the indicated
// by the Mailbox number (MBXnbr).
void mailbox_read(int16 MBXnbr)
{
   volatile struct MBOX *Mailbox;
   Mailbox = &ECanaMboxes.MBOX0 + MBXnbr;
   TestMbox1 = Mailbox->MDL.all; // = 0x9555AAAn (n is the MBX number)
   TestMbox2 = Mailbox->MDH.all; // = 0x89ABCDEF (a constant)
   TestMbox3 = Mailbox->MSGID.all;// = 0x9555AAAn (n is the MBX number)

} // MSGID of a rcv MBX is transmitted as the MDL data.

void mailbox_check(int32 T1, int32 T2, int32 T3)
{
    if((T1 != T3) || ( T2 != 0x89ABCDEF))
    {
       ErrorCount++;
    }
    else
    {
       PassCount++;

    }
}
void Canb_config(void){
    struct ECAN_REGS ECanbShadow;
    // Write to the MSGID field of RECEIVE mailboxes MBOX16 - 31
    ECanbMboxes.MBOX16.MSGID.all = 0x00000000;
    ECanbMboxes.MBOX17.MSGID.all = 0x00000001;
    ECanbMboxes.MBOX18.MSGID.all = 0x00000002;
    ECanbMboxes.MBOX19.MSGID.all = 0x00000003;
    ECanbMboxes.MBOX20.MSGID.all = 0x00000004;
    ECanbMboxes.MBOX21.MSGID.all = 0x00000005;
    ECanbMboxes.MBOX22.MSGID.all = 0x00000006;
    ECanbMboxes.MBOX23.MSGID.all = 0x00000007;
    ECanbMboxes.MBOX24.MSGID.all = 0x00000008;
    ECanbMboxes.MBOX25.MSGID.all = 0x00000009;
    ECanbMboxes.MBOX26.MSGID.all = 0x0000000A;
    ECanbMboxes.MBOX27.MSGID.all = 0x0000000B;
    ECanbMboxes.MBOX28.MSGID.all = 0x0000000C;
    ECanbMboxes.MBOX29.MSGID.all = 0x0000000D;
    ECanbMboxes.MBOX30.MSGID.all = 0x0000000E;
    ECanbMboxes.MBOX31.MSGID.all = 0x0000000F;


    ECanbRegs.CANME.all = 0xFFFF0000;
    ECanbRegs.CANMD.all = 0xFFFF0000;// 0-15tx 16-31rx

    ECanbMboxes.MBOX16.MSGCTRL.bit.DLC = 8;
    ECanbMboxes.MBOX17.MSGCTRL.bit.DLC = 8;
    ECanbMboxes.MBOX18.MSGCTRL.bit.DLC = 8;
    ECanbMboxes.MBOX19.MSGCTRL.bit.DLC = 8;
    ECanbMboxes.MBOX20.MSGCTRL.bit.DLC = 8;
    ECanbMboxes.MBOX21.MSGCTRL.bit.DLC = 8;
    ECanbMboxes.MBOX22.MSGCTRL.bit.DLC = 8;
    ECanbMboxes.MBOX23.MSGCTRL.bit.DLC = 8;
    ECanbMboxes.MBOX24.MSGCTRL.bit.DLC = 8;
    ECanbMboxes.MBOX25.MSGCTRL.bit.DLC = 8;
    ECanbMboxes.MBOX26.MSGCTRL.bit.DLC = 8;
    ECanbMboxes.MBOX27.MSGCTRL.bit.DLC = 8;
    ECanbMboxes.MBOX28.MSGCTRL.bit.DLC = 8;
    ECanbMboxes.MBOX29.MSGCTRL.bit.DLC = 8;
    ECanbMboxes.MBOX30.MSGCTRL.bit.DLC = 8;
    ECanbMboxes.MBOX31.MSGCTRL.bit.DLC = 8;

}

//===========================================================================
// No more.
//===========================================================================