我想做到連續a傳b 但是做不到
//###########################################################################
// Description:
//! \addtogroup f2833x_example_list
//! <h1>eCAN back to back (ecan_back2back)</h1>
//!
//! This example tests eCAN by transmitting data back-to-back at high speed
//! without stopping. The received data is verified. Any error is flagged.
//! MBX0 transmits to MBX16, MBX1 transmits to MBX17 and so on.... \n
//! This program illustrates the use of self-test mode
//!
//! This example uses the self-test mode of the CAN module. i.e. the
//! transmission/reception happens within the module itself (even the required
//! ACKnowldege is generated internally in the module). Therefore, there is no
//! need for a CAN transceiver to run this particular test case and no activity
//! will be seen in the CAN pins/bus. Because everything is internal, there is
//! no need for a 120-ohm termination resistor. Note that a real-world CAN
//! application needs a CAN transceiver and termination resistors on both ends
//! of the bus.
//!
//! \b Watch \b Variables \n
//! - PassCount
//! - ErrorCount
//! - MessageReceivedCount
//
//
//###########################################################################
// $TI Release: F2833x/F2823x Header Files and Peripheral Examples V142 $
// $Release Date: November 1, 2016 $
// $Copyright: Copyright (C) 2007-2016 Texas Instruments Incorporated -
// www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
// Prototype statements for functions found within this file.
void mailbox_check(int32 T1, int32 T2, int32 T3);
void mailbox_read(int16 i);
void Canb_config(void);
// Global variable for this example
Uint32 ErrorCount;
Uint32 PassCount;
Uint32 MessageReceivedCount;
long loopcount = 0;
Uint32 TestMbox1 = 0;
Uint32 TestMbox2 = 0;
Uint32 TestMbox3 = 0;
extern void test(void);
void main(void)
{
Uint16 j;
test();
// eCAN control registers require read/write access using 32-bits. Thus we
// will create a set of shadow registers for this example. These shadow
// registers will be used to make sure the access is 32-bits and not 16.
struct ECAN_REGS ECanaShadow;
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2833x_SysCtrl.c file.
InitSysCtrl();
// Step 2. Initialize GPIO:
// This example function is found in the DSP2833x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio(); // Skipped for this example
// For this example, configure CAN pins using GPIO regs here
// This function is found in DSP2833x_ECan.c
InitECanGpio();
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;
// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2833x_PieCtrl.c file.
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in DSP2833x_DefaultIsr.c.
// This function is found in DSP2833x_PieVect.c.
InitPieVectTable();
InitECan();
// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP2833x_InitPeripherals.c
// InitPeripherals(); // Not required for this example
// Step 5. User specific code, enable interrupts:
MessageReceivedCount = 0;
ErrorCount = 0;
PassCount = 0;
// Mailboxes can be written to 16-bits or 32-bits at a time
// Write to the MSGID field of TRANSMIT mailboxes MBOX0 - 15
ECanaMboxes.MBOX0.MSGID.all = 0x00000000;
ECanaMboxes.MBOX1.MSGID.all = 0x00000001;
ECanaMboxes.MBOX2.MSGID.all = 0x00000002;
ECanaMboxes.MBOX3.MSGID.all = 0x00000003;
ECanaMboxes.MBOX4.MSGID.all = 0x00000004;
ECanaMboxes.MBOX5.MSGID.all = 0x00000005;
ECanaMboxes.MBOX6.MSGID.all = 0x00000006;
ECanaMboxes.MBOX7.MSGID.all = 0x00000007;
ECanaMboxes.MBOX8.MSGID.all = 0x00000008;
ECanaMboxes.MBOX9.MSGID.all = 0x00000009;
ECanaMboxes.MBOX10.MSGID.all = 0x0000000A;
ECanaMboxes.MBOX11.MSGID.all = 0x0000000B;
ECanaMboxes.MBOX12.MSGID.all = 0x0000000C;
ECanaMboxes.MBOX13.MSGID.all = 0x0000000D;
ECanaMboxes.MBOX14.MSGID.all = 0x0000000E;
ECanaMboxes.MBOX15.MSGID.all = 0x0000000F;
// Configure Mailboxes 0-15 as Tx, 16-31 as Rx
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
ECanaRegs.CANMD.all = 0xFFFF0000;// 0-15tx 16-31rx
// Enable all Mailboxes */
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
ECanaRegs.CANME.all = 0x0000FFFF;
// Specify that 8 bits will be sent/received
ECanaMboxes.MBOX0.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX1.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX2.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX3.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX4.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX5.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX6.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX7.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX8.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX9.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX10.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX11.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX12.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX13.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX14.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX15.MSGCTRL.bit.DLC = 8;
// Write to the mailbox RAM field of MBOX0 - 15
ECanaMboxes.MBOX0.MDL.all = 0x9555AAA0;
ECanaMboxes.MBOX0.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX1.MDL.all = 0x9555AAA1;
ECanaMboxes.MBOX1.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX2.MDL.all = 0x9555AAA2;
ECanaMboxes.MBOX2.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX3.MDL.all = 0x9555AAA3;
ECanaMboxes.MBOX3.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX4.MDL.all = 0x9555AAA4;
ECanaMboxes.MBOX4.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX5.MDL.all = 0x9555AAA5;
ECanaMboxes.MBOX5.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX6.MDL.all = 0x9555AAA6;
ECanaMboxes.MBOX6.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX7.MDL.all = 0x9555AAA7;
ECanaMboxes.MBOX7.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX8.MDL.all = 0x9555AAA8;
ECanaMboxes.MBOX8.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX9.MDL.all = 0x9555AAA9;
ECanaMboxes.MBOX9.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX10.MDL.all = 0x9555AAAA;
ECanaMboxes.MBOX10.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX11.MDL.all = 0x9555AAAB;
ECanaMboxes.MBOX11.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX12.MDL.all = 0x9555AAAC;
ECanaMboxes.MBOX12.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX13.MDL.all = 0x9555AAAD;
ECanaMboxes.MBOX13.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX14.MDL.all = 0x9555AAAE;
ECanaMboxes.MBOX14.MDH.all = 0x89ABCDEF;
ECanaMboxes.MBOX15.MDL.all = 0x9555AAAF;
ECanaMboxes.MBOX15.MDH.all = 0x89ABCDEF;
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
EALLOW;
ECanaRegs.CANMIM.all = 0x0000FFFF;
ECanbRegs.CANMIM.all = 0xFFFF0000;
EDIS;
// Configure the eCAN for self test mode
// Enable the enhanced features of the eCAN.
/*EALLOW;
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.STM = 0; // Configure CAN for self-test mode
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
EDIS;*/
Canb_config();
// Begin transmitting
for(;;)
{
ECanaRegs.CANTRS.all = 0x0000FFFF; // Set TRS for all transmit mailboxes
while(ECanaRegs.CANTA.all != 0x0000FFFF ) {} // Wait for all TAn bits to be set..
ECanaRegs.CANTA.all = 0x0000FFFF; // Clear all TAn
MessageReceivedCount++;
//Read from Receive mailboxes and begin checking for data */
for(j=16; j<32; j++) // Read & check 16 mailboxes
{
mailbox_read(j); // This func reads the indicated mailbox data
mailbox_check(TestMbox1,TestMbox2,TestMbox3); // Checks the received data
}
loopcount++;
}
__asm(" ESTOP0"); // Stop here
}
void test(void)
{loopcount=2567809;}
// This function reads out the contents of the indicated
// by the Mailbox number (MBXnbr).
void mailbox_read(int16 MBXnbr)
{
volatile struct MBOX *Mailbox;
Mailbox = &ECanaMboxes.MBOX0 + MBXnbr;
TestMbox1 = Mailbox->MDL.all; // = 0x9555AAAn (n is the MBX number)
TestMbox2 = Mailbox->MDH.all; // = 0x89ABCDEF (a constant)
TestMbox3 = Mailbox->MSGID.all;// = 0x9555AAAn (n is the MBX number)
} // MSGID of a rcv MBX is transmitted as the MDL data.
void mailbox_check(int32 T1, int32 T2, int32 T3)
{
if((T1 != T3) || ( T2 != 0x89ABCDEF))
{
ErrorCount++;
}
else
{
PassCount++;
}
}
void Canb_config(void){
struct ECAN_REGS ECanbShadow;
// Write to the MSGID field of RECEIVE mailboxes MBOX16 - 31
ECanbMboxes.MBOX16.MSGID.all = 0x00000000;
ECanbMboxes.MBOX17.MSGID.all = 0x00000001;
ECanbMboxes.MBOX18.MSGID.all = 0x00000002;
ECanbMboxes.MBOX19.MSGID.all = 0x00000003;
ECanbMboxes.MBOX20.MSGID.all = 0x00000004;
ECanbMboxes.MBOX21.MSGID.all = 0x00000005;
ECanbMboxes.MBOX22.MSGID.all = 0x00000006;
ECanbMboxes.MBOX23.MSGID.all = 0x00000007;
ECanbMboxes.MBOX24.MSGID.all = 0x00000008;
ECanbMboxes.MBOX25.MSGID.all = 0x00000009;
ECanbMboxes.MBOX26.MSGID.all = 0x0000000A;
ECanbMboxes.MBOX27.MSGID.all = 0x0000000B;
ECanbMboxes.MBOX28.MSGID.all = 0x0000000C;
ECanbMboxes.MBOX29.MSGID.all = 0x0000000D;
ECanbMboxes.MBOX30.MSGID.all = 0x0000000E;
ECanbMboxes.MBOX31.MSGID.all = 0x0000000F;
ECanbRegs.CANME.all = 0xFFFF0000;
ECanbRegs.CANMD.all = 0xFFFF0000;// 0-15tx 16-31rx
ECanbMboxes.MBOX16.MSGCTRL.bit.DLC = 8;
ECanbMboxes.MBOX17.MSGCTRL.bit.DLC = 8;
ECanbMboxes.MBOX18.MSGCTRL.bit.DLC = 8;
ECanbMboxes.MBOX19.MSGCTRL.bit.DLC = 8;
ECanbMboxes.MBOX20.MSGCTRL.bit.DLC = 8;
ECanbMboxes.MBOX21.MSGCTRL.bit.DLC = 8;
ECanbMboxes.MBOX22.MSGCTRL.bit.DLC = 8;
ECanbMboxes.MBOX23.MSGCTRL.bit.DLC = 8;
ECanbMboxes.MBOX24.MSGCTRL.bit.DLC = 8;
ECanbMboxes.MBOX25.MSGCTRL.bit.DLC = 8;
ECanbMboxes.MBOX26.MSGCTRL.bit.DLC = 8;
ECanbMboxes.MBOX27.MSGCTRL.bit.DLC = 8;
ECanbMboxes.MBOX28.MSGCTRL.bit.DLC = 8;
ECanbMboxes.MBOX29.MSGCTRL.bit.DLC = 8;
ECanbMboxes.MBOX30.MSGCTRL.bit.DLC = 8;
ECanbMboxes.MBOX31.MSGCTRL.bit.DLC = 8;
}
//===========================================================================
// No more.
//===========================================================================