This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用CCS9打开control suite例程报错



Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed - 6.2.9 [C2000]. See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update. Visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest compiler support. Or <a href="software-dl.ti.com/.../a> and install the compiler, then register it with CCS through 'Preferences > CCS > Build > Compilers'. Example_2833xEPwmUpDownAQ properties Problem

按照步骤并没有找到select 'Code Generation Tools Updates'