Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed - 6.2.9 [C2000]. See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update. Visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest compiler support. Or <a href="software-dl.ti.com/.../a> and install the compiler, then register it with CCS through 'Preferences > CCS > Build > Compilers'. Example_2833xEPwmUpDownAQ properties Problem
按照步骤并没有找到select 'Code Generation Tools Updates'