This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D 将程序烧写进FLASH里面,运行时将其中一个函数拷贝到RAM里面运行,程序跑飞了Interrupt_illegalOperationHandler



#ifdef __cplusplus
#pragma CODE_SECTION(".TI.ramfunc");
#endif

void epwm1_isr_func(void) 

这是我要拷贝到RAM里面跑的函数,这个函数是在EPWM1中断里面调用,我尝试过在main函数里面调用,都会进入Interrupt_illegalOperationHandler这个里面。

#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
#if defined(__TI_EABI__)
.TI.ramfunc : {} LOAD = FLASHD,
RUN = RAMLS0| RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#else
.TI.ramfunc : {} LOAD = FLASHD,
RUN = RAMLS0| RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#endif
#else
ramfuncs : LOAD = FLASHD,
RUN = RAMLS0| RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#endif

这是拷贝用的CMD文件部分。

CCS还会返回这个提醒 Break at address "0x0" with no debug information available, or outside of program code.