This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TMS320F28335的电源

Other Parts Discussed in Thread: TMS320F28335

请问

TMS320F28335的电源有无上电顺序的要求,就如同F2812先3.3后1.9?

再有F2812同时上电了,会产生什么问题,GPIO端口在同时上电的瞬间电平是什么状态,是高是低还是高阻态?

F28335上电瞬间GPIO状态会怎样?请教了,谢谢!

  •  

    下面是28335 数据手册127页的说明。对于28335来说建议先上VDD,后上VDDIO。如果满足这个条件GPIO会是默认的输入状态。这时候如果有外部上拉或下拉

    GPIO的电平会被拉倒相应的点平,如果外部没有上拉。要查GPIO Port x Pullup Disable (GPxPUD) Registers,看默认是不是内部上拉。

    6.8 Power Sequencing

    No requirements are placed on the power up/down sequence of the various power pins to ensure the
    correct reset state for all the modules. However, if the 3.3-V transistors in the level shifting output buffers
    of the I/O pins are powered prior to the 1.9-V transistors, it is possible for the output buffers to turn on,
    causing a glitch to occur on the pin during power up. To avoid this behavior, power the VDD pins prior to or
    simultaneously with the VDDIO pins, ensuring that the VDD pins have reached 0.7 V before the VDDIO pins
    reach 0.7 V.