This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049:CAN中断接收

Other Parts Discussed in Thread: TMS320F280049

你好:

      我现在在使用TMS320F280049例程can_ex2_loopback_interrupts测试CAN中断接收。看到例程使用的是CAN_INT_IE0,我想把其修改为CAN_INT_IE1,我做了如下的程序修改:

CAN_enableInterrupt(CANA_BASE, CAN_INT_IE1);

 Interrupt_register(INT_CANA1, &canISR);

Interrupt_enable(INT_CANA1);
CAN_enableGlobalInterrupt(CANA_BASE, CAN_GLOBAL_INT_CANINT1);

canISR中断函数中修改CAN_clearGlobalInterruptStatus(CANA_BASE, CAN_GLOBAL_INT_CANINT1);

然后,我进行测试发现接收数据未进入到中断里。请问,我还需要修改哪些地方

  • 我们会在测试后给您回复
  • 好的,谢谢
  • 请您参考TRM的 26.16.2.21 CAN_IP_MUX21 Register (Offset = D8h) [reset = 0h]

    https://www.ti.com.cn/cn/lit/ug/sprui33c/sprui33c.pdf 

    在代码中您可以search一下

    //*****************************************************************************
    //
    //! Set the CAN controller Interrupt Line for each mailbox
    //!
    //! \param base is the base address of the CAN controller.
    //! \param mux bit packed representation of which message objects should
    //!        generate an interrupt on a given interrupt line.
    //!
    //! Selects which interrupt line each message object should assert when an
    //! interrupt occurs. Bit 0 corresponds to message object 32 and then bits
    //! 1 to 31 correspond to message object 1 through 31 respectively. Bits that
    //! are asserted indicate the message object should generate an interrupt on
    //! interrupt line 1, while bits that are not asserted indicate the message
    //! object should generate an interrupt on line 0.
    //!
    //! \return None.
    //
    //*****************************************************************************
    static inline void
    CAN_setInterruptMux(uint32_t base, uint32_t mux)
    {
        //
        // Check the arguments.
        //
        ASSERT(CAN_isBaseValid(base));
    
        //
        // Set the interrupt muxing for the CAN peripheral
        //
        HWREG_BP(base + CAN_O_IP_MUX21) = mux;
    }

  • 你好,很感谢你的回答,我加入了这行函数,可是,还是进不了中断。请问你有完整的有关CAN_INT_IE1的中断设置代码吗?如果有,能提供给我参考一下吗?非常感谢
  • 很抱歉,我这边暂时没有完整的有关CAN_INT_IE1的中断设置代码,且手边暂时没有板子,我会在周一给您详细代码。

  • 不用了,我这边已经测试好了,不过还是感谢你的回答。还有,现在我在测试中发现我没有加入滤波的情况下,有其他ID接收时依然可以屏蔽掉。请问,这个是F280049芯片本身已经设置好滤波了吗
  • 关于此问题,我之前有回复过其他客户,您可以参考下配置代码

    e2echina.ti.com/.../576839