This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377d双核离线运行FLASH_STANDALONE模式设置



你好,我是用自己的例程写的程序,想请问您一些问题:

1.我是用的自己的程序,那么我的小锤子旁边的三角下拉菜单只有“DEBUG”和“Release”两种模式,那么我该如何创建standalone模式呢?

2.请问是否需要加入预定义?如果是,该如何具体设置呢??

3我使用的是ccs7.4,这个设置问题和我使用的ccs版本有关系吗?

非常期待有心人的回答,感谢~~~

  • user6045432 说:
    1.我是用的自己的程序,那么我的小锤子旁边的三角下拉菜单只有“DEBUG”和“Release”两种模式,那么我该如何创建standalone模式呢?

    要独立运行,您需要将代码加载到Flash中,并将BOOTMODE引脚设置设置为BOOT to flash。

    对于standalone模式,需要将GPIO84和GPIO72驱动为高电平并将TRSTn驱动为低电平。

    另外,检查OTP_KEY的内容并确保它不是0x5A。如果是这样,则需要正确配置OTP_BMode。

    user6045432 说:
    2.请问是否需要加入预定义?如果是,该如何具体设置呢??

    是需要预定义的

    _STANDALONE

    user6045432 说:
    3我使用的是ccs7.4,这个设置问题和我使用的ccs版本有关系吗?

    CCS7应该是可以的