This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
user6154541 说:好的,非常感谢,我刚测试了,claisr7 和claisr8都能进入。
若是解决您的问题,请点击“确认此为答案”
user6154541 说:task7 和task8与claisr7和claisr8是什么关系?task7和task8是用的汇编,请问task7和task8是什么一直在运行吗?还是和claisr7和claiscla8一样在cla的中断触发源到来之后运行?
该问题和最开始的帖子不同,我会将该帖子拆分为新帖以便于查看
您好,我配置的是EPWM3中断触发cla task1,软件触发cla task8。在BSP_HRPWM.c中EPWM3配置了中断源,在BSP_CLA.c中配置了cla task1的中断触发源为EPWM3,cla task8为软件触发,并强制触发cla task8一次。InitFlash函数在f28004x_sysctrl.c中初始化,cla的具体配置都在BSP_CLA.c程序文件里边。想截图给您看看,但是不知道这个怎么粘贴图片。
参考 280049 TRM 的 5.4.2 Typical CLA Initialization Sequence可知
CLA 的初始化流程
对照您的初始化流程,没有看到Enable CLA tasks/interrupts等
我在BSP_CLA.c 文件里边的void CLA_C_Init(void)函数里边配置的。
可以参考例程内的写法
//
// Map the ISR to the CLA end-of-task interrupt.
//
Interrupt_register(INT_CLA1_1, cla1Isr1);
//*****************************************************************************
//
//! Registers a function to be called when an interrupt occurs.
//!
//! \param interruptNumber specifies the interrupt in question.
//! \param handler is a pointer to the function to be called.
//!
//! This function is used to specify the handler function to be called when the
//! given interrupt is asserted to the processor. When the interrupt occurs,
//! if it is enabled (via Interrupt_enable()), the handler function will be
//! called in interrupt context. Since the handler function can preempt other
//! code, care must be taken to protect memory or peripherals that are accessed
//! by the handler and other non-handler code.
//!
//! The available \e interruptNumber values are supplied in
//! <tt>inc/hw_ints.h</tt>.
//!
//! \note This function assumes that the PIE has been enabled. See
//! Interrupt_initModule().
//!
//! \return None.
//
//*****************************************************************************
static inline void
Interrupt_register(uint32_t interruptNumber, void (*handler)(void))
{
uint32_t address;
//
// Calculate appropriate address for the interrupt number
//
address = (uint32_t)PIEVECTTABLE_BASE +
(((interruptNumber & 0xFFFF0000U) >> 16U) * 2U);
//
// Copy ISR address into PIE table
//
EALLOW;
HWREG(address) = (uint32_t)handler;
EDIS;
}
改成CLA_TRIG_EPWM2INT就可以了。您原来是CLA_TRIG_EPWM3INT,而程序中又没有使能EPWM3INT,所以不能触发CLA
//
// Set the EPWM3 as the trigger for task 1
//
DmaClaSrcSelRegs.CLA1TASKSRCSEL1.bit.TASK1 = CLA_TRIG_EPWM2INT;;
另外需要在__interrupt void Cla1Task1 ( void )中加入下面的语句以方便调试
__mdebugstop();