This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

基于TMS320F28335的电机开发套件?

Expert 1119 points

Other Parts Discussed in Thread: TMDSCNCD28335, CONTROLSUITE

请问有没有基于TMS320F28335的电机开发套件呢?低压电机

我看了官网上的TMDSCNCD28335,该套件是可以插到可以插到高压套件基板上的。

1,我需要的只是驱动48V电机,功率也就100——200W,不知道有没有什么方案呢?

2,另外,我有一块DRV8301-69M-KIT板子,可以直接用于TMDSCNCD28335吗?

3,软件方面TMDSCNCD28335支持电机开发吗?类似motoware之类?

  • 1、目前TI提供的基于F28335的电机开发套件只有高压套件:TMDSHVMTRPFCKIT,如果低压的话可以考虑F28035,选择更多一些:www.ti.com.cn/.../TMS320F28035

    2、DRV8301-69M-KIT是一款完整的电机控制套件,而TMDSCNCD28335只是控制卡。你是不是说反了?不过TMDSCNCD28335也不能用于DRV8301-69M-KIT,因为DRV8301-69M-KIT是需要带instaspin算法的芯片的(尾缀带"F"或者"M"的芯片型号)

    3、如果是TMDSHVMTRPFCKIT的话可以在controlSUITE中找到对应的电机控制例程:C:\ti\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v2.1
  • 您好,您所描述的我已经明白,还有想继续请教一下:

    一、如果不局限于28335芯片,那么针对48V(5Amax)的电机控制套件,有什么推荐吗?客户强调了两条需求:1,需要编码器;2,可以控制同步电机和异步电机(不是同时)

    二、我现有的DRV8301-69M-KIT + 28069的组合,是否满足上述条件?

  • 可以满足的,F28069得是带尾缀"F"或者"M"的,比如F28069F或者F28069M。这样的话可以使用TI的instaSPIN算法,有感无感,同步异步电机都可以控制。
  • HVMotorCtrl+PfcKit_v2.1 这个我下载的Controlsuite没找到,是不是得重新到哪个地方下载!