This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【求助】DSP通过xintf访问fpga,写的数据不正常,读的数据正常,是怎么回事呢?



在坛子上看到一个类似的帖子,但和他的情况又不完全相同,耽搁好几天了,一直没有解决:

我用的是f28335和fpga通过xintf通信,选用的是zone7,配置如下:

 EALLOW;

XintfRegs.XINTCNF2.bit.XTIMCLK = 1;
// No write buffering
XintfRegs.XINTCNF2.bit.WRBUFF = 0;
// XCLKOUT is enabled
XintfRegs.XINTCNF2.bit.CLKOFF = 0;
// XCLKOUT = XTIMCLK/2
XintfRegs.XINTCNF2.bit.CLKMODE = 0;

XintfRegs.XTIMING7.bit.XWRLEAD = 2;
XintfRegs.XTIMING7.bit.XWRACTIVE = 5;
XintfRegs.XTIMING7.bit.XWRTRAIL = 2;
// Zone read timing
XintfRegs.XTIMING7.bit.XRDLEAD = 3;
XintfRegs.XTIMING7.bit.XRDACTIVE = 7;
XintfRegs.XTIMING7.bit.XRDTRAIL = 3;

// double all Zone read/write lead/active/trail timing
// XintfRegs.XTIMING7.bit.X2TIMING = 1;
XintfRegs.XTIMING7.bit.X2TIMING = 0;

// Zone will sample XREADY signal
//XintfRegs.XTIMING7.bit.USEREADY = 1;
XintfRegs.XTIMING7.bit.USEREADY = 0;
XintfRegs.XTIMING7.bit.READYMODE = 0; // sample asynchronous

// Size must be either:
// 0,1 = x32 or
// 1,1 = x16 other values are reserved
XintfRegs.XTIMING7.bit.XSIZE = 3;

// Bank switching
// Assume Zone 7 is slow, so add additional BCYC cycles
// when ever switching from Zone 7 to another Zone.
// This will help avoid bus contention.
XintfRegs.XBANK.bit.BANK = 7;
XintfRegs.XBANK.bit.BCYC = 7;

///GPIO属性配置

GpioCtrlRegs.GPCMUX1.bit.GPIO64 = 3; // XD15
GpioCtrlRegs.GPCMUX1.bit.GPIO65 = 3; // XD14
GpioCtrlRegs.GPCMUX1.bit.GPIO66 = 3; // XD13
GpioCtrlRegs.GPCMUX1.bit.GPIO67 = 3; // XD12
GpioCtrlRegs.GPCMUX1.bit.GPIO68 = 3; // XD11
GpioCtrlRegs.GPCMUX1.bit.GPIO69 = 3; // XD10
GpioCtrlRegs.GPCMUX1.bit.GPIO70 = 3; // XD19
GpioCtrlRegs.GPCMUX1.bit.GPIO71 = 3; // XD8
GpioCtrlRegs.GPCMUX1.bit.GPIO72 = 3; // XD7
GpioCtrlRegs.GPCMUX1.bit.GPIO73 = 3; // XD6
GpioCtrlRegs.GPCMUX1.bit.GPIO74 = 3; // XD5
GpioCtrlRegs.GPCMUX1.bit.GPIO75 = 3; // XD4
GpioCtrlRegs.GPCMUX1.bit.GPIO76 = 3; // XD3
GpioCtrlRegs.GPCMUX1.bit.GPIO77 = 3; // XD2
GpioCtrlRegs.GPCMUX1.bit.GPIO78 = 3; // XD1
GpioCtrlRegs.GPCMUX1.bit.GPIO79 = 3; // XD0

GpioCtrlRegs.GPBMUX1.bit.GPIO40 = 3; // XA0/XWE1n
GpioCtrlRegs.GPBMUX1.bit.GPIO41 = 3; // XA1
GpioCtrlRegs.GPBMUX1.bit.GPIO42 = 3; // XA2
GpioCtrlRegs.GPBMUX1.bit.GPIO43 = 3; // XA3
GpioCtrlRegs.GPBMUX1.bit.GPIO44 = 3; // XA4
GpioCtrlRegs.GPBMUX1.bit.GPIO45 = 3; // XA5
GpioCtrlRegs.GPBMUX1.bit.GPIO46 = 3; // XA6
GpioCtrlRegs.GPBMUX1.bit.GPIO47 = 3; // XA7

GpioCtrlRegs.GPCMUX2.bit.GPIO80 = 3; // XA8
GpioCtrlRegs.GPCMUX2.bit.GPIO81 = 3; // XA9
GpioCtrlRegs.GPCMUX2.bit.GPIO82 = 3; // XA10
GpioCtrlRegs.GPCMUX2.bit.GPIO83 = 3; // XA11
GpioCtrlRegs.GPCMUX2.bit.GPIO84 = 3; // XA12
GpioCtrlRegs.GPCMUX2.bit.GPIO85 = 3; // XA13
GpioCtrlRegs.GPCMUX2.bit.GPIO86 = 3; // XA14
GpioCtrlRegs.GPCMUX2.bit.GPIO87 = 3; // XA15
GpioCtrlRegs.GPBMUX1.bit.GPIO39 = 3; // XA16
GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 3; // XA17
GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 3; // XA18
GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 3; // XA19

GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 3; // XREADY
GpioCtrlRegs.GPBMUX1.bit.GPIO35 = 3; // XRNW
GpioCtrlRegs.GPBMUX1.bit.GPIO38 = 3; // XWE0

GpioCtrlRegs.GPBMUX1.bit.GPIO36 = 3; // XZCS0
GpioCtrlRegs.GPBMUX1.bit.GPIO37 = 3; // XZCS7
GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 3; // XZCS6


EDIS;

asm(" RPT #7 || NOP");

写访问程序为:

Uint16    *ExRamStart = (Uint16 *)0x200000;

*(ExRamStart + 1) = 0x5a5a;
*(ExRamStart + 2) = 0x1234;
*(ExRamStart + 3) = 0xa5a5;
*(ExRamStart + 4) = 0x4321;
*(ExRamStart + 5) = 0x5678;
*(ExRamStart + 6) = 0x9abc;
*(ExRamStart + 7) = 0xcdef;
*(ExRamStart + 8) = 0xfdec;

单步断点执行,在fpga端通过chipscope抓取数据,发现数据总线上的值和程序中写入的大部分时间都不一致,地址总线没有问题,回读也没有问题,DSP这边对应的配置寄存器也看了,确实和程序配置中的一致,查看memory的值也不对。写入的数据在不断的翻转,而且最终也没有程序写入的数据,这个会是什么问题呢?

能帮忙分析一下吗?谢谢!