1. 28388的CPU2和CM想设置成在RAM中启动。根据资料看CPU2和CM的启动RAM只有1至2K,如何运行比较大的程序。
2. 28388的DSP有没有办法访问到CPU2和CM的全部RAM,以及28388的DSP1能不能访问到CPU2和CM的全部flash。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 28388的CPU2和CM想设置成在RAM中启动。根据资料看CPU2和CM的启动RAM只有1至2K,如何运行比较大的程序。
2. 28388的DSP有没有办法访问到CPU2和CM的全部RAM,以及28388的DSP1能不能访问到CPU2和CM的全部flash。
你好:
1、TI的函数库中有个函数Memcpy()就是用于脱机运行的时候将flash运行的程序移植到ram运行,例如你可以参考例程C:\ti\c2000\C2000Ware_3_02_00_00\driverlib\f2838x\examples\c28x_cm\led中的以下代码:
#ifdef _FLASH
//
// Copy time critical code and flash setup code to RAM. This includes the
// following functions: InitFlash();
//
// The RamfuncsLoadStart, RamfuncsLoadSize, and RamfuncsRunStart symbols
// are created by the linker. Refer to the device .cmd file.
//
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
//
// Call Flash Initialization to setup flash waitstates. This function must
// reside in RAM.
//
Flash_initModule(FLASH0CTRL_BASE, FLASH0ECC_BASE, DEVICE_FLASH_WAITSTATES);
#endif
2、访问内存和flash肯定得看你具体如何设置,我觉得你应该是要问这几个核之间访问外设的权限吧?外设权限你可以参考一下这个功能方框图: