This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28035基于串口在线升级后,CLA不运行



目标:ti 28035芯片
实现功能:通过串口在线升级(自己写bootloader)
目前进展:已经可以实现上位机通过串口给DSP在线升级,并能完成boot层跳转APP层,主CPU程序运行无误,但另外一个核CLA没跑起来。

实现思路:
创建两个工程,分别实现bootloader和上层app。
bootloader运行后,判断是否已经在线升级过,是就直接跳转app,否则接受上位机升级命令,并和上位机通信完成接收数据并烧写flash,之后跳转APP。

现在的问题大概在CMD文件配置上,也就是boot层和APP层的flash以及ram的划分上。
bootloader 代码划分在flashA上,app划分在flashH~flashD上,其他的ram没有做大的改动。以下为boot层的cmd文件内容:

CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
_Cla1Prog_Start = _Cla1funcsRunStart;
-heap 0x100
-m UltraSonicPower200.map


MEMORY
{
PAGE 0:    /* Program Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
   RAMLISR_PRG   : origin = 0x008000, length = 0x000100     /* on-chip RAM block L0 */
   RAMLAPP_PRG   : origin = 0x008100, length = 0x000400     /* on-chip RAM block L0 */
   //RAMLBOOT_PRG : origin = 0x008400, length = 0x000100      /* on-chip RAM block L0 */
   //RAML1       : origin = 0x008800, length = 0x000400     /* on-chip RAM block L1 */
   RAML3       : origin = 0x009000, length = 0x001000     /* on-chip RAM block L3, for CLA run code */
   OTP         : origin = 0x3D7800, length = 0x000400     /* on-chip OTP */
   FLASHH      : origin = 0x3e8000, length = 0x00A000     /* on-chip FLASH */


  //FLASHH      : origin = 0x3E8000, length = 0x002000     /* on-chip FLASH */
  //FLASHG      : origin = 0x3EA000, length = 0x002000     /* on-chip FLASH */
  //FLASHF      : origin = 0x3EC000, length = 0x002000     /* on-chip FLASH */
  //FLASHE      : origin = 0x3EE000, length = 0x002000     /* on-chip FLASH */
  //FLASHD      : origin = 0x3F0000, length = 0x002000     /* on-chip FLASH */
   FLASHC      : origin = 0x3F2000, length = 0x002000     /* on-chip FLASH */
   FLASHA      : origin = 0x3F6000, length = 0x001F80     /* on-chip FLASH */
   CSM_RSVD    : origin = 0x3F7F80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
   BEGIN       : origin = 0x3F7FF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
   CSM_PWL_P0  : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */


   IQTABLES    : origin = 0x3FE000, length = 0x000B50     /* IQ Math Tables in Boot ROM */
   IQTABLES2   : origin = 0x3FEB50, length = 0x00008C     /* IQ Math Tables in Boot ROM */
   IQTABLES3   : origin = 0x3FEBDC, length = 0x0000AA          /* IQ Math Tables in Boot ROM */


   ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */
   RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
   VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */


PAGE 1 :   /* Data Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
           /* Registers remain on PAGE1                                                  */
   BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
   RAMM0       : origin = 0x000080, length = 0x0007B0     /* on-chip RAM block M0, and M1 is incorporated to M0 */
//  RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
   DataRAM     : origin = 0x008500, length = 0x0006FF       /*on-chip RAM block L0,L1 */
   BootFlagRAM : origin = 0x008BFF, length = 0x000001     /* on-chip RAM block L1 */
   CLARAM1       : origin = 0x008C00, length = 0x000400     /* on-chip RAM block L2 */
   //RAML3       : origin = 0x009000, length = 0x001000     /* on-chip RAM block L3 */


   CLA1_MSGRAMLOW   : origin = 0x001480, length = 0x000080
   CLA1_MSGRAMHIGH  : origin = 0x001500, length = 0x000080


   FLASHB      : origin = 0x3F4000, length = 0x002000     /* on-chip FLASH */


}


SECTIONS
{


   /* Allocate program areas: */
   .cinit              : > FLASHA      PAGE = 0
   .pinit              : > FLASHA,     PAGE = 0
   .text               : > FLASHA      PAGE = 0
   codestart           : > BEGIN       PAGE = 0


   IsrRamfuncs                : LOAD = FLASHA,
                         RUN = RAMLISR_PRG,
                         LOAD_START(_IsrRamfuncsLoadStart),
                         LOAD_END(_IsrRamfuncsLoadEnd),
                         RUN_START(_IsrRamfuncsRunStart),
                         PAGE = 0


   ramfuncs            : LOAD = FLASHA,
                         RUN = RAMLAPP_PRG,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         PAGE = 0

   csmpasswds          : > CSM_PWL_P0  PAGE = 0
   csm_rsvd            : > CSM_RSVD    PAGE = 0




   debug_ram           : > DataRAM     PAGE = 1
   BootFlagRam         : > BootFlagRAM PAGE = 1
   /* Allocate uninitalized data sections: */
   //.stack              : > RAMM0       PAGE = 1
   .stack              : > DataRAM       PAGE = 1
   .ebss               : > RAMM0       PAGE = 1
  // .esysmem            : > RAMM0       PAGE = 1
   //.sysmem            : > RAMM0       PAGE = 1


   /* Initalized sections go in Flash */
   /* For SDFlash to program these, they must be allocated to page 0 */
   .econst             : > FLASHA      PAGE = 0
   .switch             : > FLASHA      PAGE = 0


   /* Allocate IQ math areas: */
   IQmath              : > FLASHA      PAGE = 0            /* Math Code */
   IQmathTables        : > IQTABLES,   PAGE = 0, TYPE = NOLOAD


   .bss_cla                       : > CLARAM1,   PAGE = 1
   .scratchpad         : > CLARAM1,   PAGE = 1


   Cla1Prog            : LOAD = FLASHH,
                         RUN = RAML3,
                         LOAD_START(_Cla1funcsLoadStart),
                         LOAD_END(_Cla1funcsLoadEnd),
                         RUN_START(_Cla1funcsRunStart),
                         LOAD_SIZE(_Cla1funcsLoadSize),
                         PAGE = 0


   Cla1ToCpuMsgRAM     : > CLA1_MSGRAMLOW,   PAGE = 1
   CpuToCla1MsgRAM     : > CLA1_MSGRAMHIGH,  PAGE = 1
//   Cla1DataRam0                   : > CLARAM0,                  PAGE = 1
   Cla1DataRam1                   : > CLARAM1,                  PAGE = 1


   CLA1mathTables           : LOAD = FLASHB,
                         RUN = CLARAM1,
                         LOAD_START(_Cla1mathTablesLoadStart),
                         LOAD_END(_Cla1mathTablesLoadEnd),
                         RUN_START(_Cla1mathTablesRunStart),
                         LOAD_SIZE(_Cla1mathTablesLoadSize),
                         PAGE = 1


   CLAscratch          :
                       { *.obj(CLAscratch)
                       . += CLA_SCRATCHPAD_SIZE;
                       *.obj(CLAscratch_end) } > CLARAM1,
                                           PAGE = 1

   /*
   IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
   {


              IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)


   }




   /* .reset is a standard section used by the compiler.  It contains the */
   /* the address of the start of _c_int00 for C Code.   /*
   /* When using the boot ROM this section and the CPU vector */
   /* table is not needed.  Thus the default type is set here to  */
   /* DSECT  */
   .reset              : > RESET,      PAGE = 0, TYPE = DSECT
   vectors             : > VECTORS     PAGE = 0, TYPE = DSECT


}


/*
//===========================================================================
// End of file.
//===========================================================================
*/


cmd文件界定了flash和ram的使用,现在就是不太清楚,cmd到底是不是有问题?
一下是APP层的cmd文件内容:


CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
_Cla1Prog_Start = _Cla1funcsRunStart;
-heap 0x100
-m UltraSonicPower200.map


MEMORY
{
PAGE 0:    /* Program Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
   RAMLISR_PRG   : origin = 0x008000, length = 0x000100     /* on-chip RAM block L0 */
   RAMLAPP_PRG   : origin = 0x008100, length = 0x000300     /* on-chip RAM block L0 */
   RAMLBOOT_PRG : origin = 0x008400, length = 0x000100      /* on-chip RAM block L0 */
   //RAML1       : origin = 0x008800, length = 0x000400     /* on-chip RAM block L1 */
   RAML3       : origin = 0x009000, length = 0x001000     /* on-chip RAM block L3, for CLA run code */
   OTP         : origin = 0x3D7800, length = 0x000400     /* on-chip OTP */
   FLASHH      : origin = 0x3E8004, length = 0x009FFC     /* on-chip FLASH 0x3E8002 as begin 0x3E8000 as Flashed_flag*/


  //FLASHH      : origin = 0x3E8000, length = 0x002000     /* on-chip FLASH */
  //FLASHG      : origin = 0x3EA000, length = 0x002000     /* on-chip FLASH */
  //FLASHF      : origin = 0x3EC000, length = 0x002000     /* on-chip FLASH */
  //FLASHE      : origin = 0x3EE000, length = 0x002000     /* on-chip FLASH */
  //FLASHD      : origin = 0x3F0000, length = 0x002000     /* on-chip FLASH */
   FLASHC      : origin = 0x3F2000, length = 0x002000     /* on-chip FLASH */
   FLASHA      : origin = 0x3F6000, length = 0x001F80     /* on-chip FLASH */
   CSM_RSVD    : origin = 0x3F7F80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
   //BEGIN       : origin = 0x3F7FF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
   BEGIN       : origin = 0x3E8002, length = 0x000002     /* Part of FLASHH.  . */
   CSM_PWL_P0  : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */


   IQTABLES    : origin = 0x3FE000, length = 0x000B50     /* IQ Math Tables in Boot ROM */
   IQTABLES2   : origin = 0x3FEB50, length = 0x00008C     /* IQ Math Tables in Boot ROM */
   IQTABLES3   : origin = 0x3FEBDC, length = 0x0000AA          /* IQ Math Tables in Boot ROM */


   ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */
   RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
   VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */


PAGE 1 :   /* Data Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
           /* Registers remain on PAGE1                                                  */
   BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
   RAMM0       : origin = 0x000080, length = 0x0007B0     /* on-chip RAM block M0, and M1 is incorporated to M0 */
//  RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
   DataRAM     : origin = 0x008500, length = 0x0006FF       /*on-chip RAM block L0,L1 */
   BootFlagRAM : origin = 0x008BFF, length = 0x000001     /* on-chip RAM block L1 */
   CLARAM1       : origin = 0x008C00, length = 0x000400     /* on-chip RAM block L2 */
   //RAML3       : origin = 0x009000, length = 0x001000     /* on-chip RAM block L3 */


   CLA1_MSGRAMLOW   : origin = 0x001480, length = 0x000080
   CLA1_MSGRAMHIGH  : origin = 0x001500, length = 0x000080


   FLASHB      : origin = 0x3F4000, length = 0x002000     /* on-chip FLASH */


}


SECTIONS
{


   /* Allocate program areas: */
   .cinit              : > FLASHH      PAGE = 0
   .pinit              : > FLASHH,     PAGE = 0
   .text               : > FLASHH      PAGE = 0
   codestart           : > BEGIN       PAGE = 0


   IsrRamfuncs                : LOAD = FLASHH,
                         RUN = RAMLISR_PRG,
                         LOAD_START(_IsrRamfuncsLoadStart),
                         LOAD_END(_IsrRamfuncsLoadEnd),
                         RUN_START(_IsrRamfuncsRunStart),
                         PAGE = 0


   ramfuncs            : LOAD = FLASHH,
                         RUN = RAMLAPP_PRG,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         PAGE = 0
                        
   csmpasswds          : > CSM_PWL_P0  PAGE = 0
   csm_rsvd            : > CSM_RSVD    PAGE = 0




   debug_ram           : > DataRAM     PAGE = 1
   BootFlagRam         : > BootFlagRAM PAGE = 1
   /* Allocate uninitalized data sections: */
   //.stack              : > RAMM0       PAGE = 1
   .stack              : > DataRAM       PAGE = 1
   .ebss               : > RAMM0       PAGE = 1
  // .esysmem            : > RAMM0       PAGE = 1
   //.sysmem            : > RAMM0       PAGE = 1


   /* Initalized sections go in Flash */
   /* For SDFlash to program these, they must be allocated to page 0 */
   .econst             : > FLASHH      PAGE = 0
   .switch             : > FLASHH      PAGE = 0


   /* Allocate IQ math areas: */
   IQmath              : > FLASHA      PAGE = 0            /* Math Code */
   IQmathTables        : > IQTABLES,   PAGE = 0, TYPE = NOLOAD


   .bss_cla                       : > CLARAM1,   PAGE = 1
   .scratchpad         : > CLARAM1,   PAGE = 1


   Cla1Prog            : LOAD = FLASHH,
                         RUN = RAML3,
                         LOAD_START(_Cla1funcsLoadStart),
                         LOAD_END(_Cla1funcsLoadEnd),
                         RUN_START(_Cla1funcsRunStart),
                         LOAD_SIZE(_Cla1funcsLoadSize),
                         PAGE = 0


   Cla1ToCpuMsgRAM     : > CLA1_MSGRAMLOW,   PAGE = 1
   CpuToCla1MsgRAM     : > CLA1_MSGRAMHIGH,  PAGE = 1
//   Cla1DataRam0                   : > CLARAM0,                  PAGE = 1
   Cla1DataRam1                   : > CLARAM1,                  PAGE = 1


   CLA1mathTables           : LOAD = FLASHB,
                         RUN = CLARAM1,
                         LOAD_START(_Cla1mathTablesLoadStart),
                         LOAD_END(_Cla1mathTablesLoadEnd),
                         RUN_START(_Cla1mathTablesRunStart),
                         LOAD_SIZE(_Cla1mathTablesLoadSize),
                         PAGE = 1


   CLAscratch          :
                       { *.obj(CLAscratch)
                       . += CLA_SCRATCHPAD_SIZE;
                       *.obj(CLAscratch_end) } > CLARAM1,
                                           PAGE = 1

   /*
   IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
   {


              IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)


   }
   */

    /*
    IQmathTables3    : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
    {


               IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)


    }
    */




   /* .reset is a standard section used by the compiler.  It contains the */
   /* the address of the start of _c_int00 for C Code.   /*
   /* When using the boot ROM this section and the CPU vector */
   /* table is not needed.  Thus the default type is set here to  */
   /* DSECT  */
   .reset              : > RESET,      PAGE = 0, TYPE = DSECT
   vectors             : > VECTORS     PAGE = 0, TYPE = DSECT


}


/*
//===========================================================================
// End of file.
//===========================================================================
*/




希望做个的和要做的工程师们一起来讨论一下,有时候一些问题往往是在互相讨论中解决的,而且讨论问题还能互相学习没有遇到过的问题