目标:ti 28035芯片
实现功能:通过串口在线升级(自己写bootloader)
目前进展:已经可以实现上位机通过串口给DSP在线升级,并能完成boot层跳转APP层,主CPU程序运行无误,但另外一个核CLA没跑起来。
实现思路:
创建两个工程,分别实现bootloader和上层app。
bootloader运行后,判断是否已经在线升级过,是就直接跳转app,否则接受上位机升级命令,并和上位机通信完成接收数据并烧写flash,之后跳转APP。
现在的问题大概在CMD文件配置上,也就是boot层和APP层的flash以及ram的划分上。
bootloader 代码划分在flashA上,app划分在flashH~flashD上,其他的ram没有做大的改动。以下为boot层的cmd文件内容:
CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
_Cla1Prog_Start = _Cla1funcsRunStart;
-heap 0x100
-m UltraSonicPower200.map
MEMORY
{
PAGE 0: /* Program Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
RAMLISR_PRG : origin = 0x008000, length = 0x000100 /* on-chip RAM block L0 */
RAMLAPP_PRG : origin = 0x008100, length = 0x000400 /* on-chip RAM block L0 */
//RAMLBOOT_PRG : origin = 0x008400, length = 0x000100 /* on-chip RAM block L0 */
//RAML1 : origin = 0x008800, length = 0x000400 /* on-chip RAM block L1 */
RAML3 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L3, for CLA run code */
OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
FLASHH : origin = 0x3e8000, length = 0x00A000 /* on-chip FLASH */
//FLASHH : origin = 0x3E8000, length = 0x002000 /* on-chip FLASH */
//FLASHG : origin = 0x3EA000, length = 0x002000 /* on-chip FLASH */
//FLASHF : origin = 0x3EC000, length = 0x002000 /* on-chip FLASH */
//FLASHE : origin = 0x3EE000, length = 0x002000 /* on-chip FLASH */
//FLASHD : origin = 0x3F0000, length = 0x002000 /* on-chip FLASH */
FLASHC : origin = 0x3F2000, length = 0x002000 /* on-chip FLASH */
FLASHA : origin = 0x3F6000, length = 0x001F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */
IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */
IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */
ROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
/* Registers remain on PAGE1 */
BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x000080, length = 0x0007B0 /* on-chip RAM block M0, and M1 is incorporated to M0 */
// RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
DataRAM : origin = 0x008500, length = 0x0006FF /*on-chip RAM block L0,L1 */
BootFlagRAM : origin = 0x008BFF, length = 0x000001 /* on-chip RAM block L1 */
CLARAM1 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */
//RAML3 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L3 */
CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080
FLASHB : origin = 0x3F4000, length = 0x002000 /* on-chip FLASH */
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHA PAGE = 0
.pinit : > FLASHA, PAGE = 0
.text : > FLASHA PAGE = 0
codestart : > BEGIN PAGE = 0
IsrRamfuncs : LOAD = FLASHA,
RUN = RAMLISR_PRG,
LOAD_START(_IsrRamfuncsLoadStart),
LOAD_END(_IsrRamfuncsLoadEnd),
RUN_START(_IsrRamfuncsRunStart),
PAGE = 0
ramfuncs : LOAD = FLASHA,
RUN = RAMLAPP_PRG,
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
PAGE = 0
csmpasswds : > CSM_PWL_P0 PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0
debug_ram : > DataRAM PAGE = 1
BootFlagRam : > BootFlagRAM PAGE = 1
/* Allocate uninitalized data sections: */
//.stack : > RAMM0 PAGE = 1
.stack : > DataRAM PAGE = 1
.ebss : > RAMM0 PAGE = 1
// .esysmem : > RAMM0 PAGE = 1
//.sysmem : > RAMM0 PAGE = 1
/* Initalized sections go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : > FLASHA PAGE = 0
.switch : > FLASHA PAGE = 0
/* Allocate IQ math areas: */
IQmath : > FLASHA PAGE = 0 /* Math Code */
IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD
.bss_cla : > CLARAM1, PAGE = 1
.scratchpad : > CLARAM1, PAGE = 1
Cla1Prog : LOAD = FLASHH,
RUN = RAML3,
LOAD_START(_Cla1funcsLoadStart),
LOAD_END(_Cla1funcsLoadEnd),
RUN_START(_Cla1funcsRunStart),
LOAD_SIZE(_Cla1funcsLoadSize),
PAGE = 0
Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1
// Cla1DataRam0 : > CLARAM0, PAGE = 1
Cla1DataRam1 : > CLARAM1, PAGE = 1
CLA1mathTables : LOAD = FLASHB,
RUN = CLARAM1,
LOAD_START(_Cla1mathTablesLoadStart),
LOAD_END(_Cla1mathTablesLoadEnd),
RUN_START(_Cla1mathTablesRunStart),
LOAD_SIZE(_Cla1mathTablesLoadSize),
PAGE = 1
CLAscratch :
{ *.obj(CLAscratch)
. += CLA_SCRATCHPAD_SIZE;
*.obj(CLAscratch_end) } > CLARAM1,
PAGE = 1
/*
IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
}
/* .reset is a standard section used by the compiler. It contains the */
/* the address of the start of _c_int00 for C Code. /*
/* When using the boot ROM this section and the CPU vector */
/* table is not needed. Thus the default type is set here to */
/* DSECT */
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
cmd文件界定了flash和ram的使用,现在就是不太清楚,cmd到底是不是有问题?
一下是APP层的cmd文件内容:
CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
_Cla1Prog_Start = _Cla1funcsRunStart;
-heap 0x100
-m UltraSonicPower200.map
MEMORY
{
PAGE 0: /* Program Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
RAMLISR_PRG : origin = 0x008000, length = 0x000100 /* on-chip RAM block L0 */
RAMLAPP_PRG : origin = 0x008100, length = 0x000300 /* on-chip RAM block L0 */
RAMLBOOT_PRG : origin = 0x008400, length = 0x000100 /* on-chip RAM block L0 */
//RAML1 : origin = 0x008800, length = 0x000400 /* on-chip RAM block L1 */
RAML3 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L3, for CLA run code */
OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
FLASHH : origin = 0x3E8004, length = 0x009FFC /* on-chip FLASH 0x3E8002 as begin 0x3E8000 as Flashed_flag*/
//FLASHH : origin = 0x3E8000, length = 0x002000 /* on-chip FLASH */
//FLASHG : origin = 0x3EA000, length = 0x002000 /* on-chip FLASH */
//FLASHF : origin = 0x3EC000, length = 0x002000 /* on-chip FLASH */
//FLASHE : origin = 0x3EE000, length = 0x002000 /* on-chip FLASH */
//FLASHD : origin = 0x3F0000, length = 0x002000 /* on-chip FLASH */
FLASHC : origin = 0x3F2000, length = 0x002000 /* on-chip FLASH */
FLASHA : origin = 0x3F6000, length = 0x001F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
//BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
BEGIN : origin = 0x3E8002, length = 0x000002 /* Part of FLASHH. . */
CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */
IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */
IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */
ROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
/* Registers remain on PAGE1 */
BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x000080, length = 0x0007B0 /* on-chip RAM block M0, and M1 is incorporated to M0 */
// RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
DataRAM : origin = 0x008500, length = 0x0006FF /*on-chip RAM block L0,L1 */
BootFlagRAM : origin = 0x008BFF, length = 0x000001 /* on-chip RAM block L1 */
CLARAM1 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */
//RAML3 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L3 */
CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080
FLASHB : origin = 0x3F4000, length = 0x002000 /* on-chip FLASH */
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHH PAGE = 0
.pinit : > FLASHH, PAGE = 0
.text : > FLASHH PAGE = 0
codestart : > BEGIN PAGE = 0
IsrRamfuncs : LOAD = FLASHH,
RUN = RAMLISR_PRG,
LOAD_START(_IsrRamfuncsLoadStart),
LOAD_END(_IsrRamfuncsLoadEnd),
RUN_START(_IsrRamfuncsRunStart),
PAGE = 0
ramfuncs : LOAD = FLASHH,
RUN = RAMLAPP_PRG,
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
PAGE = 0
csmpasswds : > CSM_PWL_P0 PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0
debug_ram : > DataRAM PAGE = 1
BootFlagRam : > BootFlagRAM PAGE = 1
/* Allocate uninitalized data sections: */
//.stack : > RAMM0 PAGE = 1
.stack : > DataRAM PAGE = 1
.ebss : > RAMM0 PAGE = 1
// .esysmem : > RAMM0 PAGE = 1
//.sysmem : > RAMM0 PAGE = 1
/* Initalized sections go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : > FLASHH PAGE = 0
.switch : > FLASHH PAGE = 0
/* Allocate IQ math areas: */
IQmath : > FLASHA PAGE = 0 /* Math Code */
IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD
.bss_cla : > CLARAM1, PAGE = 1
.scratchpad : > CLARAM1, PAGE = 1
Cla1Prog : LOAD = FLASHH,
RUN = RAML3,
LOAD_START(_Cla1funcsLoadStart),
LOAD_END(_Cla1funcsLoadEnd),
RUN_START(_Cla1funcsRunStart),
LOAD_SIZE(_Cla1funcsLoadSize),
PAGE = 0
Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1
// Cla1DataRam0 : > CLARAM0, PAGE = 1
Cla1DataRam1 : > CLARAM1, PAGE = 1
CLA1mathTables : LOAD = FLASHB,
RUN = CLARAM1,
LOAD_START(_Cla1mathTablesLoadStart),
LOAD_END(_Cla1mathTablesLoadEnd),
RUN_START(_Cla1mathTablesRunStart),
LOAD_SIZE(_Cla1mathTablesLoadSize),
PAGE = 1
CLAscratch :
{ *.obj(CLAscratch)
. += CLA_SCRATCHPAD_SIZE;
*.obj(CLAscratch_end) } > CLARAM1,
PAGE = 1
/*
IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
}
*/
/*
IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)
}
*/
/* .reset is a standard section used by the compiler. It contains the */
/* the address of the start of _c_int00 for C Code. /*
/* When using the boot ROM this section and the CPU vector */
/* table is not needed. Thus the default type is set here to */
/* DSECT */
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
希望做个的和要做的工程师们一起来讨论一下,有时候一些问题往往是在互相讨论中解决的,而且讨论问题还能互相学习没有遇到过的问题