程序定义在RAM里面运行,出现全局变量初始化正常,单步运行正常,但是全速运行,全局变量出现异常的情况。用的TMDSCNCD280049C开发板
比如g_u16runDebugEn只初始化赋值1,后面没有进行任何的赋值操作。
单步运行,初始化时,值都正常,如下:
但是全速运行F8后,变量值全部异常:
怀疑是CMD的问题,但是始终没找到问题原因:
MAP如下:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
程序定义在RAM里面运行,出现全局变量初始化正常,单步运行正常,但是全速运行,全局变量出现异常的情况。用的TMDSCNCD280049C开发板
比如g_u16runDebugEn只初始化赋值1,后面没有进行任何的赋值操作。
单步运行,初始化时,值都正常,如下:
但是全速运行F8后,变量值全部异常:
怀疑是CMD的问题,但是始终没找到问题原因:
MAP如下:
直接使用官方的 28004x_generic_ram_lnk.cmd 是否也会出现这样的情况?
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */
BEGIN : origin = 0x000000, length = 0x000002
RAMM0 : origin = 0x0000F3, length = 0x00030D
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RESET : origin = 0x3FFFC0, length = 0x000002
/* Flash sectors: you can use FLASH for program memory when the RAM is filled up*/
/* BANK 0 */
FLASH_BANK0_SEC0 : origin = 0x080000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC1 : origin = 0x081000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC3 : origin = 0x083000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC4 : origin = 0x084000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC5 : origin = 0x085000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC6 : origin = 0x086000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC7 : origin = 0x087000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC9 : origin = 0x089000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x001000 /* on-chip Flash */
/* BANK 1 */
FLASH_BANK1_SEC0 : origin = 0x090000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC1 : origin = 0x091000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC2 : origin = 0x092000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC3 : origin = 0x093000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC4 : origin = 0x094000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC5 : origin = 0x095000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC6 : origin = 0x096000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC7 : origin = 0x097000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC8 : origin = 0x098000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC9 : origin = 0x099000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x001000 /* on-chip Flash */
PAGE 1 :
BOOT_RSVD : origin = 0x000002, length = 0x0000F1 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */
// RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMLS6 : origin = 0x00B000, length = 0x000800
RAMLS7 : origin = 0x00B800, length = 0x000800
RAMGS0 : origin = 0x00C000, length = 0x002000
RAMGS1 : origin = 0x00E000, length = 0x002000
RAMGS2 : origin = 0x010000, length = 0x002000
RAMGS3 : origin = 0x012000, length = 0x001FF8
// RAMGS3_RSVD : origin = 0x013FF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
}
/*You can arrange the .text, .cinit, .const, .pinit, .switch and .econst to FLASH when RAM is filled up.*/
SECTIONS
{
codestart : > BEGIN, PAGE = 0
.TI.ramfunc : > RAMM0, PAGE = 0
.text : >> RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 | RAMLS4, PAGE = 0
.cinit : > RAMM0, PAGE = 0
.switch : > RAMM0, PAGE = 0
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.stack : > RAMM1, PAGE = 1
#if defined(__TI_EABI__)
.bss : > RAMLS5, PAGE = 1
.bss:output : > RAMLS5, PAGE = 1
.init_array : > RAMM0, PAGE = 0
.const : > RAMLS5, PAGE = 1
.data : > RAMLS5, PAGE = 1
.sysmem : > RAMLS5, PAGE = 1
.bss:cio : > RAMLS0, PAGE = 0
#else
.pinit : > RAMM0, PAGE = 0
.ebss : > RAMLS5, PAGE = 1
.econst : > RAMLS5, PAGE = 1
.esysmem : > RAMLS5, PAGE = 1
.cio : > RAMLS0, PAGE = 0
#endif
ramgs0 : > RAMGS0, PAGE = 1
ramgs1 : > RAMGS1, PAGE = 1
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/