This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335 GPIO驱动能力



从28335的datasheet上看到,芯片的GPIO的驱动电流能达到4mA,部分管脚(Group 2)的驱动电流能达到8mA。

我将GPIO31配置为GPIO管脚,配置成output,输出高电平,外接一个1K的电阻。

程序运行起来后,高电平被拉低到了1.2V,去掉1K电阻,则正常输出3.3V,

请问有人知道是怎么回事吗?为什么驱动电流达不到手册上写的4mA